MSP430™CapTIvateSoftwareLibraryAPIGuide
1_83_00_05
|
#include <CAPT_Type.h>
Data Fields | |
tElement ** | pElements |
uint8_t | ui8NrOfElements |
typedef tCycle
The cycle structure contains the information regarding the elements which belong to that specific cycle. The total active elements in the cycle are stored, and a pointer to each of these elements.
tElement** tCycle::pElements |
Pointer to an array of element pointers that belong to this cycle. Elements should be ordered in the cycle in accordance with slider/wheel order, if applicable. One element pointer array must be created for each cycle.
uint8_t tCycle::ui8NrOfElements |
Number of elements in this cycle. This must be equal to the size of the pointer array pointed to by pElements.