Introduction¶
The purpose of this document is to give an overview of the Texas Instruments TI 15.4-Stack 2.1.0 Linux® software development kit (SDK). This overview is intended to help developers run the out-of-box example applications and create custom TI 15.4-Stack 2.1.0 applications that run on a Linux host and interface with the CC13x0 device, which runs a media access control (MAC) CoProcessor for the end products.
The TI 15.4-Stack 2.1.0 released as part of the CC13x0 SimpleLink SDK consists of the software stack from TI that implements the Institute of Electrical and Electronics Engineers (IEEE™) standard
802.15.4e/g specification; the TI 15.4-Stack also provides an implementation of a frequency-hopping scheme derived from the Wi-SUN® field area network (FAN) specification. Additionally, the SDK provides required tools, TI-RTOS, and example applications to help developers quickly get started developing star- topology-based wireless network products.
Developers who target products based on the TI 15.4-Stack 2.1.0 have two architectural choices for product development. The first option is to implement the entire TI 15.4-Stack application, which can run within the CC13x0 microcontroller unit (MCU) device. The second option is to have implement the application to run on a host (for example, the Linux operating system [OS]) and interface to the SimpleLink™ CC13x0 ultra-low-power wireless MCU that is running the MAC CoProcessor Application and the TI 15.4-Stack 2.1.0.
This document describes how to use the TI 15.4-Stack 2.1.0 Linux SDK to develop applications running on a Linux host interfacing through a serial interface with the MAC CoProcessor running on the CC13x0 device.
The TI 15.4-Stack 2.1.0 allows for rapid development of low-power and low-cost communication networks with limited power and relaxed throughput requirements. The TI 15.4-Stack is primarily designed to create star-topology wireless networks.
For more details, refer to the IEEE 802.15.4g/e specification documents available on IEEE.org.
SimpleLink, LaunchPad, Sitara, SmartRF, Code Composer Studio, BoosterPack are trademarks of Texas Instruments. ARM is a registered trademark of ARM Ltd.
Ubuntu is a registered trademark of Canonical Limited. Google is a registered trademark of Google Inc. Node.js is a trademark of Joyent, Inc.
Linux is a registered trademark of Linus Torvalds.
IEEE is a trademark of The Institute of Electrical and Electronics Engineers, Inc. Wi-SUN is a registered trademark of WI-SUN Alliance.
ZigBee is a registered trademark of Zigbee Alliance.
All other trademarks are the property of their respective owners.