Revision History
This page lists all relevant changes for all public versions of SmartRF Studio 7:
- Documentation (DOC)
- Startup Window (STARTW)
- Device Control Panel (DCP)
- Configuration data (CFG)
- Firmware (FW)
- Script module (SCRIPT)
- Drivers (DRV)
Version 2.12.0
Release date: January 9, 2019
New Features and Enhancements
- [CC13x2/CC26x2] Radio settings (Preview): All settings updated for revision E devices (SRFSTUDIO-1739).
- [CC13x0] Radio settings: New settings for the 863-930 MHz band: "GFSK 1.2kbps" and "GFSK 2.4kbps" (SRFSTUDIO-771).
- [CC13x2R, CC13x2P] The TX output power values for the 433 MHz frequency band have been updated (SRFSTUDIO-1921).
Bug fixes
- [CC13x0] Solved issue with selection of typical setting "4.8 kbps, OOK (10 dBm Tx power)" when the target board "LAUNCHXL-CC1310-CC1190" is selected.
This resulted in the error: "Failed to calculate Command value" (SRFSTUDIO-1934).
- [CC13x0] Solved issue with Packet TX for the "1.2 kbps, GFSK" and "2.4 kbps, GFSK" settings. The packet interval was too short and packets were lost (SRFSTUDIO-1882).
- [CC13xx, CC26xx] Code Export: The parameter summary given in the generated code file updated. Unrelated parameters removed (SRFSTUDIO-1835).
- [CC13x2/CC26x2] Code Export: Fixed issue with register override pointers being set (different from NULL) even if there are no overrides (SRFSTUDIO-1826).
- [CC13xx/CC26xx] Solved issue with selecting "Cancel" from the "Open config file" dialog. An error message about "Invalid Command Settings" could be seen (SRFSTUDIO-1868).
- [CC2640R2F] Solved issue with saving custom target configuration. The selected device was reported as incompatible with current device in the Device Control Panel (SRFSTUDIO-1956).
- [CC13xx/CC26xx] Solved issue with packet length in the RF Command API not being synchronized with the value in the Packet TX panel (proprietary PHYs).
When changing packet configuration to fixed packet length and changing the packet length, the packet length in the RF Command API was updated correctly.
Switching to Packet RX and then back to Packet TX, it could be seen that the packet length in the Packet TX panel and the RF Command API
were no longer the same (SRFSTUDIO-1868).
Known issues
- [CC1350] OOK setting does not work on LAUNCHXL-CC1350 targets with PCB version older than 1.3 due to a hardware issue causing unstable output frequency.
- [CC13x2R] The 14 dBm output power in proprietary mode requires CCFG_FORCE_VDDR_HH = 1 in ccfg.c,
which is not supported out-of-the-box in SimpleLink CC13x2 SDK version 1.00.00.
The measured output value using the SDK compared with SmartRF Studio may therefore be a bit lower.
- [CC13x2R] Engineering samples revision A (rev. 1.0) of CC13x2R devices do not work with SmartRF Studio.
This can be seen when starting Packet TX. It will fail with the command status = 0xbad0
- [CC13xx, CC26xx] Unplugging a LaunchPad from the USB bus while SmartRF Studio Packet RX is active causes the Device Control Panel to stop responding (SRFSTUDIO-1716).
- [CC1350] With the 5 kbps SLR setting, the Continuous RX function does not work properly. The problem can be seen from the RSSI plots. At a certain point the RSSI value is always the same (SRFSTUDIO-1456).
- [CC13xx, CC26xx] Code Export: The comments of each register override does not exist if the settings are loaded from a SmartRF Studio configuration file (Menu option: "Open cfg") (SRFSTUDIO-1693).
- [CC13xx, CC26xx] The vertical scroll bar in popup dialogs does not work properly. An attempt to click on the scroll bar makes the dialog to disappear. The workaround is to use the scroll wheel on the mouse. The scroll bar will normally only be seen with scaling other than 100% (SRFSTUDIO-1995)
- [CC13xx, CC26xx] The fixed packet length field is not validated properly. Typing in a large value may cause the Device Control Panel to crash. The workaround is to not input too large values in the length field (SRFSTUDIO-2008).
- [CC2640R2F] Code Export proprietary mode: The exported code is not compatible with the code examples from CC2640R2F SDK v2.40.00. The radio setup command in the code examples is different from the
one exported by SmartRF Studio. The workaround is to modify the CC2640R2F SDK code examples to use the radio setup command exported by SmartRF Studio (EZLINKPROP-501).
- GUI does not scale correctly on Windows 7 machines with screen scaling other than 100%.
Version 2.11.0
Release date: October 5, 2018
New Features and Enhancements
- [CC1352P] The Code Export feature has been updated to support the RF Command structure used for programming of High TX power output (High PA).
Two methods to program the High TX power output are supported, the "normal" method and the "Legacy" method. The "Legacy" method is deprecated and will be removed in the future (SRFSTUDIO-1459).
- [CC13x2R/P] Radio settings (Preview): New settings for the 863-930 MHz band. 200kbps, 2-GFSK, 50 kHz deviation PHY (SRFSTUDIO-1511, SRFSTUDIO-1522).
- [CC13x0] Radio settings : New settings for the 863-930 MHz band. WB-DSSS: Wideband Direct Sequence Spread Spectrum (SRFSTUDIO-1509).
- [CC13x0] Radio settings : New settings for the 430-520 MHz band. OOK, 4.8 kbps (SRFSTUDIO-1799).
- [CC13x0] Code export for CC13x0 devices is no longer compatible with SimpleLink TI-RTOS v2.2x due to a API definition mismatch in command CMD_PROP_RADIO_SETUP. As a consequence, template "default_tirtos_template" has been removed for these devices (SRFSTUDIO-1864).
- [CC2654] Device icon has been removed from the Startup Window because the CC256x Bluetooth Hardware Evaluation Tool is no longer available from TI.com (SRFSTUDIO-1841).
Bug fixes
- [CC13x0] Code export: The PA table is not exported if the modulation is equal "OOK" (SRFSTUDIO-1808).
- [CC13x0] Radio settings : Whitening turned off by default for all OOK settings (SRFSTUDIO-919, SRFSTUDIO-1733).
- [CC13x0] Radio settings : The maximum packet length in RX updated to 255 for all settings where it was not already 255.
- [CC13xx] Fixed issue with sending of packets with fixed packet length. The length field was sent over the air even if fixed packet length was selected (SRFSTUDIO-1873)
Known issues
- [CC1350] OOK setting does not work on LAUNCHXL-CC1350 targets with PCB version older than 1.3 due to a hardware issue causing unstable output frequency.
- GUI does not scale correctly on Windows 7 machines with screen scaling other than 100%.
- [CC13x2R] The 14 dBm output power in proprietary mode requires CCFG_FORCE_VDDR_HH = 1 in ccfg.c,
which is not supported out-of-the-box in SimpleLink CC13x2 SDK version 1.00.00.
The measured output value using the SDK compared with SmartRF Studio may therefore be a bit lower.
- [CC13x2R] Engineering samples revision A (rev. 1.0) of CC13x2R devices do not work with SmartRF Studio.
This can be seen when starting Packet TX. It will fail with the command status = 0xbad0
- [CC13xx, CC26xx] Unplugging a LaunchPad from the USB bus while SmartRF Studio Packet RX is active causes the Device Control Panel to stop responding (SRFSTUDIO-1716).
- [CC1350] With the 5 kbps SLR setting, the Continuous RX function does not work properly. The problem can be seen from the RSSI plots. At a certain point the RSSI value is always the same (SRFSTUDIO-1456).
- [CC13xx/CC26xx] Selecting "Cancel" from the "Open config file" dialog will give an error message about "Invalid Command Settings". The error message can be ignored (SRFSTUDIO-1868).
Version 2.10.0
Release date: July 6, 2018
New Features and Enhancements
- [DRV] Installer includes version 8.0.27.9 of the XDS Emulator SW drivers (SRFSTUDIO-1500).
- [CC13x2R/P, CC26x2R] Radio settings: Added text label with either "(Preview)" or "(Release Candidate)" in description field for all settings that have not been fully characterized.
- [CC13x2R/P] Radio settings (Preview)*: New settings for the 430-520 MHz band. 50kbps, 2-GFSK, 25 kHz deviation PHY (SRFSTUDIO-1398, SRFSTUDIO-1356).
- [CC13x2R/P] Radio settings (Preview)*: New settings for the 430-520 MHz band. SimpleLink Long Range PHY (data rates of 5 kbps, 2.5 kbps) (SRFSTUDIO-1267).
- [CC13x2R/P] Radio settings: Updated settings for the 863-930 MHz band. 50kbps, 2-GFSK, 25 kHz deviation PHY. The settings are in fully characterized state (SRFSTUDIO-1400).
- [CC2640R2F] Radio settings: New settings for 100kbps, 2-GFSK and 250kbps, 2-GFSK (SRFSTUDIO-1362).
- [CC1352R/P] Radio settings: Updated Bluetooth 5 to characterized state (all PHY variants: LE 1M, LE 2M, LE Coded) (SRFSTUDIO-1396, SRFSTUDIO-1402).
- [CC13x0] Radio settings: Updated all CPE patches with improved synthesizer start-up sequence that reduces the probability of synthesizer calibration failure.
- [CC13x0] Radio settings: Added MCE patch for generic FSK ("genfsk") PHY to avoid receive sensitivity degradation in continuous RX operation over long time.
- [CC13x0, CC13x2R/P] Modified packet configuration used for SimpleLink Longe Range Mode PHY to enable data whitening by default.
* The TX power values used for all the settings in the 430-530 MHz band are copied from the 770-930 MHz band and may not be accurate.
Bug fixes
- [CC2640R2F] Device Control Panel status bar now shows the correct silicon revision for CC2640R2F (revision 2.5). Status bar previously showed revision 1.0 (SRFSTUDIO-1479).
- [CC2640R2F, CC13x2R/P, CC26x2R] Fixed issue where the Device Control Panel status bar did not show the reel revision of the device (letter), only the silicon revision (x.y number) (SRFSTUDIO-1480).
- [CC2640R2F, CC13x2R/P, CC26x2R] Fixed issue with default frequency in Packet TX/RX not being the same as the default in Cont. TX/RX (SRFSTUDIO-1498).
- [CC2642R] Fixed issue with Command values in Command view not being updated when the RF Parameter is changed (SRFSTUDIO-1497).
- [CC13xx, CC26xx] Fixed issue with the custom target configuration. The "Apply" button was not enabled when deleting a IO pin from the configuration (SRFSTUDIO-1071).
- [CC13xx, CC26xx] Fixed issue with Code Export where the "extern" definition of the TX Power Table variable was missing in the generated header file (SRFSTUDIO-1473).
- [CC13xx, CC26xx] Code Export: Fixed issue with export of the RX commands. If Code Export was started without the Packet RX tab being activated, the RX command could be generated with "empty" field values. (SRFSTUDIO-1501).
- [CC13xx, CC26xx] Code Export: Fixed issue with the "Type Qualifier" option. The Qualifier was not appended properly to the "Override" type (SRFSTUDIO-1717, SRFSTUDIO-1718).
- [CC1352P] The default value of the "TX Output Power High PA" checkbox will be set depending on the selected Target Board and frequency band (SRFSTUDIO-1331, SRFSTUDIO-1470).
- [CC2640R2F] Radio settings: Increased synth programming timeout for all PHYs from 166 us to 192 us to account for maximum processing time in the beginning of Bluetooth commands (SRFSTUDIO-1504).
- [CC2640R2F] Radio settings: Bluetooth 5, LE Coded PHY: Updated setting for RX AGC reference level for more robust RX performance at lowest temperatures (SRFSTUDIO-1504).
- [CC13x0, CC26x0, CC2640R2F] Radio settings: Updated all CPE patches to align frequency word representation between frequency synthesizer and demodulator. This prevents temporary loss of receive function during continuous receive operation over long time for any "fractFreq" setting used.
- [CC2640R2F] Fixed issue where BLE channel was not saved/loaded correctly in the configuration file of SmartRF Studio (SRFSTUDIO-1454).
- [CC2642R] Fixed issue where SmartRF Studio failed to connect to CC2642R devices (SRFSTUDIO-1475).
- [CC26x2R, CC1352R/P] Fixed issue where wrong command value was used for PA values -12dBm and -15dBm in the 2.4GHz band (SRFSTUDIO-1474).
- [CC31xx, CC32xx] Fixed issue where a "Missing Library Files" error was seen when launching CC31xx/CC32xx Radio Tool from SmartRF Studio (SRFSTUDIO-1484).
- [CC13x0] Fixed issue with link test for "2.5 kbps, SLR" setting. The PER result was not always "0%". The packet interval increased to give target more time to send the packet (SRFSTUDIO-1694).
Known issues
- [CC1350] OOK setting does not work on LAUNCHXL-CC1350 targets with PCB version older than 1.3 due to a hardware issue causing unstable output frequency.
- GUI does not scale correctly on Windows 7 machines with screen scaling other than 100%.
- [CC13x2R] The 14 dBm output power in proprietary mode requires CCFG_FORCE_VDDR_HH = 1 in ccfg.c,
which is not supported out-of-the-box in SimpleLink CC13x2 SDK version 1.00.00.
The measured output value using the SDK compared with SmartRF Studio may therefore be a bit lower.
- [CC13x2R] Engineering samples revision A (rev. 1.0) of CC13x2R devices do not work with SmartRF Studio.
This can be seen when starting Packet TX. It will fail with the command status = 0xbad0
- [CC13xx, CC26xx] Unplugging a LaunchPad from the USB bus while SmartRF Studio Packet RX is active causes the Device Control Panel to stop responding (SRFSTUDIO-1716).
- [CC1350] With the 5 kbps SLR setting, the Continuous RX function does not work properly. The problem can be seen from the RSSI plots. At a certain point the RSSI value is always the same (SRFSTUDIO-1456).
- [DRV] The installation of the required drivers for the XDS Debugger sometimes fails on Windows 10 PCs. When connecting one of the Launchpads with the XDS Debugger, the driver cannot be found. A possible workaround is to install the latest EMU pack: Emulation Software Package (SRFSTUDIO-940).
Version 2.9.0
Release date: April 6, 2018
New Features and Enhancements
- [CC1352P] Added support for CC1352P with High Output power PA (proprietary API, BLE API and IEEE 802.15.4 API).
- [CC26xx, CC13xx] Code Export: Now supports exporting the TX output power table for the selected PA (SRFSTUDIO-625).
- [CC26xx, CC13xx] Code Export: Removed "static" keyword in front of the register overrides variable. Variable declaration has been added to the header file with the "extern" keyword (SRFSTUDIO-1202).
- [CC26x2R, CC13x2R] Packet TX: Sending of packets is now controlled by the target device, resulting in improved throughput (SRFSTUDIO-1083).
- [DCP, STARTW] Built with new tool chain: Visual Studio 2015 Pro + Qt 5.9.2.
- [STARTW] Devices are now listed by family, newest device families are listed first (SRFSTUDIO-1214).
- [CC26x2R] Radio settings: BLE5 updated (all PHY variants: LE 1M, LE 2M, LE Coded) (SRFSTUDIO-1251).
- [CC26x2R, CC1352R, CC2640R2] Radio settings: IEEE 802.15.4 O-QPSK DSSS, 2.4 GHz band updated. This includes faster RF synth calibration (SRFSTUDIO-1247, SRFSTUDIO-1269).
- [CC13x2R] Radio settings: Proprietary 50 kbps, 2-GFSK, 25 kHz deviation for 863-930 MHz band Updated. This includes faster RF synth calibration (SRFSTUDIO-1249).
- [CC13x2R] Radio settings: IEEE 802.15.4g PHY updated (SRFSTUDIO-1249).
- [CC13x2R] Radio settings: SimpleLink Long Range PHY updated (data rates of 5 kbps, 2.5 kbps, and 1.25 kbps). This includes faster RF synth calibration (SRFSTUDIO-1253).
Bug fixes
- [CC13x2R, CC26x2R] Custom Target Configuration: Corrected the definition of available IO pins of the different device packages (SRFSTUDIO-1175).
- [CC26xx, CC13xx] Packet TX panel: Fixed issue when selecting 'text' instead of 'random' payload format that gave a parameter error message. (SRFSTUDIO-1220).
- [CC1310] Corrected an issue where wrong output power values were shown for 433 MHz band. This has now been corrected and aligned with the CC1350 device (SRFSTUDIO-1200).
- [CC26xx, CC13xx] Fixed issue when loading config file. After loading a config file, starting Packet TX or Packet RX would show execution of RF Commands that were not relevant. (SRFSTUDIO-1226).
Known issues
- [CC1350] OOK setting does not work on LAUNCHXL-CC1350 targets with PCB version older than 1.3 due to a hardware issue causing unstable output frequency.
- GUI does not scale correctly on Windows 7 machines with screen scaling other than 100%.
- [CC13x2R] The 14 dBm output power in proprietary mode requires CCFG_FORCE_VDDR_HH = 1 in ccfg.c,
which is not supported out-of-the-box in SimpleLink CC13x2 SDK version 1.00.00.
The measured output value using the SDK compared with SmartRF Studio may therefore be a bit lower.
- [CC13x2R] Engineering samples revision A (rev. 1.0) of CC13x2R devices do not work with SmartRF Studio.
This can be seen when starting Packet TX. It will fail with the command status = 0xbad0
Version 2.8.0
Release date: December 20, 2017
New Features and Enhancements
- [CC13xx, CC26xx] The RF Command used to stop the radio when ending a test function is now shown in the command view panel (SRFSTUDIO-494).
- [CC13x2R] Radio CPE patch name aligned with SimpleLink SDKs using Core SDK 3.40.00. Patch renamed to rf_patch_cpe_prop (SRFSTUDIO-1070).
- [CC13xx, CC26xx] Added support for tuning internal capacitor array for easy calibration of external crystal oscillators (SRFSTUDIO-46).
- [CC13xx] New settings in proprietary mode to support the IEEE 802.15.4g specification (SRFSTUDIO-1040).
Bug fixes
- [CC13xx] Fixed issue with Packet RX when enabling address filtering. Packets with wrong address were not "flushed" even if
the flag rxConfig.bAutoFlushIgnored was set (SRFSTUDIO-906).
- [CC13xx, CC26xx] Fixed issue with frequency not being set correctly when running "frequency sweep" in Cont. TX (SRFSTUDIO-629).
- [CC13x2R] The RX bandwidth values updated to improve RX performance (SRFSTUDIO-1072, SRSTUDIO-1077).
- [CC13x2R, CC26x2R] Updated all Bluetooth 5 settings (all PHY variants: LE 1Mbps, LE 2Mbps, LE Coded 125kbps, LE Coded 500kbps) with improved RF synthesizer settings
for faster calibration and reduced pilot tone length (SRFSTUDIO-1061)
- [CC13x2R, CC26x2R] Updated all radio settings with new DC/DC regulator settings for stable performance.
- [CC13xx] Implemented workaround (for the Sub-1 GHz band) to solve errata issue where radio stops responding for a period after a long time in RX (SRFSTUDIO-1056).
- [DCP] Fixed issue with the Bit Error Rate (BER) calculation in Packet RX when fixed packet length is used. The number of bytes used for calculation was incorrect giving a too low BER (SRFSTUDIO-1055).
Known issues
- [CC1350] OOK setting does not work on LAUNCHXL-CC1350 targets with PCB version older than 1.3 due to a hardware issue causing unstable output frequency.
- GUI does not scale correctly on Windows 7 machines with screen scaling other than 100%.
- [CC13x2R] The 14 dBm output power in proprietary mode requires CCFG_FORCE_VDDR_HH = 1 in ccfg.c,
which is not supported out-of-the-box in SimpleLink CC13x2 SDK version 1.00.00.
The measured output value using the SDK compared with SmartRF Studio may therefore be a bit lower.
Version 2.7.0
Release date: October 5, 2017
New Features and Enhancements
- [CC13x0] New settings for CC13xx 4.8 kbps 2-GFSK 868MHz (SRFSTUDIO-769).
- [CC1352, CC2652R] Added support for IEEE 802.15.4-2006 PHY (SRFSTUDIO-870, SRFSTUDIO-961).
- [CC1352, CC26x2R] Added support for BLE PHY (SRFSTUDIO-848, SRFSTUDIO-851).
- [CC1352] Added support for SimpleLink Long Range settings (SRFSTUDIO-855, SRFSTUDIO-856).
- [CC13xx] Default fixed packet length is set to be the same in packet RX and packet TX (SRFSTUDIO-281).
- [CC13xx] Calculation of the symbol rate used in the command API changed. The "prescaler" value is fixed and the "rateWord" is set
to find the best match for the given Symbol Rate. (SRFSTUDIO-484).
- [DCP] Added length byte to the displayed packets in packet RX for variable length mode (SRFSTUDIO-2).
- [CC13xx, CC26xx] Added possibility to select settings with the Space or Return keys (SRFSTUDIO-869).
- [CC2640R2] New setting to send Bluetooth 4.x compatible packets ("ADV_NONCONN_IND" PDU) (SRFSTUDIO-847).
- [CC1350] Added more output power values for LAUNCHXL-CC1350-4 in the 433 MHz band (SRFSTUDIO-971).
Bug fixes
- [DCP, STARTW] Fixed several layout issues when having screen scaling other than 100% on Windows 7 machines.
- [DCP] Fixed issue where "parameter out of range" error was shown at wrong time (SRFSTUDIO-448).
- [STARTW] Fixed issue where no emulators were shown if XDS200 enumeration failed (SRFSTUDIO-805).
- [CC2540] Fixed issue with selecting frequency after register reset (SRFSTUDIO-799).
- [MSP-FET] Fixed issue where SmartRF Studio blocked access to the MSP430 debugger (SRFSTUDIO-781).
- [STARTW] Startup Window default size is changed to avoid unnecessary scrolling, and device icons are now listed in 6 columns (SRFSTUDIO-867).
- [CC110L, CC113L, CC115L] Fixed issue where some register values were given in decimal value instead of hexadecimal (SRFSTUDIO-875).
- [CC2640R2F] Fixed issue when sending packets with channels 37, 38 and 39 using the command CMD_BLE5_ADV_AUX (SRFSTUDIO-885).
- [CC1310] Fixed issue with detection of the "US" variant of the LaunchPad "LAUNCHXL-CC1310-CC1190" (SRFSTUDIO-918).
- [CC1350] Fixed issue in BLE mode where there was a mismatch in the sent/received PDU header when including sequence numbers (SRFSTUDIO-873).
Known issues
- [CC1350] OOK setting does not work on LAUNCHXL-CC1350 targets with PCB version older than 1.3 due to a hardware issue causing unstable output frequency.
- GUI does not scale correctly on Windows 7 machines with screen scaling other than 100%.
- [CC13x2R] The 14 dBm output power in proprietary mode requires CCFG_FORCE_VDDR_HH = 1 in ccfg.c,
which is not supported out-of-the-box in SimpleLink CC13x2 SDK version 1.00.00.
The measured output value using the SDK compared with SmartRF Studio may therefore be a bit lower.
Version 2.6.1
Release date: July 19, 2017
New Features and Enhancements
- [CC13xx, CC26xx] Added support for new SDK include format in Code Export (SRFSTUDIO-871).
Bug fixes
- [CC1350 BLE] Fixed issue when trying to change access address (SRFSTUDIO-859).
- [CC13xx, CC26xx] Fixed issue when using the start/stop buttons on the toolbar.
The Device Control panel could crash if switching between the two too quickly (SRFSTUDIO-909).
Version 2.6.0
Release date: March 10, 2017
New Features and Enhancements
- [DCP] Added a toolbar with possibility to start/stop test functions and show/hide panels (SRFSTUDIO-795).
- [DCP] Fixed several layout issues when having screen scaling other than 100% on Windows 7 machines.
- [CC13xx, CC26xx] Configuration of I/O signals from the HW Configuration panel updated to use register settings given in xml file (SRFSTUDIO-608).
- [CC13xx, CC26xx] Packet RX performance is improved. Packets can be received at faster rate without buffer overflows (SRFSTUDIO-756).
- [CC13xx, CC26xx] New settings for SimpleLink Long Range(SLR)mode (SRFSTUDIO-682).
- [CC13xx, CC26xx] New settings for CC13xx 500 kbps 2-GFSK 868MHz (SRFSTUDIO-759).
- [CC13xx, CC26xx] New settings for CC13xx 400 kbps 2-GFSK 868MHz (SRFSTUDIO-791).
- [CC13xx, CC26xx] New settings for CC13xx 300 kbps 2-GFSK 868MHz (SRFSTUDIO-792).
- [CC13xx, CC26xx] New settings for CC13xx 200 kbps 2-GFSK 868MHz (SRFSTUDIO-793).
- [CC13xx, CC26xx] New settings for CC13xx 10 kbps 2-GFSK 868MHz (SRFSTUDIO-770).
- [CC13xx, CC26xx] New settings for CC13xx 4.8 kbps OOK 868MHz (SRFSTUDIO-490, 801).
- [CC13xx, CC26xx] New settings for BT5 1Mbps (SRFSTUDIO-775).
- [CC13xx, CC26xx] New settings for BT5 2Mbps (SRFSTUDIO-441).
- [CC13xx, CC26xx] New settings for BT5 125kbps (SRFSTUDIO-778).
- [CC13xx, CC26xx] New settings for BT5 500kbps (SRFSTUDIO-441).
- [CC13xx, CC26xx] The exported RF Commands in Cont. TX/RX will now by default be the same as used by SmartRF Studio.
Previously the default was to always export the Packet TX/RX commands (SRFSTUDIO-358).
- [CC13xx] Improved feedback on dependencies between RX Filter BW, Symbol Rate and Frequency (SRFSTUDIO-165)
- [CC13xx, CC26xx] The optional serial number shown in Packet TX/RX for BLE devices has been changed from being part of the
Adv. Address to the first two bytes of the Adv. Data (SRFSTUDIO-546).
- [CC13xx, CC26xx] Added command descriptions in Command View and in generated source code (SRFSTUDIO-305)
- [CC13xx] Added support for 255 byte packets in fixed length mode (SRFSTUDIO-52).
Bug fixes
- [CC13xx, CC26xx] Fixed issue with wrong option for the I/O signal in the HW Configuration Panel (SRFSTUDIO-754).
- [CC13xx] Fixed issue when sending packets with fixed length (SRFSTUDIO-810).
Known issues
- [CC1350] OOK setting does not work on LAUNCHXL-CC1350 targets with PCB version older than 1.3 due to a hardware issue causing unstable output frequency.
- GUI does not scale correctly on Windows 7 machines with screen scaling other than 100%.
Version 2.5.1
Release date: January 17, 2017
New Features and Enhancements
- [CC2640R2F] Added support for WCSP Package (DSBGA 2.7x2.7) (SRFSTUDIO-693).
- [CC13xx, CC26xx] Added documentation of Serial Mode Output on CC13xx LaunchPad (SRFSTUDIO-748).
Bug fixes
- [CC13xx, CC26xx] Fixed problem with save/load configuration data where Address parameter in Packet TX was not saved (SRFSTUDIO-733).
- [CC13xx, CC26xx] Fixed problem where loading configuration data multiple times could cause SmartRF Studio to crash (SRFSTUDIO-748).
- [CC13xx, CC26xx] Fixed problem where resetting configuration data could cause SmartRF Studio to crash (SRFSTUDIO-722).
Known issues
- GUI does not scale correctly on Windows 7 machines with screen scaling other than 100%.
Version 2.5.0
Release date: December 2, 2016
New Features and Enhancements
- [CC2640R2F] Added support for device CC2640R2F (SRFSTUDIO-626).
- [CC13xx, CC26xx] Tooltip given for each of the items that can be selected from the "Target board" drop down list (SRFSTUDIO-146).
- [CC13xx, CC26xx] Code export now supports the format for the "SimpleLink SDK" format (SRFSTUDIO-680).
- [CC2538] Added Support for CC2538 by the Perl script module (SRFSTUDIO-253).
- [CC1310] Support added for Launchpad with the CC1310 combined with the front end CC1190 (SRFSTUDIO-677).
- [CC13xx, CC26xx] Default file name on Code Export is changed to smartrf_settings.h/c (SRFSTUDIO-482).
Bug fixes
- [STARTW] Fixed issue with starting SmartRF Flash Programmer 2 from SRF Studio when specifying installation path (SRFSTUDIO-591).
- [SCRIPT] Fixed issue with the 'dal_test' script (SRFSTUDIO-683).
- [CC26xx] Fixed issue with code export files seen using the GCC compiler (SRFSTUDIO-668).
- [CC112x, CC120x] Fixed issue with warning given when changing to easy mode from "RX Sniff mode" (SRFSTUDIO-660, SRFSTUDIO-661).
- [STARTW, DCP] Fixed scaling issue seen on Windows 10 machines with screen scaling other than 100%. (SRFSTUDIO-696).
- [CC13xx] Fixed issue with missing preamble length option (SRFSTUDIO-700).
- [CC13xx] Fixed issue with startup of the Device Control Panel after FW update of XDS110 (SRFSTUDIO-597).
- [CC1350] Fixed incorrect PA setting value for 0dBm in the 2.4GHz band (SRFSTUDIO-697).
Known issues
- GUI does not scale correctly on Windows 7 machines with screen scaling other than 100%.
Version 2.4.3
Release date: September 2, 2016
New Features and Enhancements
- [CC1350] Added characterized 2GFSK 50 kbps settings for the 431 - 527 MHz frequency range (SRFSTUDIO-501).
- [CC1350] Added characterized Long Range Mode 625 bps settings for the 431 - 527 MHz frequency range (SRFSTUDIO-616).
Bug fixes
- [CC1350] Fixed issue where some Whitening options were missing in the Device Control Panel (SRFSTUDIO-633).
- [CC13xx] Removed invalid options from Preamble Count and Sync Word Length drop-downs (SRFSTUDIO-634).
- [CC13xx] Fixed issue where max output power for custom targets was too low in 868 MHz band (SRFSTUDIO-642).
- [STARTW] Fixed issue where connecting to XDS emulators sometimes failed (SRFSTUDIO-563).
Version 2.4.2
Release date: June 25, 2016
Important Notice
Studio 2.4.2 code export is only compatible with TI-RTOS 2.18.00 or later.
Bug fixes
- [CC13xx] Updated GENFSK RFE patch with improved internal PA ramping (SRFSTUDIO-621).
- [CC13xx] Fixed issue in Code Export where overrides were sometimes duplicated (SRFSTUDIO-586).
- [CC13xx] Fixed issue in Code Export where override comments were missing for device revision 2.0 (SRFSTUDIO-622).
Version 2.4.1
Release date: June 17, 2016
Important Notice
Studio 2.4.1 code export is only compatible with TI-RTOS 2.18.00 or later.
Bug fixes
- [CC26xx] Fixed issue where CC2640/30/20 radio configuration did not work correctly (SRFSTUDIO-613).
Version 2.4.0
Release date: June 16, 2016
Important Notice
Studio 2.4.0 code export is only compatible with TI-RTOS 2.18.00 or later.
New Features and Enhancements
- [CC13xx, CC26xx] Added new Target Configuration dialog with options to configure Custom I/O signals and Output Power values (SRFSTUDIO-29).
- [CC1350] Added support for CC1350 BLE mode (SRFSTUDIO-469).
- [CC1350] Added Code Export support for CC1350 BLE mode (SRFSTUDIO-342).
- [CC26xx] Added Code Export support for CC2640 and CC2650 BLE mode (SRFSTUDIO-549).
- [CC26xx] Added support for writing non-standard frequency values in parameter panel.
- [CC13xx] Improved GUI design for Code Export dialog (SRFSTUDIO-493).
- [CC13xx, CC26xx] Reduced minimum size of Code Export dialog to improve user experience on smaller screens (SRFSTUDIO-493).
- [CC13xx] SmartRF Studio build number is now included in Code Export (SRFSTUDIO-371).
- [CC13xx] Added more whitening options to RF parameter panel.
- [CC430] Interface library for MSP-FET debugger updated (msp430.dll version 3.7.1.0) (SRFPROG-213).
- [DRV] Installer includes version 6.0.228.0 of the XDS Emulator SW drivers (SRFPROG-223).
Bug fixes
- [CC13xx, CC26xx] RF parameter combo boxes now display "Unknown" if command field value is not recognized (SRFSTUDIO-246).
- [CC2564] Fixed issue with downloading required application at startup (SRFSTUDIO-412).
- [CC13xx] Fixed issue where legal override value was shown as illegal in override editor (SRFSTUDIO-505).
- [CC112x] Fixed issue with random order of fields in the parameter summary for register export (SRFSTUDIO-461).
- [CC13xx] Fixed issue with inconsistent use of capital letters in hex values in Command View and Code Export (SRFSTUDIO-495).
Version 2.3.1
Release date: January 29, 2016
New Features and Enhancements
- Added indication of FW update required for XDS110 emulator in Startup Window (SRFSTUDIO-408).
Bug fixes
- [CC1101-CC1190] Fixed a problem where selected EM revisions were not displayed in dropdown list (SRFSTUDIO-315).
- [CC13xx] Fixed an issue where the symbol rate command value changed slightly when switching between test modes (SRFSTUDIO-401).
- [CC2541-CC2590] Fixed issue where high gain mode pin for CC2590 was not set correctly (SRFSTUDIO-316).
- [CC2541-CC2590] Corrected RSSI offset values for CC2541 used with CC2590 range extender (SRFSTUDIO-316).
Version 2.3.0
Release date: December 16, 2015
New Features and Enhancements
- [CC13xx] The directory used for code export is remembered between sessions.
- [CC26xx/CC13xx] Improved target selection panel in Device Control Panel.
- [CC13xx] Code export header file include guard is set according to file name.
- [CC13xx] Added prompt to save template when code export panel is closed.
- [CC13xx/CC26xx] Added help button for target selection panel.
- [CC26xx] Added support for CC2650 LaunchPad.
- [CC13xx] Added support for OOK setting.
- [CC13xx] Updated GFSK and LRM radio settings.
- [CC13xx] Added override editor feature.
- Added automatic firmware update feature for XDS110 emulator.
Bug fixes
- [CC13xx] Fixed a problem with wrong endianness of sync word less than 32 bits in Packet TX.
- [CC13xx] Fixed a problem with incorrect handling of address configuration in Packet RX.
- [CC1120] Fixed a problem with closing the Device Control during Packet RX.
- [CC26xx] Fixed a problem with frequency sweep feature in Continuous TX.
- [CC2640/CC2650 BLE] Fixed a problem where length field in PDU header incorrectly displayed in decimal format.
- [CC2630/CC2650 IEEE 15.4] Fixed a problem where packets were lost after the 256th packet.
- [CC26xx] Fixed a problem where TX power was incorrect after target selection was changed.
- Fixed a problem where the installer did not install XDS110 emulator drivers.
- Fixed a problem where loading Studio config file resulted in wrong RF_Mode struct in Code Export.
Version 2.2.1
Release date: September 28, 2015
New Features and Enhancements
- [CC13xx] Improved calculation of frequency divider settings.
- [CC13xx] Improved handling of template files in code export.
- [CC13xx] Updated radio settings.
- [CC13xx] The format of code generated by Code Export is updated to match TI-RTOS version 2.14.02.
- [CC13xx] Added information section in Code Export about code change required for TX power values.
Bug fixes
- [CC254x] Fixed issue with Continuous RX/TX in Perl scripts.
- [CC13xx] Fixed issue with serial mode in Continuous RX.
- [CC13xx] Fixed issue with loading configuration file in DC panel.
- [DCP] Fixed issue with DC panel crash if closed after device is disconnected.
- [CC13xx] Fixed issue with incorrect code color in Code Export.
- [CC1200] Removed duplicated whitening checkbox when in 802.15.4g mode.
Known Issues
- [CC13xx] Address configuration in Packet RX does not take effect.
Version 2.2.0
Release date: August 24, 2015
Important Notice
This version of SmartRF Studio is based on a pre-release version of software for the CC1310,
and ‘Code Export’ output should not be used in production versions of CC1310 software.
The CC1310 production release software is in its final stages of development and verification,
and it should be expected that radio-specific timings and parameters will change in that release.
This notice does not apply to the CC2620/30/40/50.
New Features and Enhancements
- A New SW library to do testing of the CC26xx and CC13xx devices.
- [STARTW] The connected "XDS" devices will be auto detected when changes on the USB port is detected.
- [STARTW] The "Tools menu" has been updated with more entries: SmartRF Flash Programmer 2, SmartRF Packet Sniffer and SmartRF Test environment.
- [CC26xx/CC13xx] The packet throughput in Packet TX/RX has been improved.
- [CC13xx] The Code Export has been improved:
- The exported settings are compatible with TI-RTOS code examples for CC13xx.
- Custom selections in the Code Export View will be kept when closed and opened again.
- [CC13xx] New settings for 868MHz Long Range Mode.
- [CC13xx] Radio settings for CC13xx are updated
- [CC26xx/CC13xx] The PER test and Range test FW included. This can be found under ../Texas Instruments/SmartRF Tools/firmware/EMK
Bug fixes
- [STARTW] Enumeration of "XDS" devices failed when a MSP-FET debugger was connected.
- [DCP] Copy text from the register description could lead to an application crash.
- [CC26xx] The Modulated signal in Cont. TX was not correct
- [CC13xx] The Unmodulated signal in Cont. TX was not correct
- [CC13xx] The use of Non-default packet interval in Packet TX did not have any effect.
- [CC13xx] Preamble in Packet TX was not updated when preamble configuration was changed.
- [CC12xx] Error message changed to a warning when attempting to use "no sync word".
- [CC26xx] When using XDS110 and default packet interval packets were lost.
Known Issues
Version 2.1.0
Release date: May 13, 2015
New Features and Enhancements
- Added support for new devices: CC1350 Rev A
- Added support for XDS110 emulator for CC26xx/CC13xx
- XML configuration redesigned for the CC26xx/CC13xx devices
- [CC13xx]Added support for these HW boards:
- CC13xxEM-7XD-4251
- CC1310EM-7PA-4751
- CC13xxEM-SKY66115-4751
- Added parameter summary to code export
- Added GUI control for DC/DC enable and disable
- Added support for IO handling for TX/RX/Idle states from XML files.
Bug fixes
- [CC2538] Range extender combo box was disabled
- [CC2620] Startup of DC panel for CC2620 failed
- [CC26xx/Cc13xx] Parameters set by user were reset when test function changed.
- [CC2640/CC2540] Packet TX/Packet RX did now work between CC2540 and CC2640 when whitening enabled.
- [CC120x] Length for 15.4g mode packets was not correctly calculated.
- [CC26xx/CC13xx] Show/hide RF parameters did not work for CC26xx/CC13xx.
- [CC26xx/CC13xx] Missing checkbox for show/hide command view.
- [CC112x] Sniff mode setting was not calculated correctly after load config.
- [CC13xx] Config data save gave error message.
Known Issues
- [CC1310] Flash must be erased on CC1310 early sample revisions (Rev 1.0) before using SmartRF Studio
- [CC13xx/CC26xx] The default packet interval is too low when XDS110 is in use. The packet interval must be set higher to avoid packet loss.
- See known issues for previous release
Version 2.0.0
Release date: February 25, 2015
New Features and Enhancements
- Added support for new devices: CC2650, CC2640, CC2630, CC2620 and CC1310
- Added support for XDS200 for CC26xx/CC13xx
- Code Export feature for CC1310
Bug fixes
- [CC1125] Fixed a bug where RSSI value locked in Continuous RX
Known Issues
- [CC1310] Flash must be erased on CC1310 before using SmartRF Studio
- See known issues for previous release
Version 1.18.0
Release date: December 19, 2014
New Features and Enhancements
- [CC3100/CC3200] Support for CC3100 and CC3200.
- [CC2538] The device revision will be displayed.
- [CC2541] More output power values. Aligned with Data Sheet.
- [CC1101/CC1120/CC1200] New easy mode settings. Settings that will make link testing between the different device types easier.
- [CC430] Interface library for MSP-FET debugger updated (msp430.dll version 3.4.3.4)
- [CC2530-CC2592] Output Power settings added.
Bug fixes
- [CC120x] Maximum packet length for non 802.15.4g mode increased to 253. The limitations are due to EB FW.
- [CC430] Read/write of non RF registers (16 bits).
- [CC430] Use of new MSP-FET (Black box). Update of FW from the initial FW version did not work.
- [CC430/CC11xx/CC112x/CC120x] Packet RX more robust. Crash after receiving packets over a longer period.
- [CC11xL] The modulation format OOK was previously removed by a mistake.
Known Issues
- Same as previous release.
Version 1.16.1
Release date: July 29, 2014
New Features and Enhancements
- [CC1121] Support for range extender CC1190 added.
- [CC2541] Support for range extender CC2592 added.
- [CC2530] Support for range extender CC2592 added.
- [CC120x] Default preamble and sync word changed when 802.15.4 mode and FEC selected.
- [CC120x, CC112x] Frequency values outside the ranges given in data sheet allowed. Warning given.
- [CC2541] Max number of payload bytes in SmartRF Studio set to 128 - length(1) - status(2) --> 125 bytes.
- [CC430] Latest driver (msp430.dll) version of the MSP-FET430UIF interface: "3.4.1.0".
- [CC112x] The typical settings for chip rev. 2.3 will now use automatic calibration.
- [DCP] Calculation of BER result in packet RX improved. Now taking into account all bytes sent over the air.
Bug fixes
- [CC120x] 802.15.4 mode turned off in Cont. TX.
- [CC120x] Inconsistent settings for "50kbps/ARIB standard". Register FS_DIG0 in Cont. TX/Packet TX both set to 0x55.
- [CC120x] Default sync word when selecting 802.15.4g mode and FEC.
- [CC2530] Not able to change the IO Port registers P0 and P1 from register view.
- [CC254x] The maximum packet length was limited by the typical settings to 64 bytes.
- [CC2541] Inconsistent settings for the carrier frequency. Now defaults to 2420 MHz.
- [CC112x] Wrong parsing of packet in RX Sniff mode.
- [CC430] Packet interval set in Packet TX did not have any effect.
- [DCP] Wrong parsing of packet in easy mode.
- [FW] FW for SmartRF05EB, TrxEB and CC Debugger updated (44). Packet handler for CC2520 improved to fix problem with missing "ACKs".
- [DOC] The help document could not be opened from the window startup menu.
Known Issues
- [CC120x] When selecting the 802.15.4g option it is also required to change the "Sync word length" configuration on the transmitter.
"16D bits (DualSync search)" should be selected.
- [CC120x] Forward Error Correction (FEC) in 802.15.4g mode is currently not supported for packet greater than 120 bytes.
- [CC2541-CC2592] Output power settings have not been defined.
- [CC2530-CC2592] Output power settings have not been defined.
Version 1.16.0
Release date: February 26, 2014
New Features and Enhancements
- [CC2538] Support for range extender CC2592 added.
- [CC120x] Support for range extender CC1190 added.
- [DCP] Definition of payload aligned with documentation of application examples.
- [STARTW] The enumeration of "XDS" devices has been improved.
- [STARTW] The USB drivers for TrxEB, SmartRF05EB and CC Debugger have been signed.
- [CC254x] For BLE devices an input field for Device address has been added.
- [FW] New EB FW with protection for device ID "0000". A random number will be generated.
- [SCRIPT] Support for Perl 5.16 ActiveState.
Bug fixes
- [STARTW] Start in off-line mode from context menu on device icon.
- [DOC] Open of Help document from the Startup Menu.
- [CC254x] Max packet length in proprietary mode.
- [CC254x] Content of drop down box to select sync word length.
- [CC11xL] Output power settings for Value line devices.
Known Issues
- Same as previous release.
Version 1.15.0
Release date: December 20, 2013
New Features and Enhancements
- [CC3000] CC3000 added to the list of 2.4GHz devices.
- [CC2564] CC2564 added to the list of 2.4GHz devices.
Bug fixes
- [STARTW] Enumeration of XDS devices made more robust.
- [DOC] Open of Help document from the Startup Menu.
Known Issues
- Same as previous release.
Version 1.14.2.1
Release date: December 6, 2013
New Features and Enhancements
- [CC120x] Parameter to select Low Power Mode added.
- [CC120x] "PA shaping" enabled by default for the "1.2kbps" settings.
Bug fixes
- [CC120x] RSSI Offset when selecting range extender: "SKY65313_915MHz".
- [CC2541] Carrier frequency changed when selecting unmodulated signal and then back to modulated again.
- [SCRIPTS] Problem with wrong name of environment variable.
Known Issues
- Same as previous release.
Version 1.14.2.0
Release date: November 21, 2013
New Features and Enhancements
- [CC112x, CC120x] Calculations of sleep and RX time for RX Sniff mode improved. The algorithms have
been lined up with Design Note DN511
- [CC120x] Added new settings for data rate 130kbps and 150kbps. Both settings with 4GFSK modulation.
- [STARTW] The context menu (right click on device icon) has been updated with more links to online documents.
Bug fixes
- [CC120x] Calculation of ASK_CFG.ASK_DEPTH.
- [CC120x] "ARIB" Settings updated.
- [CC110X] Register TEST0 not updated when channel spacing and channel number updated.
- [CC2541] Programming of MDMTEST1.TX_TONE in Cont. TX when unmodulated signal selected.
- [DCP] Selecting TX output Power when range extender used could in some cases crash.
- [CC110x, CC11xL, CC111x] Phase transition time when selecting MSK modulation.
Known Issues
- Same as previous release.
Version 1.14.1
Release date: October 3, 2013
Bug fixes
- [DCP] Wrong packet format in Packet RX for all SoCs and CC2520.
- [CC1101] Calculation of Deviation and RX BW when changing the Crystal frequency.
- [CC1101] CRC error on last packet when Packet TX stopped.
Known Issues
- Same as previous release.
Version 1.14.0
Release date: September 3, 2013
New Features and Enhancements
- [CC1201] Added support for CC1201
- [CC120x] Added support for long packets in 802.15.4g mode.
Bug fixes
- [CC120x] Calculation of RX BW for CC120x updated to take into account a rule for register AGC_REF.
- [CC120x] Valid crystal frequency changed to 38.4 - 40 MHz.
- [CC120x] Wrong name of subfield of register SYNC_CFG0 when error message about invalid RX BW.
- [CC120x] Register setting for Transparent serial mode in Continuous RX. MDMCFG0.TRANSPARENT_MODE_EN was not set correctly.
- [STARTW] Check for updates failed due to changes in text on web page.
Known Issues
- [CC120x] When selecting the 802.15.4g option it is also required to change the "Sync word length" configuration on the transmitter.
"16D bits (DualSync search)" should be selected.
- [CC120x] Forward Error Correction (FEC) in 802.15.4g mode is currently not supported for packet greater than 120 bytes.
Version 1.13.0
Release date: July 4, 2013
New Features and Enhancements
- [CC1200] New feature to support Advanced RF parameters.
- [CC1200] RX Sniff mode added.
- [CC1200] Typical settings updated according latest data from characterization.
- [CC112x] RX Sniff mode updated to be in line with Design Note DN511.
Bug Fixes
- [CC1200] Changing of Data Format in Continuous RX mode.
Known Issues
- [CC1200] When selecting the 802.15.4g option it is also required to change the "Sync word length" configuration on the transmitter.
"16D bits (DualSync search)" should be selected.
- [CC1200] Max packet length is 255 bytes.
- [CC1200] Forward Error Correction (FEC) in 802.15.4g mode is currently not supported for packet greater than 120 bytes.
Version 1.12.0
Release date: May 2, 2013
New Features and Enhancements
- [CC1200] Support for new device.
- [CC1125] New group of typical settings for "ETSI CAT1" regulations.
- [CC112x] Register names changed: DRATEx -> SYMBOL_RATEx, SOFT_TX_DATA_CFG -> CFM_DATA_CFG,
SOFT_TX_DATA_IN -> CFM_TX_DATA_IN, SOFT_RX_DATA_OUT -> CFM_RX_DATA_OUT.
Bug Fixes
- [CC2538] Register export of 32 bits registers.
- [CC2538] Easy mode in Off-line mode and startup of Device Control Panel on a PC where
SmartRF Studio was installed for the first time (No entries in windows registry).
- [CC1120] Whitening and Manchester parameter changed when switching between Packet TX and Packet RX.
Known Issues
- [CC1200] When selecting the 802.15.4g option it is also required to change the "Sync word length" configuration on the transmitter.
"16D bits (DualSync search)" should be selected.
- [CC1200] Max packet length is 255 bytes.
- [CC1200] Forward Error Correction (FEC) in 802.15.4g mode is currently not supported for packet greater than 120 bytes.
Version 1.11.0
Release date: April 18, 2013
New Features and Enhancements
- [CC2538] Support for new device.
- [CC1120] Support of CC1120-SKY65313 (915 MHz).
Bug Fixes
- [CC1125] Allowed crystal frequency range changed to 32 MHz - 44 MHz.
- [DCP] Problem with loading of config file if crystal value outside the recommended range.
Known Issues
- [CC2538] Register export only writes 16 bits of the 32 bits register addresses
Version 1.10.3
Release date: November 6, 2012
New Features and Enhancements
- [CC1125] Allowed crystal frequency changed to the range 32 MHz to 44 MHz.
Bug Fixes
- [DCP] Parameter fields in Packet TX/RX advanced panel missing and wrong alignment.
Known Issues
Version 1.10.2
Release date: October 12, 2012
New Features and Enhancements
- [CC430] Support for CC430F6147 added.
Bug Fixes
- [CC112x] GPIO port signals in Cont. TX/RX.
- [CC112x-SKY65367-11] Name front end changed from "SKYWORKS" to "SKY65367-11 and output power values have been updated.
- [CC112x] Dependencies of modulation format when calculating the FS_CHP register removed.
- [CC1101] Problem with selection of crystal frequencies.
- [SCRIPT] Installed on user folder to solve problem with access rights. Documentation updated.
- [DCP] Problem with handling of Payload size in Packet TX.
Known Issues
Version 1.10.0
Release date: July 11, 2012
New Features and Enhancements
- [CC1101-CC1190] Support for CC1101-CC1190 on TrxEB.
- [CC1120-CC1190] Support for combo board CC1120-CC1190 on TrxEB.
- [CC112x-SKYWORKS] Support for combo board CC1120-SKYWORKS on TrxEB.
- [CC2531] Support for CC2531-CC2591.
- [CC112x] New advanced parameter to handle bit oriented packet length.
- [DCP] The maximum limit for packet interval has been increased to 99999 ms.
- [CC254x] Several SFR registers added to The Register view.
- [CC2530] Enabled range extender with CC Debugger.
Bug Fixes
- [DCP] Strobe commands for "power down" in command panel not working. The RF device goes
more or less directly back to IDLE state.
- [CC1101] Calculation of Deviation and RX BW parameter when changing the crystal parameter wrong.
- [CC112x] Calculation of average current consumption for RX Sniff mode updated.
- [CC1101] Crash on startup of Device Control Panel when using SmartRF04EB + CC1101EM.
Known Issues
- [CC112x-SKYWORKS] The output power value displayed in the RF Parameter panel is the power level out of CC112x.
It does not show the real value out of the SKYWORKS front end.
The RSSI offset value used to calculate the RSSI value is the same as the offset value
used for a standalone CC112x EM. This probably have to be adjusted in the future to get the
correct RSSI value displayed in Packet RX and Cont. RX
Version 1.9.1
Release date: May 7, 2012
New Features and Enhancements
- [CC2545] Support for CC2545.
- [CC1125] The rules used to apply "Charge pump" modification after calibration has been changed.
Dependencies of data rate and RX BW removed.
- [CC11xx] Handling of fixed packet length when using TrxEB added.
- [CC112x] Added parameter for Performance mode.
- [CC430] The MSP430.dll updated to version 3.2.3.15
Bug Fixes
- [CC2543, CC2544] Cont. TX/RX not working after typical setting selected.
- [CC2543, CC2544] The RSSI offset value has been modified.
- [CC254x] The frequency parameter was not recalculated when changing the IF frequency.
- [CC11xx] Loading of configuration file gave an error message about invalid frequency.
- [CC112x] ASK depth only set when ASK/OOK modulation format selected.
- [CC115L] Error message about "Sync word length" when selecting a typical or easy mode setting.
Known Issues
Version 1.8.0
Release date: March 27, 2012
New Features and Enhancements
- [CC1125] Support for CC1125.
- [CC2543] Support for CC2543.
- [CC2544] Support for CC2544.
Bug Fixes
- [CC2541] 2 bytes missing in the packet view of Packet RX if status bytes not inserted in FIFO by the chip.
- [DCP] RSSI plot in Cont. RX did not work properly after about 9 - 10 minutes of RSSI measurements.
- [CC110x, CC111x, CC11xL, CC2500, CC251x] Problem with update of registers that will be written when starting
a test function (click on start button). E.g. Packet TX/RX. These are registers that need to be refreshed
each time the function is started because the chip will do updates when strobe commands have been executed.
(E.g. FSCALx)
Known Issues
Version 1.7.2
Release date: February 21, 2012
Bug Fixes
- [CC254x] Register settings not restored after being in Cont. TX. As a result Packet TX/RX did not work.
- [CC254x] The carrier frequency was 1 MHz off in Cont. TX.
- [CC112x] Calculation of Deviation registers not correct when exponent equal zero.
Version 1.7.1
Release date: January 11, 2012
Bug Fixes
- [CC1101] Register settings of IOCFGx registers when selecting data format in Cont. RX.
- [CC254x] Receive data in Packet RX when "Text" format and "sequence number included" was selected.
- [CC2541] Register settings for modulated/unmodulated signal in Cont. TX.
- [CC2510] Update of parameter values when "Device Reset" button clicked.
- [DCP] Fixed packet length in Packet TX not updated when text or hex mode selected.
Version 1.7.0
Release date: December 7, 2011
New Features and Enhancements
- [CC2541] Support for CC2541.
- [CC1120] The register descriptions in register view have been updated.
- [DCP] The Register export function has been updated. Templates stored as xml files. The layout of the dialog has been changed.
- [CC430] The MSP430.dll updated to version 3. This is a major upgrade and the FW of the MSP-FET430UIF will have to be updated when starting
a session for CC430. To downgrade to previous version a special procedure must be followed. See www.ti.com/mspds for more details.
Bug Fixes
- [CC112x] Register settings for "Synchronous" and "Transparent" mode in Cont. TX/RX updated.
- [DCP] Problem with slow update of the packet list in Packet RX solved.
- [DCP] Problem with address filtering solved.
Version 1.6.1
Release date: September 13, 2011
New Features and Enhancements
- [CC1175] Support for CC1175.
- [CC112x] The default signal detection in RX sniff mode set to "RSSI".
- [CC112x] The TX power values have been updated.
- [DCP] Automatic scrolling in Packet RX turned off as default.
- [CC11xL] The registers CHANNR, MDMCFG0 and MDMCFG1 added to the Register view.
Bug Fixes
- [CC112x] Handling of invalid RX Filter BW added when the register CHAN_BW has been changed in register view.
- [CC112x] The registers IF_ADC0 and FREQ_IF_CFG set depending on crystal value. Improved RX performance for 40MHz crystal value.
- [CC112x] The RSSI offset value has been updated.
- [CC112x] When selecting unmodulated signal in Cont. TX, the modulation format will be changed to "FSK" if it was "ASK/OOK".
- [CC1101] Typical settings not reset when selecting antenna for range extender RF3858.
- [CC1101] Problem with loading of channel number from configuration file solved.
- [CC1101] The RSSI offset value and the TX power settings have been updated when using the range extender RF3858.
- [CC11xx] Solved problem with loading of correct DEVIATN register value from the configuration file.
- [CC430] Problem with selection of "Random" mode in Cont. TX solved.
- [DCP] Problem with persistent yellow background on the frequency parameter solved.
- [CC2520] The packet handler has been updated to handle "automatic CRC generation off".
Known Issues
- [CC1120, CC1121, CC1175] Narrow band settings do not always give a working link.
Make sure that both boards are aligned in terms of the RF frequency.
Verify this by using the “continuous RX” mode and vary the TX frequency (a few kHz) until
maximum RSSI is reached. Use low TX power for the testing such that the RSSI level is lower than -30dBm.
- [DCP] In Packet RX the display of received packets is not always synchronized with what has really been received. The update of the window can be delayed.
- [CC1101, CC2500] Handling of fixed packet length only supported by the TrxEB board.
- [CC1175] The register definition used in register view is based on the same source as for CC112x. That means
that some registers for RX related parameters might seem to be available while input to those registers will not have any effect.
Version 1.5.0
Release date: June 28, 2011
New Features and Enhancements
- [CC112x] Support for CC1120 and CC1121 added.
- [CC11xL] Support for CC110L, CC113L and CC115L added.
- [DCP] Improved the settings view with categories organized in a tree structure.
- [DCP] New feature to change the packet interval in Packet TX
- [DCP] Automatic scrolling added to the packet view in the Packet RX panel.
- [DCP] To make the selection of modulated/unmodulated signal in Continuous TX more intuitive,
the check box has been replaced with radio buttons.
- [DCP] Packet RX/TX: Sequence number moved to first position in packet payload
- [DCP] Code export: exports by default all registers with value different from reset
- [DCP] Improved user interface in Command Strobe panel
- [DCP] Registers sorted on address in Register export.
- [DCP] RSSI Offset, used in the "Cont. RX" and the "command" panel, updated when using range extender boards.
- [DCP] HTML tags in bit-field descriptions not correctly decoded.
- [STARTW] Problem with FW update of EB boards while more than one device connected.
- [DOC] The documentation of the script module has been improved
- [DOC] Register export documentation improved
- [CC430] Support for all CC430 devices.
- [CC430] Error message when failing to start Device Control Panel improved.
- [CC1101-CC1190] Updated register settings
- [CC1101-CC1190] The correct categories of settings will be selected automatically depending on the selected front end and revision.
- [CC111x, CC251x] Added support for fixed packet length.
Bug Fixes
- [DCP] PER result in Packet RX fixed to handle sequence numbers
from the received packet that is out of range (Higher than expected number of packets).
The packet will be counted as an error.
- [DCP] Save Config will only save register values different from the reset value.
This solves problem seen for CC430 with loading of config file.
Known Issues
Version 1.4.9
Release date: February 21, 2011
New Features and Enhancements
- Certified USB Drivers with support for 64 bit operating systems included in the installer.
- The default folder location for the installation has been changed. All SmartRF tools will be installed under "SmartRF Tools".
- An option to uninstall SmartRF Studio 7 added to the startup menu.
- [DCP] Save/Load config improved. The config file will be saved as xml file.
- [CC1101] Support for range extender added.
- [CC430] RF devices connected via MSP-FET430 will not be automatically shown in the list of
connected devices. The user must click the "refresh" button to get the CC430 board visible
in the list of connected devices.
Bug Fixes
- [CC430] The allowed frequency range has been changed for the 868MHz band: 779 - 928 MHz.
- [DCP] The Register view was hidden after minimized/maximized of the Device Control Panel.
- [DCP] After maximizing the Device Control Panel, some registers where updated depending on current test function.
The registers will no longer be updated on maximize.
- [DCP] Problem with programming of registers when loading config files for some RF Devices (E.g. CC1101).
- [CC2540] Crash on Reset Config and Save Config fixed.
- [CC2533, CC2531 and CC2540] Reconnect after the device has been disconnected from the USB bus.
Known Issues
- FW update of a connected Evaluation Board can fail if more than one board is connected.
If FW update is required, make sure that only one board is connected.
Version 1.3.2
Release date: November 15, 2010
New Features and Enhancements
- [STARTW] Feature to bring up Device Control Panel on top of desktop when click on line in list of connected devices.
Bug Fixes
- [CC2540] Register settings for unmodulated signal in Cont. TX updated. MDMCTRL0::TX_IF=1.
- [CC430] Problem with crash when attempting to open Device Control Panel for not supported MSP430 device.
Known Issues
- [CC430] On some PC's it might be a problem to detect all the MSP-FET430+CC430EB devices when more than one is connected.
Version 1.3.1
Release date: September 15, 2010
New Features and Enhancements
- [DCP] Packet TX set as default test function on startup.
- [DCP] The behavior of the push buttons has been changed. If the user press the button and move the mouse out
of the "button focus" before releasing it, the applicable function will not be activated.
- [DCP] A "Reset" button has been added to the top of the control panel. The button will only be visible if the register view
is disabled. The button has the same function as the one that can be found on the bottom of the Register View panel.
- [DCP] For the packet view in Easy Mode, the XML file defining the packet has been changed. To include "read only" fields in the
packet payload a new element has been added: "AppendToPayLoad". The default value is false.
- [DCP] The RSSI value for each packet will be shown in expert mode for Packet RX.
- [CC253x] The registers OBSSEL0 - OBSSEL5 added to the register view.
Bug Fixes
- [DCP] Problem with wrong display of the device id on the LCD of the Evaluation Board solved. When using the "identify board"
function from the menu, the device id was displayed with a "0x0x" prefix.
- [CC430] Delay time between sent packets in Packet TX changed to enable testing with lower data rate than 1.2 kBaud.
- [CC430] Typical settings for 38.4 kBaud, current optimization: MDMCFG2 changed from 0x83 to 0x93(Modulation changed from 2-FSK to GFSK)
Known Issues
- [CC430] On some PC's it might be a problem to detect all the MSP-FET430+CC430EB devices when more than one is connected.
Version 1.3.0
Release date: August 20, 2010
New Features and Enhancements
- [CC2540] Support for this RF Device added.
Known Issues
- [CC430] On some PC's it might be a problem to detect all the MSP-FET430+CC430EB devices when more than one is connected.
Version 1.2.3
Release date: August 17, 2010
Bug Fixes
- [CC430] Problem with FW update of the MSP-FET430 debugger has been solved.
Known Issues
- [CC430] On some PC's it might be a problem to detect all the MSP-FET430+CC430EB devices when more than one is connected.
Version 1.2.2
Release date: July 23, 2010
Bug Fixes
- [CC2533] The text on the device icon has been updated.
- [CC2533] The Device description has been added.
- [CC110x/CC2500] Problem with Save/Open Configuration data solved.
Version 1.2.1
Release date: June 29, 2010 (Build ID: 15070)
New Features and Enhancements
- [CC110x/CC2500] PER test configuration panel added.
- [DCP] "Code export" changed to "Register export". The option is now also available from the file menu.
Bug Fixes
- [DCP] The unit of output power was given twice in some panels. This has been corrected.
Version 1.2.0
Release date: June 7, 2010
New Features and Enhancements
- [CC2533] Support for this RF Device added.
- [DCP] When a button is pressed it will be visible for the user.
- [DCP] Added input fields for number of packets in Easy-mode.
- [DCP] The appearance of fields to show status in Packet TX/RX changed to make it
clear that it is not for input. In addition the unit has been added to the
frequency and output power parameters.
- [DCP] Added input fields for number of packets in Easy-mode.
Bug Fixes
- [DCP] The sequence number has been added to the SimpliciTI packet header for IEEE 802.15.4 devices.
Version 1.1.1
Release date: May 4, 2010 (Build ID: 14768)
New Features and Enhancements
- [CC430] Support for this RF Device added.
Bug Fixes
- [CC2520] The Packet TX function has been updated to improve the Packet Error Rate.
Version 1.0.3
Release date: April 16, 2010 (Build ID: 14545)
The first official release of SmartRF Studio 7.
New Features and Enhancements
- [DCP] New feature for logging in Device Control Panel.
The user can select if the log of register writes and strobe commands should be
directed to a file or it should be seen directly in a "Log window".
- [DCP] New feature in Easy mode: "Packet view".
The data sent over the air will be a valid packet and is depending on the selected Easy mode option.
The content of the packet is visualized with details for each field in the packet.
Version 0.9.1
Release date: February 3, 2010 (Build ID: 13859)
New Features and Enhancements
- [DOC] Software Manifest added.
- [DCP] Scroll bars added to the Device Control Panel.
Bug Fixes
- [STARTW] Solved problem with application crash after reconnecting device on USB port.
Version 0.8.1
Release date: January 21, 2010 (Build ID: 13721)
This is the first public beta release of SmartRF Studio version 7.