TI BLE5-Stack Quick Start¶
This section serves as a road map for users developing applications and products using the TI SimpleLink CC26x2 wireless MCU platform for Bluetooth low energy applications. Whether a seasoned developer or just getting started, TI has created a variety of resources to simplify development on the CC26x2 platform. These resources will enhance your experience with the TI SimpleLink TI BLE5-Stack 1.60.00.43 from the out-of-the-box demo to production.
Figure 47. shows the suggested work flow for getting started with TI’s SimpleLink Bluetooth low energy (BLE) development environment.
 
Figure 47. Suggested Workflow
Using BLE5-Stack Projects with CCS¶
Importing BLE5-Stack app projects into CCS will also import BLE5-Stack stack library projects into CCS. The stack library project is a dependent project and will be automatically built when the example is built.
Projects that contain the TI Over-the-Air Download (OAD) Profile will also import the Boot Image Manager (BIM) into the workspace. For more information on the TI OAD Profile and the BIM see the OAD Chapter of the BLE5-Stack User’s Guide.
For more details and how to change configurations look at the SimpleLink TI BLE5-Stack User’s Guide.
Import Project Using Resource Explorer¶
A quick and easy way to start working with the SDK is to use the TI Resource Explorer in CCS.
This section describes how to import and build an existing project and references the project_zero project. All of TI BLE5-Stack projects included in the development kit have a similar structure.
- Open the CCS IDE from the Start Menu. 
- Create a workspace. - Attention - Ensure that the CCS workspace path does not contain a whitespace. 
- Import a CCS Project using Resource Explorer - Open Resource Explorer (if not open already): View -> Resource Explorer
- Navigate to the CCS folder for your chosen example: Software → SimpleLink CC26x2 SDK → Examples → CC26x2 LaunchPad → ble5stack → project_zero → TI-RTOS → CCS Compiler → project_zero_app
   - Figure 48. Import CCS Projects 
- Select the CCS Logo button to import project into Project Explorer - Attention - The import process will also install the SimpleLink CC26x2 SDK if a local version does not exist. You must accept the End User License Agreement to proceeed.   - Figure 49. Install SimpleLink CC26x2 SDK - After the installation finishes, you must reopen CCS before importing the project. - If you get a pop-up window with an error message, under “Details >>” saying “Error: A project with the name ‘xx_stack_library’ already exists in the workplace!”, that is fine. You accidentally imported the stack twice. Just click OK.
- If everything is successful, three projects should appear in Resource Explorer: one for the application code (ble5_project_zero_cc26x2r1lp_app), one for the stack code (ble5_project_zero_cc26x2r1lp_stack_library), and one for the BIM (cc26x2r1lp_bim_offchip).
 - Note - Not all projects in the SimpleLink CC26x2 SDK will have both an app and a stack library project. Refer to the relevant protocol Quick Start section for working with non-BLE5-Stack projects in the SimpleLink CC26x2 SDK.   - Figure 50. Projects Imported into CCS 
Build and Download Project¶
For all build configurations, the Stack project should always be built before the Application project. For projects containing the TI OAD Profile, it is recommended to build the BIM first.
To build & download Project Zero:
- Build the BIM project. - Set the BIM project as the active project. Make sure the Debug project configuration is used.
- Select Project -> Build All to build the BIM project.
 
- Load the BIM project - Select Run -> Debug to download the BIM
- Once the debugging session starts, click the red stop button
 
- Build the Stack Library project. - Set the Stack Library project as the active project.
- Select Project -> Build All to build the Stack Library project.
 
- Build the Application project. - Set the Application project as the active project.
- Select Project -> Build All to build the Application project.
 
- Load the Application project (this will include the Stack Library) - Select Run -> Debug to download the application
 
Note
Application projects that consume the stack in a library form will not have hard defined image boundaries.
After the initial build, if the stack project is not modified, only the application project needs to be rebuilt.
Before beginning execution, open a terminal window with the following settings:
| UART Param | Default Values | 
|---|---|
| Baud Rate | 115200 | 
| Data length | 8 bits | 
| Parity | None | 
| Stop bits | 1 bit | 
| Flow Control | None | 
When the debugging session opens, click the Green start button to start execution.
Continue on to the Running the Demo section for information about using
Project Zero.
Using BLE5-Stack Projects with IAR¶
When building with IAR, it is recommended to enable all build messages. This can be done by right-clicking in the Build window and selecting “All” as shown below:

Figure 51. Enable All Build Messages
Import Project Using Workspace¶
This section describes how to open and build an existing project and references the project_zero project.
All of the TI BLE5-Stack workspace included in the SimpleLink CC26x2 SDK have an Application project and a Stack Library project.
In addition, applications containing the TI Over-the-Air Download (OAD) Profile will also include the Boot Image Manager (BIM) project. For more information on the TI OAD Profile and the BIM see the OAD Chapter of the BLE5-Stack User’s Guide.
Error
If you have imported the global
<SDK_INSTALL_DIR>/tools/iar/SIMPLELINK_CC13XX_CC26XX_SDK.custom_argvars
as described in Using TI Drivers Projects with IAR,
then TI BLE5-Stack examples will fail to build. For TI BLE5-Stack examples,
you must remove this custom_argvars file from your IAR global custom
arguments.
- Open the IAR Embedded Workbench IDE from the Start Menu. 
- Open an IAR workspace project: File -> Open -> Workspace… - For this example, select <SDK_INSTALL_DIR>\examples\rtos\|DEVBOARD|\ble5stack\project_zero\tirtos\iar\ble5_project_zero.eww
 
This workspace file is for the project_zero project. When selected, the files associated with the workspace become visible in the Workspace pane on the left side of the screen. See Figure 52.
Select either project as the active project by clicking the respective tab at the bottom of the workspace pane. In Figure 52., the Overview tab is selected. This tab displays the file structure for both projects simultaneously. In this case, use the drop-down menu at the top of the workspace pane to select the active project. Each of these projects produces a separate downloadable object.
Build and Download Project¶
For all build configurations, the Stack project should always be built before the Application project. For projects containing the TI OAD Profile, it is recommended to build the BIM first.
To build & download Project Zero:
- Build the BIM project. - Set the BIM project as the active project. Make sure the Debug project configuration is used.
- Select Project -> Make to build the BIM project.
 
- Load the BIM project - To download without debugging: Select Project -> Download ->
- Download Active Application
 
- When the download process is complete, you will see a message that the .out file was downloaded to flash memory in the Debug Log.
 
- Build the Stack Library project. - Select the Stack project.
- Select Project -> Make to build the Stack Library project.
 
- Build the Application project. - Select the Application project.
- Select Project -> Make to build the Application project.
 
- Load the Application project (this will include the Stack Library) - To download and debug: Select Project -> Download and Debug
- To download without debugging: Select Project -> Download ->
- Download Active Application
 
 
Note
Application projects that consume the Stack in a library form will not have hard defined image boundaries.
After the initial build, if the Stack project is not modified, only the application project needs to be rebuilt.
Refer to the Project Zero readme for more information about this project.
Before beginning execution, open a terminal window with the following settings:
| UART Param | Default Values | 
|---|---|
| Baud Rate | 115200 | 
| Data length | 8 bits | 
| Parity | None | 
| Stop bits | 1 bit | 
| Flow Control | None | 
When the debugging session opens, click the start button to start execution.
Continue on to the Running the Demo section for information about
using Project Zero.
Running the Demo¶
After hitting the play button, your terminal window should display the Project Zero initialization information as shown below:

Figure 53. Project Zero Initialization
This provides information about the services present in Project Zero. Project Zero has 4 interactive services: the LED service, the button service, the data service, and the OAD service.
Writing a non-zero value to the LED service will cause the LEDs on the LaunchPad to light up. Writing zero will turn them off. Enabling notifications on the Button service will cause the Peripheral to send notifications of current button state (0 - not pressed, 1 - pressed) to the Central device. The Data service can be used to read and write multiple bytes of data. The OAD service can be used for updating the image currently running on the LaunchPad.
Choose the Central device from the list below to connect with. If you wish to perform an OAD, you must use either an iOS device or BTool with another CC26x2 LaunchPad as your Central.
Host Test Setup
The easiest way to connect to Project Zero with another CC13xx/26xx LaunchPad is by using BTool. BTool allows you to send HCI commands to the LaunchPad to easily establish BLE communication with another device.
To use BTool, you must flash your second CC26x2 LaunchPad with the Host Test firmware from a compatible version of the TI BLE-Stack/BLE5-Stack. Pre-built Host Test binaries are included in the ble5stack examples directory of the SDK.
Uniflash can be used to program the LaunchPad with the Host Test firmware:
 
Figure 54. Flash Host Test using Uniflash
Open BTool from the toolsble5stackbtool folder of the SDK_INSTALL_DIR. Select the XDS110 UART COM Port for your Host Test LaunchPad:
 
Figure 55. BTool Serial Port Settings
When BTool connects to the LaunchPad, it will issue several initialization commands. If the commands succeed, you will receive multiple HCI Events with a Status of “SUCCESS”.
Connect to Project Zero
Scan for nearby advertising Bluetooth devices by selecting the Scan button in the Discovery window. Make sure your Project Zero LaunchPad is connected to power and advertising.
Compare the device addresses in the Slave BDA dropdown with the address shown in the Project Zero terminal window. Select the matching address and click “Establish” to connect to Project Zero.
 
Figure 56. Scanning & Connecting with BTool
After the connection has established, discover & read the current value of the services and characteristics available on Project Zero by right-clicking on the Handle in the Connection Info section and selecting Read Values.
 
Figure 57. BTool GATT Table Discovery
The bottom of the BTool GUI will display the Project Zero GATT Table to help you navigate and control the Project Zero services.
 
Figure 58. BTool GATT Table Discovery
Using the LED Service
Writing 0x01 to the characteristics in the LED Service will turn on the Project Zero LaunchPad LEDs. You can write to the characteristic by double clicking the Value field of the LED0 State or LED1 State characteristics.
 
Figure 59. Writing to a Characteristic
The Project Zero terminal window will update with the current LED state:
 
Figure 60. Turning on Project Zero LEDs
Using the Button Service
You can choose to receive notifications about the current state of the Project Zero Button Service by writing 01:00 to the Client Characteristic Configuration Descriptors of the Button Service. After enabling notifications, the current value of the Button state will be displayed in BTool.
 
Figure 61. Enabling Notifications in BTool
 
Figure 62. Pressing & Releasing Buttons
Using the Data Service
You can read and write multiple bytes of data by using the Data Service. Double click on the Value field of the String Char. You can write the new value directly in ASCII or you can choose a different type by selecting from the Value Type dropdown menu.
 
Figure 63. Writing to the Data Service
 
Figure 64. Data Service Value change
Using the OAD Service
Project Zero includes the TI OAD Profile which allows you to download new firmware images over-the-air. Images must be compatible with the CC26x2 and contain the TI OAD Profile in order to be downloaded successfully. For more information on creating a new image for OAD, please see the OAD Chapter of the BLE5-Stack User’s Guide.
Note
If Project Zero was not the first image containing the TI OAD Profile you flashed on your LaunchPad Out-of-the-Box, the factory image in your external flash may not be Project Zero. This could mean that you will be unable to return to Project Zero by using the factory reset option after performing an OAD and will have to use the debugger to load a new image.
Refer to the Project Zero readme for more information about this project and resetting the factory image contained in external flash.
In BTool, choose Over The Air Download in the “Select Device Operation” box. In this demo, we will use Project Zero as our example since a valid image was created during the build process.
Select the new image to load on your CC26x2 LaunchPad by clicking Read Image
File. Navigate to your Project Zero build output directory. Select the
*_oad.bin file. The *_oad.bin file will contain a valid image header.
BTool will send a connection parameter update at the beginning of an OAD to attempt a faster download. The embedded application will also attempt a parameter update (if enabled). It is recommended to wait until the application’s connection parameter update has taken place before starting an OAD. If you are experiencing a slow OAD, this may be the cause. The parameter update is complete once the following message is shown in the BTool log:
--------------------------------------------------------------------
[7] : <Rx> - 04:16:04.518
-Type           : 0x04 (Event)
-EventCode      : 0x00FF (HCI_LE_ExtEvent)
-Data Length    : 0x0B (11) bytes(s)
 Event          : 0x0607 (1543) (GAP_LinkParamUpdate)
 Status         : 0x00 (0) (SUCCESS)
 ConnHandle     : 0x0000 (0)
 ConnInterval   : 0x0024 (36)
 ConnLatency    : 0x0000 (0)
 ConnTimeout    : 0x00C8 (200)
Dump(Rx):
0000:04 FF 0B 07 06 00 00 00 24 00 00 00 C8 00       ........$.....
--------------------------------------------------------------------
 
Figure 65. Updating Firmware Image with BTool
Once you are sure this is the image you want to run, click Send to begin the OAD process.
The Status bar will provide information on the current status of the download. If the download completes successfully, you will receive a “OAD Download Successful” message in BTool.
Note
After an OAD has completed, you may need to manually hit the reset button on the CC26x2 LaunchPad in order to trigger a full reset and jump to BIM. This step is only required after first programming the device.
This will disconnect the debugger and terminate the debugging section.
Download the latest version of the TI SensorTag app (v5.1+) from the iOS app store. When the download completes, open the app:

Figure 66. SimpleLink Starter App
Connect to Project Zero
When the app opens, nearby Bluetooth low energy devices will appear. You should see ProjectZero advertising as shown below:

Figure 67. Project Zero Advertising
Press the Project Zero item and select Sensor View. The services present in Project Zero will appear as shown below:

Figure 68. Project Zero Advertising
The Project Zero terminal information will also update with connection information including the peer device address, PHY, and MTU Size. For more information about these parameters, see the BLE5-Stack User’s Guide.

Figure 69. Project Zero After Connection
Using the LED Service
To turn on an LED, press one of the buttons on the LED service. The left button turns the Red LED (DIO6). The right LED turns on the Green LED (DIO7). Pressing the button again will turn the LED off. The Project Zero terminal window will update with the current LED state.

Figure 70. Project Zero LED Service

Figure 71. Turning on Project Zero LEDs
Using the Button Service
Button press notifications are automatically enabled when connecting through the Sensor View. If you press and release either button, the Sensor View will update with the current state and the button state graph will show the button state over time (High corresponds to button pressed, low corresponds with button released).

Figure 72. Project Zero Button Service

Figure 73. Pressing & Releasing Buttons
Using the Data Service
The Data Service is not displayed in Sensor View. To use the Data Service, close the Sensor View by pressing the < Sensor Tag button in the upper left. This returns you to the main SensorTag view. Press the ProjectZero icon again and now select Service Explorer. The Data Service is the service with the UUID that begins with F0001130 (List Item 3). Press the item and you will see two characterisitics. The first characteristic can be used to read and write multiple bytes of data. You can do this by pressing Read characteristic to get data from ProjectZero and Write w/response characteristic to send multiple bytes of data to ProjectZero.

Figure 74. Project Zero Button Service

Figure 75. Writing to the Data Service
Using the OAD Service
Return to the Sensor View by returning to the main SensorTag view and reconnecting to Project Zero using the Sensor View. Select FW Download (Enhanced) to use the TI OAD Profile to download a new image to your LaunchPad Over-the-Air.
Note
If Project Zero was not the first image containing the TI OAD Profile you flashed on your LaunchPad Out-of-the-Box, the factory image in your external flash may not be Project Zero. This could mean that you will be unable to return to Project Zero by using the factory reset option after performing an OAD and will have to use the debugger to load a new image.
Refer to the Project Zero readme for more information about this project and resetting the factory image contained in external flash.
Select a new image to load on your CC26x2 LaunchPad by pressing Select FW File.
This will display a selection of available firmware images. To select a new
BLE5-Stack image, choose either Project Zero or Simple BLE Peripheral, then
select Start OAD. To select a new image for a different wireless technology,
choose the firmware image of choice, select Start OAD and skip to the
applicable Running the Demo section of the Quick Start Guide.
After selecting Start OAD, the SimpleLink Starter app will display download
progress:

Figure 76. Performing an OAD
Note
After an OAD has completed, you may need to manually hit the reset button on the CC26x2 LaunchPad in order to trigger a full reset and jump to BIM This step is only required after first programming the device.
This will disconnect the debugger and terminate the debugging section.
The instructions for this tutorial are written to use the BLE Scanner application but you can use any BLE Client application that you are familiar with.

Figure 77. BLE Scanner App
Connect to Project Zero Open the BLE Scanner app on your device. The app should begin scanning for BLE devices automatically but you can toggle scanning on and off by clicking the magnifying glass in the top right corner of the app. A “Scanning stop” message will appear. Make sure your Project Zero LaunchPad is nearby and advertising. Project Zero should appear in the Near By devices list:

Figure 78. Discovering Project Zero
Click the Connect button to establish a connection to Project Zero. In BLE Scanner, you will see the services available on Project Zero. Three services have unique names and four services are named “Custom Service”.

Figure 79. Project Zero Services
Using the LED Service
The UUID for the LED Service begins with F0001110. Tap the Custom Service item matching the LED Service UUID to display the available characteristics. To read the current state of the LEDs, press the R circle. To write to the LED service, press the W circle. Select Byte Array. Writing 01 will turn on the LEDs on the LaunchPad, writing 00 will turn off the LEDs. The Project Zero terminal window will update with the current state of the LEDs.

Figure 80. Project Zero LED Service

Figure 81. Turning on Project Zero LEDs
Using the Button Service
The UUID for the Button Service begins with F0001120. Tap the Custom Service item matching the Button Service UUID to display the available characteristics. The Button Service has the ability to send notifications to the peer device when the current state changes. These notifications can be enabled by tapping the N circle.

Figure 82. Project Zero Button Service

Figure 83. Pressing & Releasing Buttons
Using the Data Service
The UUID for the Data Service begins with F0001130. Tap the Custom Service item matching the Data Service UUID to display the available characteristics. The Data Service allows you to read and write multiple bytes of data to Project Zero. Press the R circle in the top characteristic to read the value of the String characteristic. You can write a new value by pressing the W circle.

Figure 84. Project Zero Button Service

Figure 85. Writing to the Data Service
Learning More About TI BLE5-Stack¶
Resources contained in the Learn track of Figure 47. are intended for users who are new to BLE or TI-RTOS. These modules demonstrate how to create custom applications with TI BLE5-Stack and TI’s Real Time Operation System (TI-RTOS).
- SimpleLink Academy www.ti.com/simplelinkacademy
SimpleLink Academy provides a comprehensive set of training tools that allow users from beginners to experienced developers to learn about the SimpleLink MCU Platform.
Using introductory material and labs, learn the fundamentals of BLE and how to develop a custom BLE profile.
SimpleLink Academy also contains modules written to demonstrate the rich debug environment and peripheral driver capability provided by TI-RTOS.
- TI-RTOS Kernel Workshop www.training.ti.com/ti-rtos-kernel-workshop
This material teaches users who are new to TI-RTOS or any RTOS programming in general about TI’s RTOS kernel implementation.
Modules within the kernel training greatly expand the information presented in the TI-RTOS Overview chapter in the TI BLE5-Stack User’s Guide.
Learn how the TI-RTOS provides the most optimal power management and design flexibly.
Developing a New BLE5-Stack Based Application¶
The develop track of Figure 47. is intended for programmers who are ready to start developing an end product using the CC26x2. To begin:
Get Familiar with the BLE5-Stack User’s Guide
This User’s Guide is meant to be used alongside the TI BLE5-Stack when developing an end product. It contains documentation on the stack architecture, APIs, and suggestions for developing applications.
Important
For the latest User’s Guide, see the Online BLE5-Stack User’s Guide.
Select an Example Project
The TI BLE5-Stack includes a basic set of projects to use as a starting point for development of your custom application. Click the links below to find out more information about each project:
| Name | Description | 
| host_test | A network processor project that is interfaced with HCI and Vendor Specific HCI commands. | 
| multi_role | Provides the ability to operate function in multiple simultaneous connection roles | 
| project_zero | Feature rich peripheral application that provides LED and button functionality OOB | 
| simple_broadcaster | Demonstrates a simple Bluetooth low energy broadcaster application that implements non-connectable advertisements | 
| simple_central | Implements a basic BLE central device with GATT client functionality. | 
| simple_peripheral | Demonstrates a simple Bluetooth low energy slave application that implements connectable advertisements and a simple profile. | 
| simple_peripheral_oad_offchip | Same as simple_peripheral above with the addition of the OAD service to enable wireless firmware updates | 
Troubleshooting Help
While developing your custom application, you may run into issues that require the use of a debugger. See the Debugging chapter in the TI BLE5-Stack User’s Guide for guidance.
Enhance Your Project¶
The enhance track of Figure 47. is intended to take your product to the next level by leveraging TI’s web-based collateral. Additional resources found in these pages include application-specific source code examples, smart phone source code, and complete sub-system designs.
- TI SimpleLink GitHub TI SimpleLink GitHub
Additional sample applications created to implement specific use cases and examples. These are made to work in conjunction with the SDK.
- Bluetooth Developer’s Studio Plugin TI BDS Plugin
TI offers a plugin for the Bluetooth Developer Studio tool. Developers can use this tool, developed by the Bluetooth Special Interest Group (SIG), with TI’s SimpleLink plugin to reduce development time by automatically generating compilable code for proprietary and adopted profiles running on the CC26x2. See SimpleLink Academy for instructions on integrating a BDS profile with a sample project.
- TI Designs™ https://www.ti.com/tidesigns
Examples of system designs containing complete hardware and software examples, using the CC26x2.
Getting Support¶
The support track of Figure 47. is intended to provide you additional help and resources that aren’t contained in the previous tracks.
- BLE-Wiki www.ti.com/ble-wiki
A collection of webpages that contain step-by-step guides and code snippets that enable certain features and enhancements to the CC26x2, such as production test mode and certification.
- E2E Forums www.ti.com/ble-forum
A support community providing answers to questions relating to the 1.60.00.43 and the CC26x2. You can browse questions from other developers or ask your own questions if you run into issues developing with 1.60.00.43.