Release date: February 2, 2017
New features
- CC26x0R2
- [RF_API] BT5: Added command header files.
- [RF_PATCH] BT5: Added CPE patch.
- CC26x0
- [RF_API] IEEE 802.15.4: Added command header files.
- [RF_PATCH] IEEE 802.15.4: Added CPE patch.
- [RF_PATCH] IEEE 802.15.4: Added MCE/RFE patches for use with single ended frontend.
- CC13x0
- [RF_PATCH] WMBUS: Added S1- and S2-Mode CPE, MCE and RFE patch.
Improvements
- Changes that applies to all devices
- [RF_PATCH] General: All MCE and RFE patches have new include paths for the hw_type.h file.
- [RF_PATCH] General: Added RFE_PATCH_MODE and MCE_PATCH_MODE defines for future partial patching support.
- [DRV_SRC] General: Removed deprecated functions:
- OSCInterfaceEnable()
- OSCInterfaceDisable()
- SysCtrlPowerEverything()
- [DRV_SRC] ChipInfo: Added support for new chip and package types (Note that packages available for a specific device are shown in the device datasheet).
- Added PACKAGE_7x7_Q1 as new return option from function ChipInfo_GetPackageType() and added function ChipInfo_PackageTypeIs7x7Q1().
- Added HWREV_2_4 as new return option from function ChipInfo_GetHwRevision() and added function ChipInfo_HwRevisionIs_GTEQ_2_4().
- [HW_INC] General: Updated/improved hardware register descriptions (inc/hw_*.h and doc/../*.html files).
- CC26x0R2
- [RF_API] BLE: Updating structures with BT5 fields.
- [DRV_SRC] SysCtrl: Added RSTSRC_WAKEUP_FROM_TCK_NOISE as new return option from function SysCtrlResetSourceGet().
- CC26x0
- [RF_API] General: Adding dummy define for rfc_CMD_BLE5_RADIO_SETUP_t to increase compatibility with other chips.
- CC13x0
- [RF_API] General: Adding dummy define for rfc_CMD_BLE5_RADIO_SETUP_t to increase compatibility with other chips.
Bug fixes
- Changes that applies to all devices
- [DRV_SRC] Crypto: Function CRYPTOAesLoadKey(): Corrected problem with storing multiple keys.
- CC13x0
- [RF_PATCH] General: CMD_SCH_IMM could cause loss of commands. Fixed with CPE patch.
Known Issues
- CC26x0
- CC26xxR2
- [RF_PATCH] General: CMD_SCH_IMM could cause loss of commands.
- For an updated list of known issues (including issues found after the release), see CC13xx_CC26xx_driverlib on the Texas Instruments wiki.