Sensor Controller ================= The Sensor Controller (:term:`SC`) is an autonomous processor within the |DEVICE|. The Sensor Controller can control peripherals independently of the main CPU. For example, the main CPU does not have to wake up to execute an ADC sample or poll a digital sensor over SPI. This saves both current and wake-up time that would otherwise be wasted. A PC tool lets you configure the Sensor Controller and choose which peripherals are controlled and which conditions wake up the main CPU. Sensor Controller Studio (:term:`SCS`) is a stand-alone IDE to develop and compile microcode for execution on the Sensor Controller. Refer to Sensor Controller Studio Help for more details and documentation on the Sensor Controller. #. Install the Sensor Controller Studio. Sensor Controller Studio can be downloaded from `here `_ #. Find documentation in Sensor Controller Studio by pressing **F1** or by going to *Help* -> *Sensor Controller Studio Help*