TI BLE-Stack for Bluetooth 4.2 API Documentation
3.01.00.07
|
Commands Acronyms / Event Name | Origin | Type | TL Cmd0 | TL Cmd1 | Parameter structure |
---|---|---|---|---|---|
SNP_POWER_UP_IND | NP | Async | SNP_NPI_ASYNC_CMD_TYPE (0x55) | SNP_POWER_UP_IND (0x01) | |
SNP_MASK_EVT_REQ | AP | Sync Req | SNP_NPI_SYNC_REQ_TYPE (0x35) | SNP_MASK_EVT_REQ (0x02) | snpMaskEventReq_t |
SNP_MASK_EVENT_RSP | NP | Sync Rsp | SNP_NPI_SYNC_RSP_TYPE (0x75) | SNP_MASK_EVENT_RSP (0x02) | snpMaskEventRsp_t |
SNP_GET_REVISION_REQ | AP | Sync Req | SNP_NPI_SYNC_REQ_TYPE (0x35) | SNP_GET_REVISION_REQ (0x03) | |
SNP_GET_REVISION_RSP | NP | Sync Rsp | SNP_NPI_SYNC_RSP_TYPE (0x75) | SNP_GET_REVISION_RSP (0x03) | snpGetRevisionRsp_t |
SNP_HCI_CMD_REQ | AP | Async | SNP_NPI_ASYNC_CMD_TYPE (0x55) | SNP_HCI_CMD_REQ (0x04) | snpHciCmdReq_t |
SNP_HCI_CMD_RSP | NP | Async | SNP_NPI_ASYNC_CMD_TYPE (0x55) | SNP_HCI_CMD_RSP (0x04) | snpHciCmdRsp_t |
SNP_EVENT_IND | NP | Async | SNP_NPI_ASYNC_CMD_TYPE (0x55) | SNP_EVENT_IND (0x05) | snpEvt_t |
SNP_GET_STATUS_REQ | AP | Sync Req | SNP_NPI_SYNC_REQ_TYPE (0x35) | SNP_GET_STATUS_REQ (0x06) | |
SNP_GET_STATUS_RSP | NP | Sync Rsp | SNP_NPI_SYNC_RSP_TYPE (0x75) | SNP_GET_STATUS_RSP (0x06) | snpGetStatusCmdRsp_t |
SNP_GET_RAND_REQ | AP | Sync Req | SNP_NPI_SYNC_REQ_TYPE (0x35) | SNP_GET_RAND_REQ (0x07) | |
SNP_GET_RAND_RSP | NP | Sync Rsp | SNP_NPI_SYNC_RSP_TYPE (0x75) | SNP_GET_RAND_RSP (0x07) | snpGetRandRsp_t |
SNP_TEST_REQ | AP | Sync Req | SNP_NPI_SYNC_REQ_TYPE (0x35) | SNP_TEST_REQ (0x10) | |
SNP_TEST_RSP | NP | Sync Rsp | SNP_NPI_SYNC_RSP_TYPE (0x75) | SNP_TEST_RSP (0x10) | snpTestCmdRsp_t |
SNP_SYNC_ERROR_CMD_IND | NP | Async | SNP_NPI_ASYNC_CMD_TYPE (0x55) | SNP_SYNC_ERROR_CMD_IND (0x07) |
All these command have some parameters. The parameters can be found/set using the indicated Parameter structure. All Parameter/Structures should be little-endian format (LSB first). For UUID parameters, dealing with UUID
NP -> AP (N/A)
CMD 0 | CMD 1 |
---|---|
0x55 | 0x01 |
SNP_NPI_ASYNC_CMD_TYPE | SNP_GET_REVISION_RSP |
This event is send by the SNP once the device has powered up. This event will be received if the device is reset unexpectedly. One reception of this event the AP should consider that the NP lost any previous configuration.
When this event is received, the following services are initialized and ready to be used:
This command doesn't have any parameters
NP -> AP (N/A)
CMD 0 | CMD 1 |
---|---|
0x55 | 0x05 |
SNP_NPI_ASYNC_CMD_TYPE | SNP_EVENT_IND |
This indication is send by the SNP to signal an event. Events can be masked by using the SNP_maskEvt API (SNP_maskEvt). Only one event will be indicated at a time per packet. If several events occur, each will be encapsulated in their own TL packet.
Each event has a 2-bytes Event type, list of asynchronous events generated by the SNP. Along with Event type, some events might have some parameters associated with them.
Events parameters are mapped on the snpEvt_t structure, which contains a union of snpConnEstEvt_t, snpConnTermEvt_t , snpUpdateConnParamEvt_t , snpAdvStatusEvt_t and snpATTMTUSizeEvt_t
The table below list the events and the structure used to MAP the parameter of those events:
Event | Parameter Structure | Related |
---|---|---|
SNP_CONN_EST_EVT | snpEvt_t + snpConnEstEvt_t | N / A |
SNP_CONN_TERM_EVT | snpEvt_t + snpConnTermEvt_t | SNP_terminateConn |
SNP_CONN_PARAM_UPDATED_EVT | snpEvt_t + snpUpdateConnParamEvt_t | SNP_updateConnParam |
SNP_ADV_STARTED_EVT | snpEvt_t + snpAdvStatusEvt_t | SNP_startAdv |
SNP_ADV_ENDED_EVT | snpEvt_t + snpAdvStatusEvt_t | SNP_stopAdv |
SNP_ATT_MTU_EVT | snpEvt_t + snpATTMTUSizeEvt_t | SNP Characteristic Read Indication (0x87) |
SNP_ERROR_EVT | snpEvt_t + snpErrorEvt_t | SNP Synchronous Invalid Command Indication (0x07) |
NP -> AP
snpEvt_t
Size | Description |
---|---|
2 Byte | SNP_CONN_PARAM_UPDATED_EVT |
X Byte | Parameter Structure based on table above |
The default ATT_MTU size is set to 23 bytes. The GATT client can request an ATT_MTU_EXCHANGE method to change the maximum possible ATT MTU size. The SNP is compatible with ATT MTU sizes up to 251 Bytes. If an update occurs due to a request from a peer device, the corresponding event will be send by the SNP to inform AP that MTU size has changed. If this event is not received, the AP must assume that ATT MTU size is 23.
NP -> AP
snpEvt_t
Size | Description |
---|---|
2 Byte | SNP_ATT_MTU_EVT |
1 Byte | Connection Handle |
2 Byte | MTU Size of Connection |
This error event occurs if something unexpected occurs while SNP is running some operation. The list of all possible SNP errors can be found here list of status generated by the SNP.
NP -> AP (N/A)
CMD 0 | CMD 1 |
---|---|
0x55 | 0x07 |
SNP_NPI_ASYNC_CMD_TYPE | SNP_SYNC_ERROR_CMD_IND |
NP -> AP (N/A)
CMD 0 | CMD 1 |
---|---|
0x55 | 0x05 |
SNP_NPI_ASYNC_CMD_TYPE | SNP_EVENT_IND |
This indication packet will be send over TL if a unknown synchronous packet is send to the TL.
This indication is sent back to prevent TL lock up while waiting for a response.
NP -> AP
No Parameter Structure
In addition to the indication, SNP_EVENT_IND with SNP_ERROR_EVT will be sent to AP with faulting opcode in parameter structure.
NP -> AP
snpEvt_t
Size | Description |
---|---|
2 Byte | SNP_ERROR_EVT |
2 Byte | SNP Opcode which produced error |
1 Byte | Error Status list of status generated by the SNP. |