Generic Access Profile (GAP)

The GAP layer of the Bluetooth low energy protocol stack is responsible for connection functionality. This layer handles the access modes and procedures of the device including device discovery, link establishment, link termination, initiation of security features, and device configuration. See GAP State Diagram. for more details.

../_images/image72.jpeg

Figure 39. GAP State Diagram.

Based on the role for which the device is configured, GAP State Diagram. shows the states of the device. The following describes these states.

  • Standby: The device is in the initial idle state upon reset.
  • Advertiser: The device is advertising with specific data letting any initiating devices know that it is a connectible device (this advertisement contains the device address and can contain some additional data such as the device name).
  • Scanner: When receiving the advertisement, the scanning device sends a scan request to the advertiser. The advertiser responds with a scan response. This process is called device discovery. The scanning device is aware of the advertising device and can initiate a connection with it.
  • Initiator: When initiating, the initiator must specify a peer device address to which to connect. If an advertisement is received matching that address of the peer device, the initiating device then sends out a request to establish a connection (link) with the advertising device with the connection parameters described in Connection Parameters.
  • Slave/Master: When a connection is formed, the device functions as a slave if the advertiser and a master if the initiator.

Connection Parameters

This section describes the connection parameters which are sent by the initiating device with the connection request and can be modified by either device when the connection is established. These parameters are as follows:

  • Connection Interval - In Bluetooth low energy connections, a frequency-hopping scheme is used. The two devices each send and receive data from one another only on a specific channel at a specific time. These devices meet a specific amount of time later at a new channel (the link layer of the Bluetooth low energy protocol stack handles the channel switching). This meeting is where the two devices send and receive data is known as a connection event. If there is no application data to be sent or received, the two devices exchange link layer data to maintain the connection. The connection interval is the amount of time between two connection events in units of 1.25 ms. The connection interval can range from a minimum value of 6 (7.5 ms) to a maximum of 3200 (4.0 s). See Connection Event and Interval for more details.
../_images/image73.jpeg

Figure 40. Connection Event and Interval

Different applications may require different connection intervals. As described in Connection Parameter Considerations, these requirements affect the power consumption of the device. For more detailed information on power consumption, see Measuring Bluetooth Smart Power Consumption Application Report (SWRA478).

  • Slave Latency - This parameter gives the slave (peripheral) device the option of skipping a number of connection events. This ability gives the peripheral device some flexibility. If the peripheral does not have any data to send, it can skip connection events, stay asleep, and save power. The peripheral device selects whether to wake or not on a per connection event basis. The peripheral can skip connection events but must not skip more than allowed by the slave latency parameter or the connection fails. See Slave Latency for more details.
../_images/image74.jpeg

Figure 41. Slave Latency

  • Supervision Time-out - This time-out is the maximum amount of time between two successful connection events. If this time passes without a successful connection event, the device terminates the connection and returns to an unconnected state. This parameter value is represented in units of 10 ms. The supervision time-out value can range from a minimum of 10 (100 ms) to 3200 (32.0 s). The time-out must be larger than the effective connection interval (see Effective Connection Interval for more details).

Effective Connection Interval

The effective connection interval is equal to the amount of time between two connection events, assuming that the slave skips the maximum number of possible events if slave latency is allowed (the effective connection interval is equal to the actual connection interval if slave latency is set to 0).

The slave latency value represents the maximum number of events that can be skipped. This number can range from a minimum value of 0 (meaning that no connection events can be skipped) to a maximum of 499. The maximum value must not make the effective connection interval (see the following formula) greater than 16 s. The interval can be calculated using the following formula:

Effective Connection Interval = (Connection Interval) * (1 + [Slave Latency])

Consider the following example:

  • Connection Interval: 80 (100 ms)
  • Slave Latency: 4
  • Effective Connection Interval: (100 ms) * (1 + 4) = 500 ms

When no data is being sent from the slave to the master, the slave transmits during a connection event once every 500 ms.

Connection Parameter Considerations

In many applications, the slave skips the maximum number of connection events. Consider the effective connection interval when selecting or requesting connection parameters. Selecting the correct group of connection parameters plays an important role in power optimization of the Bluetooth low energy device. The following list gives a general summary of the trade-offs in connection parameter settings.

Reducing the connection interval does as follows:

  • Increases the power consumption for both devices
  • Increases the throughput in both directions
  • Reduces the time for sending data in either direction

Increasing the connection interval does as follows:

  • Reduces the power consumption for both devices
  • Reduces the throughput in both directions
  • Increases the time for sending data in either direction

Reducing the slave latency (or setting it to zero) does as follows:

  • Increases the power consumption for the peripheral device
  • Reduces the time for the peripheral device to receive the data sent from a central device

Increasing the slave latency does as follows:

  • Reduces power consumption for the peripheral during periods when the peripheral has no data to send to the central device
  • Increases the time for the peripheral device to receive the data sent from the central device

Connection Parameter Limitations with Multiple Connections

There are additional constraints that exist when connected to multiple devices or performing multiple GAP roles simultaneously. See the multi_role example in BLE-Stack 3.01.01.00.

Connection Parameter Update

In some cases, the central device requests a connection with a peripheral device containing connection parameters that are unfavorable to the peripheral device. In other cases, a peripheral device might have the desire to change parameters in the middle of a connection, based on the peripheral application. The peripheral device can request the central device to change the connection settings by sending a Connection Parameter Update Request. For Bluetooth 4.1 and 4.2-capable devices, this request is handled directly by the Link Layer. For Bluetooth 4.0 devices, the L2CAP layer of the protocol stack handles the request. The Bluetooth low energy stack automatically selects the update method.

This request contains four parameters: minimum connection interval, maximum connection interval, slave latency, and time-out. These values represent the parameters that the peripheral device needs for the connection (the connection interval is given as a range). When the central device receives this request, it can accept or reject the new parameters.

Sending a Connection Parameter Update Request is optional and is not required for the central device to accept or apply the requested parameters. Some applications try to establish a connection at a faster connection interval to allow for a faster service discovery and initial setup. These applications later request a longer (slower) connection interval to allow for optimal power usage.

Depending on the GAPRole, connection parameter updates can be sent asynchronously with the GAPRole_SendUpdateParam() or GAPCentralRole_UpdateLink() command. The peripheral GAPRole can be configured to automatically send a parameter update a certain amount of time after establishing a connection. For example, the simple_peripheral application uses the following preprocessor-defined symbols:

1
2
3
4
5
6
#define DEFAULT_ENABLE_UPDATE_REQUEST         GAPROLE_LINK_PARAM_UPDATE_INITIATE_BOTH_PARAMS
#define DEFAULT_DESIRED_MIN_CONN_INTERVAL     80
#define DEFAULT_DESIRED_MAX_CONN_INTERVAL     800
#define DEFAULT_DESIRED_SLAVE_LATENCY         0
#define DEFAULT_DESIRED_CONN_TIMEOUT          1000
#define DEFAULT_CONN_PAUSE_PERIPHERAL         6

Six seconds after a connection is established, the GAP layer automatically sends a connection parameter update. This action can be disabled by changing DEFAULT_ENABLE_UPDATE_REQUEST to e.g. GAPROLE_LINK_PARAM_UPDATE_WAIT_REMOTE_PARAMS. See Peripheral Role for an explanation of how the parameters are configured.

Connection Termination

Either the master or the slave can terminate a connection for any reason. One side initiates termination and the other side must respond before both devices exit the connected state.

GAP Abstraction

The application and profiles can directly call GAP API functions to perform Bluetooth low energy-related functions such as advertising or connecting. Most of the GAP functionality is handled by the GAPRole Task. GAP Abstraction shows this abstraction hierarchy.

../_images/image75.jpeg

Figure 42. GAP Abstraction

Access the GAP layer through direct calls or through the GAPRole task as described in GAPRole Task. Use the GAPRole task rather than direct calls when possible. Configuring the GAP Layer describes the functions and parameters that are not handled or configured through the GAPRole task and must be modified directly through the GAP layer.

Configuring the GAP Layer

The GAP layer functionality is mostly defined in library code. The function headers can be found in gap.h in the protocol stack project. Most of these functions are used by the GAPRole and do not need to be called directly. For reference, see BLE Stack API Reference (GATTServApp section). Several parameters exist which may be desirable to modify before starting the GAPRole. These parameters can be set or get through the GAP_SetParamValue() and GAP_GetParamValue() functions and include advertising and scanning intervals, windows, and so forth (see the API for more information). The following is the configuration of the GAP layer in simple_peripheral_init():

Listing 57. GAP configuration in simple_peripheral_init().
1
2
3
4
5
6
7
8
9
  // Set advertising interval
{
  uint16_t advInt = DEFAULT_ADVERTISING_INTERVAL;

  GAP_SetParamValue(TGAP_LIM_DISC_ADV_INT_MIN, advInt);
  GAP_SetParamValue(TGAP_LIM_DISC_ADV_INT_MAX, advInt);
  GAP_SetParamValue(TGAP_GEN_DISC_ADV_INT_MIN, advInt);
  GAP_SetParamValue(TGAP_GEN_DISC_ADV_INT_MAX, advInt);
}

The above code sets the advertising interval for limited and general advertising modes. By default, the peripheral advertises in general discoverable mode. To use limited discoverable mode, the corresponding fields inside the advertising data packet should be changed by defining DEFAULT_DISCOVERABLE_MODE to GAP_ADTYPE_FLAGS_LIMITED.