This section will explain how to adapt a BLE application from the SimpleLink CC2640R2 SDK to run on custom hardware. In general, the steps required to migrate a BLE application from a development kit to a custom board are minimal and involve changing the pin configuration as well as selecting the correct RF configuration. These steps, including a bring up guide, are detailed in the subsections below.

TI Provided Board Files

In order to make the SimpleLink CC2640R2 SDK‘s sample applications portable across different board and package types, a high level gateway file is used to select the proper board file based on the <board_type> predefined symbol. The top-level board file (board.c) then uses this symbol to include the correct board file into the project. This top-level board file can be found at <SDK_INSTALL_DIR>\source\ti\blestack\target\board.c, and is located under the Startup folder in the project workspace:

../_images/image178.jpeg

The board file links in another gateway board file located at <SDK_INSTALL_DIR>\source\ti\blestack\target\<kit_type>, which finally links in the actual board file from <SDK_INSTALL_DIR>\source\ti\boards\<board_type>.

<kit_type> indicates a handful of reference board files supported by the SimpleLink CC2640R2 SDK such as:

  • cc2640r2em
  • cc2640r2lp
  • cc2640r2rc

Warning

The <kit_type> is an intermediate step within the board gateway and will not need to be modified by the user while running on a TI EM or LP. Don’t try to set <kit_type> as a predefined symbol in your application.

The <board_type> define is set by the app project’s predefined symbols. The following defines are supported by the SimpleLink CC2640R2 SDK and refer to a reference design (EM or LaunchPad) created by TI.

By changing the define above, the application project will pull in a board file that is adopted for the TI reference designs or development kits with same name. Click the links above for more information on their respective TI reference designs.

Note

The CC2640R2F is pin compatible with the CC2650 and CC2640 wireless MCUs in equivalent QFN package sizes, so the above reference designs can be used when designing with the CC2640R2F.

Note that within the <board_name>.h file the symbol used to select the board’s RF front end configuration will be defined. See ble_user_config.h and Configuring the RF Front-End for Custom Hardware for more information on available RF front end configurations.

Package Type and Board Files

Most of the examples within the SimpleLink CC2640R2 SDK will run on the CC2640R2 Launchpad out of the box. Board files based on the TI CC26xx evaluation module (EM) reference designs are also provided for your convenience. (See TI Provided Board Files for more info) However, for custom hardware designs it may be necessary to modify the provided board files based on your selected package and RF configuration.

The board file for CC2640R2_LAUNCHXL is made for the 7x7 mm QFN package using differential RF front end and internal biasing. To convert this board file to use for other smaller device packages (5x5 mm and 4x4 mm QFN), the board file will need to be modified since limited number of IO pins are available in the smaller packages.

Note

It is recommended to start customizing board file(s) based on a reference design that is similar to your selected package type and RF configuration. For example a design for a 5x5 mm QFN package with a differential front end and external bias should use the CC2640R2DK_5XD board files as a reference.

See the datasheet for all the package options and IO descriptions: CC2640R2 Datasheet

For example, to change to the 4x4 package, remove all defines for all IOs not available (IOID_10 and higher) since the 4x4 package has only 10 DIO pins as listed in the datasheet.

The table below shows the number of GPIOs supported by each package:

Package Option Total GPIO Pins MAX IOID
7x7 mm QFN 31 IOID_30
5x5 mm QFN 15 IOID_14
4x4 mm QFN 10 IOID_9
2.7 x 2.7 mm WCSP 14 IOID_13

Creating a Custom Board File

TI-RTOS drivers rely on “board files” for their board-specific configuration parameters. The convention is to name these files based on the development kits provided by TI in addition to a generic Board.h with Board_* definitions to map the proper pins defined by ioc.h.

For example, for the simple_peripheral project, the following comprise the set of board files used by the CC2640R2 LaunchPad development kit:

Board.h CC2640R2_LAUNCHXL.h CC2640R2_LAUNCHXL.c

Note

simple_peripheral board files are located in <SDK_INSTALL_DIR>\source\ti\boards\CC2640R2_LAUNCHXL

TI recommends to start with the existing set of board files when porting a BLE application to custom development boards. When modifying or porting these board files, the user should consult with TI Driver APIs.

Tip

Board files provided by TI include TI-RTOS driver configuration data structures for various drivers. If the application does not use the associated TI-RTOS drivers, the linker will simply omit them from the application image.

The following steps provide guidance on customizing board files for a BLE-Stack 3.01.01.00 project.

  1. Duplicate existing board files from existing CC2640R2_LAUNCHXL board files.

    • These files can be found at: <SDK_INSTALL_DIR>\source\ti\boards\CC2640R2_LAUNCHXL
    • Create a copy of the CC2640R2_LAUNCHXL directory and give it a unique meaningful name for your development platform. In this example, we call it MYBOARD.

    Caution

    The SimpleLink CC2640R2 SDK also contains board files for TI-RTOS kernel and driver examples. These are not compatible with the BLE-Stack 3.01.01.00 because of differences in RF driver SWI priorities and custom drivers (e.g. TRNG) required by BLE-Stack 3.01.01.00. For BLE-Stack projects, use the files specified above for reference from simple_peripheral.

    • In the MYBOARD directory, rename CC2640R2_LAUNCHXL.c and CC2640R2_LAUNCHXL.h to their MYBOARD.c and MYBOARD.h respectively.
    • Search and replace all references of CC2640R2_LAUNCHXL with MYBOARD in Board.h, MYBOARD.c and MYBOARD.h.
  2. Add a new preprocessor define in your project’s board.c and board.h files.

    Continuing with the MYBOARD example, modify board.c and board.h in <SDK_INSTALL_DIR>\source\ti\target

    • Replace CC2640R2_LAUNCHXL by MYBOARD in your project’s application predefined symbols (See Accessing Preprocessor Symbols or Accessing Preprocessor Symbols)

    • In board.h, add a link to your Board.h file.

      1
      2
      3
      4
      #elif defined(CC2640R2_LAUNCHXL)
          #include "./cc2640r2lp/cc2640r2lp_board.h"
      #elif defined(MYBOARD)
          #include "../../boards/MYBOARD/Board.h"
      
    • In board.c, add the highlighted lines shown below:

      1
      2
      3
      4
      5
      #elif defined(CC2640R2_LAUNCHXL)
          #include "./cc2640r2lp/cc2640r2lp_board.c"
      #elif defined(MYBOARD)
          #include "../../boards/MYBOARD/Board.h"
          #include "../../boards/MYBOARD/MYBOARD.c"
      
    • Explicit references to CC2640R2_LAUNCHXL.h need to be replaced by MYBOARD.h

  3. Modify board files to match application requirements

Board Level Middleware

There are also several board driver files which are a layer of abstraction on top of TI-RTOS drivers, to function for a specific board, for example Board_key.c, or ExtFlash.c If desired, these files can be adapted to work for a custom board.

Using 32-kHz Crystal-Less Mode

BLE-Stack 3.01.01.00 includes support for operating the CC2640R2F in a 32-kHz crystal-less mode for peripheral and broadcaster (beacon) role configurations. By using the internal low-frequency RC oscillator (RCOSC_LF), the 32-kHz crystal can be removed from the board layout. By removing it you lower the bill of material (BOM) cost, reduce the required board space and simplify procurement. On the other hand, the current consumption will vary depending on the role of the device compared to when using the external 32-kHz crystal. More info in the SWRA499 Applicaion Note.

Note

Following project in the SDK already have a RCOSC build configuration:

  • simple_broadcaster
  • host_test
  • simple_np (SPI)
  • simple_peripheral

There are a few steps that must be taken into account to enable this feature. For any peripheral project, the following change is required for IAR. CCS users should see the Running Bluetooth Low Energy on CC2640 Without 32 kHz Crystal for the needed steps to enable RCOSC_LF in a project. You will find more detail regarding this feature in the aforementioned application note.

  1. Include rcosc_calibration.c, rcosc_calibration.h and ccfg_app_ble_rcosc.c files which locate at <SDK_INSTALL_DIR>\source\ti\blestack\common\cc26xx\rcosc

  2. Exclude ccfg_app_ble.c from build.

  3. Add USE_RCOSC to Defined symbols.

  4. Add the following code to your peripheral project.c

    Listing 82. RCOSC calibration include
    #ifdef USE_RCOSC
    #include "rcosc_calibration.h"
    #endif //USE_RCOSC
    
  5. Add the following code to your peripheral project_init function in peripheral project.c:

    Listing 83. RCOSC calibration enable
    #ifdef USE_RCOSC
    RCOSC_enableCalibration();
    #endif // USE_RCOSC
    
  6. If you are using a custom board file, enable the RCOSC in the power config. The board files included with the BLE-Stack:

    Listing 84. Power driver configuration
    PowerCC26XX_Config PowerCC26XX_config = {
      .policyInitFxn     = NULL,
      .policyFxn         = &PowerCC26XX_standbyPolicy,
      .calibrateFxn      = &PowerCC26XX_calibrate,
      .enablePolicy      = TRUE,
      .calibrateRCOSC_LF = TRUE,
      .calibrateRCOSC_HF = TRUE,
    };
    
  7. Constrain the temperature variation to be less than 1°C/sec. If the temperature is to change faster than 1°C/sec, then a short calibration interval must be used. Calibration interval can be tuned in rcosc_calibration.h

    Listing 85. RCOSCLF calibration interval
    // 1000 ms
    #define RCOSC_CALIBRATION_PERIOD   1000
    

Note

Use of the internal RCOSC_LF requires a sleep clock accuracy (SCA) of 500 ppm.

Configuring the RF Front-End for Custom Hardware

The CC2640R2F supports multiple RF front-end options to optimize performance or cost. Reference designs are available for multiple RF front-end options to aid in decoupling and RF layout. In order to achieve optimal sensitivity, it is important to configure the BLE application with the correct RF front-end setting used on the custom board. An incorrectly configured RF front-end may result in substantially degraded RF performance such as the inability to maintain a connection with a peer device. Configuration of the RF front-end is done within the board file.

For example, within the simple_peripheral project, the RF front-end configuration is defined in CC2640R2_LAUNCHXL.h with:

1
#define CC2650EM_7ID

The defined symbol is used in ble_user_config.h and ble_user_config.c to set the correct RF front-end mode, and the select the appropriate PA table for that configuration. In ble_user_config.h, CC2650EM_7ID is processed to define RF_FE_MODE_AND_BIAS:

 1
 2
 3
 4
 5
 6
 7
 8
 9
10
#define CC2650EM_7ID

// RF Front End Mode and Bias configuration

#if defined( CC26XX )

#if defined( CC2650EM_7ID )

#define RF_FE_MODE_AND_BIAS           ( RF_FE_DIFFERENTIAL |\
                                        RF_FE_INT_BIAS)

This configures the project to use a differential RF with internal bias. Other configurations can also be found in ble_user_config.h, select the configuration appropriate to your project.

In ble_user_config.c, CC2650EM_7ID selects the appropriate PA table, in this case for differential RF. For CC2640R2F, there are three PA tables; one for differential operation on QFN packages, one for single ended on QFN, and one for single ended on WCSP.

1
2
3
4
5
6
7
8
#elif defined( CC26XX )

  #if defined( CC2650EM_7ID ) || defined( CC2650EM_5XD ) || defined( CC2650M5A )

  // Differential Output

  // Tx Power Values (Pout, IB, GC, TC)
  const txPwrVal_t TxPowerTable[] =

Note

There are several other parameters being configured in ble_user_config. For CC2640R2F it is only the RF front-end mode and PA table that have to be changed for different boards.

For information on front ends and antenna configurations, see CC26xx RF FrontEnds and Antennas.

For information on other hardware considerations, see TI Bluetooth Low Energy Wiki.

Configuring Device Parameters for Custom Hardware

  1. Set parameters, such as the sleep clock accuracy of the 32.768-kHz crystal. See HCI_EXT_SetSCACmd()
  2. Define the CCFG parameters in ccfg_app_ble.c to enable or disable the ROM serial bootloader, JTAG access (DAP), flash protection, and so forth.

Note

For a description of CCFG configuration parameters, see the CC26xx Technical Reference Manual.

Initial Board Bring Up

When powering up a custom board with the CC2640R2F for the first time, it is recommended to complete the HW checklist items on the TI BLE Wiki. After confirming that the board is being powered correctly by the battery or power supply and can be identified by the JTAG tool, programming the device with a minimal SW application to verify stability is also suggested.

TI recommends using the simple_peripheral sample application for initial board bring up with modifications to the board file to:

  1. Disable all GPIO pin access
  2. Select the correct RF front end setting.

To disable all GPIO pin configuration, set the BoardGpioInitTable in the board file to PIN_TERMINATE:

1
2
3
4
const PIN_Config BoardGpioInitTable[] = {

    PIN_TERMINATE
};

The TI BLE-Stack does not require any GPIO pins to be configured in order to establish and maintain a BLE connection. Ensure that Display_DISABLE_ALL is defined in the application Predefined Symbols so that diagnostic logging data is not routed to any GPIO pin. If your custom board uses a different device configuration, such as the 32 kHz crystal-less RCOSC_LF configuration, be sure to make these device changes to the project. With this minimal application configuration you should be able to establish a BLE connection (e.g., with a smart phone or BTool) to your board at the expected range. If you are not able to complete this step, then it is likely there is a misconfiguration of the RF front end or you have other board related or layout issues. Refer to the hardware troubleshooting tips on the TI BLE Wiki.

After confirming that your board can maintain a BLE connection, you can now validate that your BLE application functions as expected on the custom board. Again, it is suggested to enable your GPIO pins one at a time in the board file and comment-out access to other GPIO pins in your application. If you do encounter a CPU exception (HWI abort) during this phase it is likely that a GPIO pin is incorrectly mapped in your custom board file or your application is attempting to access a GPIO pin that does not exist in your device package type.