Build date: 08142018
Compatibility Note
This release of VLIB contains libraries compiled using version
(8.2.4) of the C6000 DSP compiler,
whereas previous versions were using the version 7.4.2. Please refer to the
(compiler release notes)
for feature updates. One of the major differences between these two versions is
that version 7.x supported both COFF and ELF ABIs (both of which were delivered in
prior VLIB releases), but compiler version 8.x and beyond will only support ELF ABI.
Therefore, this version of VLIB only contains ELF libraries. TI recommends those
using COFF ABI refer to the (C6000 EABI Migration Guide)
to migrate their projects to use ELF. For those who need the bug fixes from this
release and can not migrate to ELF in the short term, you can download a version of
this release which includes the libraries compiled with the legacy compiler version 7.4.2
at the following https://software-dl.ti.com/libs/vlib/3_3_2_0-legacy/index_FDS.html.
| Title | Description | Size | |
|---|---|---|---|
| Vision Library (VLIB) Downloads | |||
| VLIB Documentation | |||
![]() |
VLIB_C64P_Function_Reference.chm | VLIB C64x+ Function Reference | 1488K |
![]() |
VLIB_C66_Function_Reference.chm | VLIB C66x Function Reference | 1728K |
![]() |
VLIB_C674_Function_Reference.chm | VLIB C674x Function Reference | 1488K |
![]() |
Software_Manifest.html | VLIB Software Manifest | 16K |
| C66x VLIB (little-endian) | |||
![]() |
vlib_c66x_obj_3_3_2_0_Win32.exe | VLIB for C66x Windows Installer | 15896K |
![]() |
vlib_c66x_obj_3_3_2_0_Linux.bin | VLIB for C66x Linux Installer | 15728K |
| C64x+ VLIB (little-endian) | |||
![]() |
vlib_c64Px_obj_3_3_2_0_Win32.exe | VLIB for C64x+ Windows Installer | 13236K |
![]() |
vlib_c64Px_obj_3_3_2_0_Linux.bin | VLIB for C64x+ Linux Installer | 13072K |
| C674x VLIB (little-endian) | |||
![]() |
vlib_c674x_obj_3_3_2_0_Win32.exe | VLIB for C674x Windows Installer | 13232K |
![]() |
vlib_c674x_obj_3_3_2_0_Linux.bin | VLIB for C674x Linux Installer | 13068K |
| Checksums | |||
| MD5 Checksums | 4K | ||
Fill in Form. Approved users receive download URL in 1 minute.
Fill in Form. TI will contact you in 1-2+ business days.