![]() |
TIOVX User Guide
|
Meaning of terms in the following tables,
This table lists the mapping of standard OpenVX kernels to compute targets on the Jacinto7 platform. When mapped to C66x DSP, it indicates if it is implemented using BAM DMA acceleration, or cache only.
All of the below kernels default to running on the C66x DSP 1. If a different target is needed, it can be selected from the available targets indicated below by using the vxSetNodeTarget() API.
| Kernel | C66x 1 | C66x 2 | HWA | PC Emulation Support |
|---|---|---|---|---|
| Absolute Difference | Cache | Cache | Yes | |
| Accumulate | Cache | Cache | Yes | |
| Accumulate Squared | Cache | Cache | Yes | |
| Accumulate Weighted | Cache | Cache | Yes | |
| Arithmetic Addition | Cache | Cache | Yes | |
| Arithmetic Subtraction | Cache | Cache | Yes | |
| Bitwise AND | Cache | Cache | Yes | |
| Bitwise EXCLUSIVE OR | Cache | Cache | Yes | |
| Bitwise INCLUSIVE OR | Cache | Cache | Yes | |
| Bitwise NOT | Cache | Cache | Yes | |
| Box Filter | Cache | Cache | Yes | |
| Canny Edge Detector | Cache | Cache | Yes | |
| Channel Combine | Cache | Cache | Yes | |
| Channel Extract | Cache | Cache | Yes | |
| Color Convert | Cache | Cache | Yes | |
| Convert Bit depth | Cache | Cache | Yes | |
| Custom Convolution | Cache | Cache | Yes | |
| Dilate Image | Cache | Cache | Yes | |
| Equalize Histogram | Cache | Cache | Yes | |
| Erode Image | Cache | Cache | Yes | |
| Fast Corners | Cache | Cache | Yes | |
| Gaussian Filter | Cache | Cache | Yes | |
| Non Linear Filter | Cache | Cache | Yes | |
| Harris Corners | Cache | Cache | Yes | |
| Histogram | Cache | Cache | Yes | |
| Gaussian Image Pyramid | Cache | Cache | VPAC_MSC* | Yes |
| Laplacian Image Pyramid | Cache | Cache | Yes | |
| Reconstruction from a Laplacian Image Pyramid | Cache | Cache | Yes | |
| Integral Image | Cache | Cache | Yes | |
| Magnitude | Cache | Cache | Yes | |
| Mean and Standard Deviation | Cache | Cache | Yes | |
| Median Filter | Cache | Cache | Yes | |
| Min, Max Location | Cache | Cache | Yes | |
| Optical Flow Pyramid (LK) | Cache | Cache | Yes | |
| Phase | Cache | Cache | Yes | |
| Pixel-wise Multiplication | Cache | Cache | Yes | |
| Remap | Cache | Cache | Yes | |
| Scale Image | Cache | Cache | VPAC_MSC* | Yes |
| Sobel 3x3 | Cache | Cache | Yes | |
| TableLookup | Cache | Cache | Yes | |
| Thresholding | Cache | Cache | Yes | |
| Warp Affine | Cache | Cache | Yes | |
| Warp Perspective | Cache | Cache | Yes |
Note: the below node implementation locations have changed from the 8.6 to 9.0 releases. The new locations can be referenced in Directory Structure document.
| Kernel | Target | Remote Core(s) | PC Emulation Support |
|---|---|---|---|
| tivxCaptureNode | CSIRX | MCU2_0 | No |
| tivxDisplayNode | DSS | MCU2_0 | No |
| tivxTIDLNode | C7x + MMA | C7X_1 | Yes |
| tivxVpacVissNode | VPAC_VISS | MCU2_0 | Yes |
| tivxVpacLdcNode | VPAC_LDC | MCU2_0 | Yes |
| tivxVpacNfGenericNode | VPAC_NF | MCU2_0 | Yes |
| tivxVpacNfBilateralNode | VPAC_NF | MCU2_0 | Yes |
| tivxVpacMscScaleNode | VPAC_MSC | MCU2_0 | Yes |
| tivxVpacMscPyramidNode | VPAC_MSC | MCU2_0 | Yes |
| tivxVpacFcVissMscNode | VPAC_FC | MCU2_0 | Yes |
| tivxDmpacSdeNode | DMPAC_SDE | MCU2_1 | Yes |
| tivxDmpacDofNode | DMPAC_DOF | MCU2_1 | Yes |
| tivxCsitxNode | CSITX | MCU2_0 | Yes |
| tivxDisplayM2MNode | DSS | MCU2_0 | Yes |
| tivxObjArraySplitNode | MPU / MCU2_0 | A72 / MCU2_0 | Yes |