8. Frequently Asked QuestionsΒΆ
- 8.1. FAQ - Common
- 8.2. FAQ - CAN
- 8.3. FAQ - FVID2
- 8.4. FAQ - C7x : Steps to switch C7x SysBIOS application from secure mode to non-secure mode
- 8.4.1. Introduction
- 8.4.2. Step 1: SysBIOS config file changes to enable boot to non-secure
- 8.4.3. Step 2: Linker command file changes
- 8.4.4. Step 3: MMU initialization to setup secure and non-secure MMU tables
- 8.4.5. Step 4: CLEC initialization to allow non-secure mode access
- 8.4.6. Step 5: Cache initialization to partition L1/L2 as cache vs RAM
- 8.4.7. Step 6: Sciclient init to use non-secure mode
- 8.4.8. Step 7: Build and run
- 8.5. FAQ - Used Resources - Interrupt
- 8.6. FAQ - Supported Cores by example applications
- 8.7. FAQ - How to set the clock for a given module and clock
- 8.8. FAQ - Running Apps on secure devices
- 8.9. FAQ - CSI2RX