Product Release Notes
Table of Contents
Introduction
This is the release notes for mcusw 11.01.00 release, produced on 2025-08-22. The MCUSW package consists of MCAL Driver & Demos/Applications for J721E/J7200/J721S2/J784S4/J742S2 family of devices. The MCAL modules are compliant to AUTOSAR specification versioned 4.3.1 .
Licensing
Refer to Processor SDK Automotive manifest at top level and MCUSW Manifest for MCUSW Manifest.
Getting Started
The MCUSW User Guide provides the documentation and references necessary to begin development on TI’s platforms using MCUSW
Documentation
MCUSW User Guide: This document details Supported driver, Installation, Dependencies, Build instructions, Steps to run example applications, Module Specific User Guides, API Guide, Test Reports, Design Document and others.
MCUSW Configurator User Guide: Refer this before attempting to reconfigure MCAL modules. This include steps to Install Configurator (EB), Configurator Licensing, Generation of MCAL Configurations and others.
Dependencies
List of items needs along with MCUSW Package:
Configurator package contains following items:
Configurator package is released as a secure resource. Please contact TI represtative to get access for same. Refer user guide for detailed steps of installing and using the configurator package.
What’s New
New features supported in this release:
- Several Fixed Defects.
- Multi-flash support features
Compatibility
IMPORTANT NOTE: User should ensure to use below modules version for MCUSW_J7_11.01.00 release. User should take care to not mis-match or mix-and-match the versions with various MCUSW releases. Bundle Version of all plugins is 11.1.0.
Module | Previous Module Verson | Current Module Version | Remarks |
---|---|---|---|
ADC | 9.2.0 | 9.2.0 | None |
CAN | 10.2.0 | 10.2.1 | Patch version Update |
CDD IPC | 11.2.0 | 11.3.0 | Minor version Update |
DIO | 10.1.0 | 10.1.0 | None |
GPT | 9.2.0 | 9.2.1 | Patch version Update |
ICU | 9.1.0 | 9.1.0 | None |
PWM/EPWM | 11.1.0 | 11.1.0 | None |
MCU | 10.0.0 | 10.1.1 | Minor and Patch Version Update |
SPI | 9.2.0 | 9.2.1 | Patch version Update |
FLS | 11.1.0 | 12.0.0 | Major Version Update |
WDG | 9.1.0 | 9.1.0 | None |
ETH | 11.0.0 | 11.0.0 | None |
ETH TRCV | 11.0.0 | 11.0.0 | None |
OS | 9.0.1 | 9.0.1 | None |
EcuM | 9.0.0 | 9.0.0 | None |
DEM | 9.0.0 | 9.0.0 | None |
Device Support
Supported SoCs: J721E & J721S2 & J7200 & J784S4 & J742S2
Validation
This release was built and validated using the following tools.
Build Tools (included in Processor SDK)
ti-cgt-armllvm_4.0.1.LTS
Fixed Defects
ID | Summary |
---|---|
MCAL-30607 | WDG: Watchdog Reaction set as non configurable parameter in Configurator |
MCAL-31713 | GPT: Invalid allocation of Gpt_ChannelStateType size to channelWakeupEnFlag |
MCAL-31670 | SPI: Wrong selection of external id in spi _copyconfig API |
MCAL-31473 | IPC: CDD IPC control message boundary check is invalid |
MCAL-31460 | SPI: Duplicate container for SpiDemEventParameterRefs in epd file |
MCAL-31459 | MCU: Max value for McuResetReason is 3 in arxml file but default value supports higher value for reset reason |
MCAL-31458 | FLS: Duplicate short-name and default-values tags in epd file |
MCAL-31457 | IPC: Use of int32_t for prototype definition in CDD_IPC |
MCAL-30733 | CAN: Wrong base address in Can_RegisterReadback API |
MCAL-30470 | MCAN: MCAN module of MCAL has undefined register initialization |
MCAL-29774 | FLS: DET reported by Fls_Erase when not aligned with NOR_BLOCK_SIZE |
MCAL-29484 | IPC: In IPC,endpoint requested is greater than 256 error needs to be reported |
MCAL-28234 | IPC: RPMessage_enqueMsg() handles incoming messages twice, first queue is ignored. |
MCAL-27141 | MCU: Mcu_PerformSoftSysReset API doesn't perform soft system reset |
Known Limitations
None
Support
For technical support and additional assistance, visit E2E or contact local TI Field Application Engineer.