Demo Configuration file

The demo config file uses YAML format to define input sources, models, outputs and finally the flows which defines how everything is connected. Config files for out-of-box demos are kept in edge_ai_apps/configs folder. The folder contains config files for all the use cases and also multi-input and multi-inference case. The folder also has a template YAML file app_config_template.yaml which has detailed explanation of all the parameters supported in the config file.

Config file is divided in 4 sections:

  1. Inputs

  2. Models

  3. Outputs

  4. Flows

Inputs

The input section defines a list of supported inputs like camera, filesrc etc. Their properties like shown below.

inputs:
    input0:                                     #Camera Input
        source: /dev/video2                     #Device file entry of the camera
        format: jpeg                            #Input data format suported by camera
        width: 1280                             #Width and Height of the input
        height: 720
        framerate: 30                           #Framerate of the source

    input1:                                     #Video Input
        source: ../data/videos/video_0000.mp4   #Video file
        width: 1280
        height: 720
        framerate: 25

    input2:                                     #Image Input
        source: ../data/images/%04d.jpg         #Sequence of Image files, printf style formatting is used
        width: 1280
        height: 720
        index: 0                                #Starting Index (optional)
        framerate: 1

All supported inputs are listed in template config file. Below are the details of most commonly used inputs.

Camera sources (v4l2)

v4l2src GStreamer element is used to capture frames from camera sources which are exposed as v4l2 devices. In Linux, there are many devices which are implemented as v4l2 devices. Not all of them will be camera devices. You need to make sure the correct device is configured for running the demo successfully.

Run the following command to decide the right device to be used:

root@j7-evm:/opt/edge_ai_apps# gst-device-monitor-1.0 Video | grep "name\|device.path"
    name  : UVC Camera (046d:0825)
            device.vendor.name = 046d
            device.product.name = "UVC\ Camera\ \(046d:0825\)"
            device.path = /dev/video2
    name  : UVC Camera (046d:0825)
            device.vendor.name = 046d
            device.product.name = "UVC\ Camera\ \(046d:0825\)"
            device.path = /dev/video4
    name  : j721e-csi2rx
            device.product.name = j721e-csi2rx
            device.path = /dev/video1

From the above log we can determine that 2 USB cameras are connected (/dev/video2, /dev/video4), and 1 CSI camera is connected (/dev/video1) camera is connected. You can also remove grep filters in the command to see more details about the devices.

Using this method, you can configure correct device for camera capture in the input section of config file.

input0:
    source: /dev/video2  #USB Camera
    format: jpeg         #if connected USB camera supports jpeg
    width: 1280
    height: 720
    framerate: 30

input1:
    source: /dev/video1  #CSI Camera
    format: auto         #let the gstreamer negotiate the format
    width: 1280
    height: 720
    framerate: 30

Make sure to configure correct format for camera input. jpeg for USB camera that supports (Ex. C270 logitech USB camera).

Video sources

H.264 encoded videos can be provided as input sources to the demos. A sample video file is provided under /opt/edge_ai_apps/data/videos/video_0000.mp4

input1:
    source: ../data/videos/video_0000.mp4
    width: 1280
    height: 720
    framerate: 25

Image sources

JPEG compressed images can be provided as inputs to the demos. A sample set of images are provided under /opt/edge_ai_apps/data/images. The names of the files are numbered sequentially and incrementally and the demo plays the files at the fps specified by the user.

input2:
    source: ../data/images/%04d.jpg
    width: 1280
    height: 720
    index: 0
    framerate: 1

RTSP sources

H.264 encoded video streams either coming from a RTSP compliant IP camera or via RTSP server running on a remote PC can be provided as inputs to the demo.

input0:
    source: rtsp://172.24.145.220:8554/test # rtsp stream url, replace this with correct url
    width: 1280
    height: 720
    framerate: 30

Note

Usually video streams from any IP camera will be encrypted and cannot be played back directly without a decryption key. We tested RTSP source by setting up an RTSP server on a Ubuntu 18.04 PC by refering to this writeup, Setting up RTSP server on PC

Models

The model section defines a list of models that are used in the demo. Path to the model directory is a required argument for each model and rest are optional properties specific to given use cases like shown below.

models:
    model0:
        model_path: ../models/segmentation/ONR-SS-871-deeplabv3lite-mobv2-cocoseg21-512x512   #Model Directory
        alpha: 0.4                                                                            #alpha for blending segmentation mask (optional)
    model1:
        model_path: ../models/detection/TFL-OD-202-ssdLite-mobDet-DSP-coco-320x320
        viz_threshold: 0.3                                                                    #Visualization threshold for adding bounding boxes (optional)
    model2:
        model_path: ../models/classification/TVM-CL-338-mobileNetV2-qat
        topN: 5                                                                               #Number of top N classes (optional)

Below are some of the use case specific properties:

  1. alpha: This determines the weight of the mask for blending the semantic segmentation output with the input image alpha * mask + (1 - alpha) * image

  2. viz_threshold: Score threshold to draw the bounding boxes for detected objects in object detection. This can be used to control the number of boxes in the output, increase if there are too many and decrease if there are very few

  3. topN: Number of most probable classes to overlay on image classification output

The content of the model directory and its structure is discussed in detail in Import Custom Models

Outputs

The output section defines a list of supported outputs.

outputs:
    output0:                                                     #Display Output
        sink: kmssink
        width: 1920                                              #Width and Height of the output
        height: 1080
        connector: 39                                            #Connector ID for kmssink (optional)

    output1:                                                     #Video Output
        sink: ../data/output/videos/output_video.avi             #Output video file
        width: 1920
        height: 1080

    output2:                                                     #Image Output
        sink: ../data/output/images/output_image_%04d.jpg        #Image file name, printf style formatting is used
        width: 1920
        height: 1080

All supported outputs are listed in template config file. Below are the details of most commonly used outputs

Display Sink (kmssink)

When you have only one display connected to the EVM, kmssink will try to use it for displaying the output buffers. In case you have connected multiple display monitors (e.g. Display Port and HDMI), you can select a specific display for kmssink by passing a specific connector ID number. Following command finds out the connected displays available to use.

Note: Run this command outside docker container. The first number in each line is the connector-id which we will use in next step.

root@j7-evm:/opt/edge_ai_apps# modetest -M tidss -c | grep connected
39      38      connected       DP-1            530x300         12      38
48      0       disconnected    HDMI-A-1        0x0             0       47

From above output, we can see that connector ID 39 is connected. Configure the connector ID in the output section of the config file.

Video sinks

The post-processed outputs can be encoded in H.264 format and stored on disk Please specify the location of the video file in the configuration file.

output1:
    sink: ../data/output/videos/output_video.avi
    width: 1920
    height: 1080

Image sinks

The post-processed outputs can be stored as JPEG compressed images. Please specify the location of the image files in the configuration file. The images will be named sequentially and incrementally as shown.

output2:
    sink: ../data/output/images/output_image_%04d.jpg
    width: 1920
    height: 1080

Flows

The flows section defines how inputs, models and outputs are connected. Multiple flows can be defined to achieve multi input, multi inference like below.

flows:
    flow0:                              #First Flow
        input: input0                   #Input for the Flow
        models: [model1, model2]        #List of models to be used
        outputs: [output0, output0]     #Outputs to be used for each model inference output
        mosaic:                         #Positions to place the inference outputs in the output frame
            mosaic0:
                width:  800
                height: 450
                pos_x:  160
                pos_y:  90
            mosaic1:
                width:  800
                height: 450
                pos_x:  960
                pos_y:  90
    flow1:                              #Second Flow
        input: input1
        models: [model0, model3]
        outputs: [output0, output0]
        mosaic:
            mosaic0:
                width:  800
                height: 450
                pos_x:  160
                pos_y:  540
            mosaic1:
                width:  800
                height: 450
                pos_x:  960
                pos_y:  540

Each flow should have exactly 1 input, n models to infer the given input and n outputs to render the output of each inference. Along with input, models and outputs it is required to define n mosaics which are the position of the inference output in the final output plane. This is needed because multiple inference outputs can be rendered to same output (Ex: Display).

Command line arguments

Limited set of command line arguments can be provided, run with ‘-h’ or ‘–help’ option to list the supported parameters.

usage: Run : ./app_edgeai.py -h for help

positional arguments:
  config           Path to demo config file
                       ex: ./app_edgeai.py ../configs/app_config.yaml

optional arguments:
  -h, --help       show this help message and exit
  -n, --no-curses  Disable curses report
                   default: Disabled
  -v, --verbose    Verbose option to print profile info on stdout
                   default: Disabled