|
|
The release components in this version is based on TI Linux kernel and hostap package.
Below you can find the full list of patches applied on top of these sources.
Linux Kernel baseline is located in git://git.ti.com/ti-linux-kernel/ti-linux-kernel.git
This release is based on ti2016.00-int tag <ref>
Commit | Description |
---|---|
13c25bc | Revert “wl18xx/wlcore : time sync demo [TMP]” |
517c7c0 | Revert “mmc: Wait for card_busy before starting sdio requests” |
22544cf | Arp Filtering: Add protection against null ip address |
3a17b90 | AP-WoW: Fix ap stop warn on [SQUASH] |
2715d52 | wlcore/wl18xx: add radar_debug_mode handling |
76002c6 | mac80211: Add support for aborting an ongoing scan |
249e81c | cfg80211: Add support for aborting an ongoing scan |
3c4b0aa | AP WoW: Fix bug where we configure wrong IP after recovery. |
7f9c7bc | mesh: max_peers reached falsely |
e2408bf | wlcore/wl12xx: Fix fw logger over sdio |
231fda8 | Revert “Revert”wlcore: Fix regression in wlcore_set_partition()“” |
55f5805 | Revert “wlcore: Fix regression in wlcore_set_partition()” |
9356957 | wlcore: remove timestamp strings prints |
b8e49e1 | wlcore: add version and timestamp strings (INTERNAL) |
a232820 | Revert “tcp: refine pacing rate determination” [WORAROUND]. |
59ba261 | wlcore: Fix regression in wlcore_set_partition() |
2b1d59b | wlcore: fix error handling in wlcore_event_fw_logger |
be4e2a8 | wlcore/wl18xx: fw logger over sdio |
aa4dc8c | WoW: Add WoW when acting as AP. fixes #WILINK8_SW_DEV-506 |
3959c20 | bbb:dts: update wilink8 capes to the latest version |
b3fdb01 | dts:am335x-evm-wow : update dtb with latest changes |
2a92d0a | dts :am335x-evm-wow: update dts file with latest changes |
10ff29a | wl18xx: multi-role AP & GO doesn’t work |
bf20836 | mesh: mesh is not connected properly after recovery |
84bf225 | mesh: frames received out of order |
c4baf3d | mesh: path selection improvements |
ea59734 | mesh: TO is always enabled. Only targets responmd to Originator |
30ebf70 | mesh: PREQs will be forwarded by a Destination MP |
118c1f3 | mac80211: Unify mesh and mpp path removal function |
e9603cd | mac80211: let unused MPP table entries timeout |
e5ed0f1 | mac80211: Remove MPP table entries with MPath |
5a3077f | mac80211: mesh: drop constant field mean_chain_len |
208eaa5 | mac80211: mesh_plink: remove redundant sta_info check |
77fb7a4 | mesh : proactive path selection improvements |
8aef43f | mesh: update path table only with better PREQ path to next hop |
8f42398 | mesh : PREQ: increase the PREQ lifetime to imporve performance |
3d8c110 | mesh: increase PREQ/PRES action frames reliability |
eb86de3 | Mesh: bypass blockack encryption [WORKAROUND] |
7578101 | mac80211: mesh: fixed HT ies in beacon template |
c50dda0 | mac80211: mesh: fix call_rcu() usage |
541e192 | mesh: delayed path reply |
b9c70b6 | mesh: Fix healing time when a mesh peer is disconnecting |
47f313b | mesh: implement mac80211 op: get_rate_info |
2c55c2a | mesh: support mesh metric calculation |
7d8bade | mesh: mac80211 opcode, get rate for metric from driver |
e326667 | ieee80211: mesh: handle secured PREQ frames |
05eb4a7 | wlcore: mesh: Add support for RX Boradcast Key |
d71cd1c | mac80211: mesh: flush stations before beacons are stopped |
efbc0a4 | wl18xx: firmware minor version update |
be44d03 | mesh: added initial mesh support for wl8 |
4a10364 | wl18xx/wlcore : time sync demo [TMP] |
db720d4 | wlcore: mesh: add zone time sync support |
5331cc5 | am335x-evm : add support Wake on Wlan for EVM |
cbd9f24 | am335x-bone : add support for different wilink8 capes for BBB |
hostap baseline is located in http://w1.fi/cgit/hostap/
This release is based on 235c56e7 commit
Commit | Description |
---|---|
2f81a83 | mesh on demand: Several fixes |
ec433fc | mesh on demand: Allow BG scan user configuration (tag: R8.7_RC14) |
0bfdbd1 | Fix deauth with reason 7 due to multiple assoc_req received |
3c033f6 | ap: add missing WLAN_STA_ASSOC_REQ_OK flag cleanups |
b82d28a | mesh on demand: Perform BG Scan only on serving channel |
54762b1 | mesh: Cannot perform scan on mesh IF while mesh is connected with security |
3e26762 | Mesh: Fixed max peer links |
03a57ad | Mesh: Don’t allow SISO40 pri/sec channel switch |
7cb82c8 | Mesh: Cannot create mesh network on channel 40 |
a79621c | Mesh: Can’t join other mesh network after joining mesh network |
b42b713 | Mesh: mesh on demand support |
a1651f7 | Mesh: bug fix - make sure when we disconnect we wait for plink_close to be received |
c030add | mesh: fix error print upon join |
8a96e36 | AP-Mesh channel sync |
012bb3a | mesh : set OFDM basic rates as default |
21df09b | Mesh: Connection fixes |
eb51e3c | Mesh: max peer parameter doesn’t work |
18b7bcb | mesh: enable disassoc_low_ack event for mesh |
9c760d6 | P2P: accept provision discovery with bcast group ID [IOP] |
0779f3b | P2P: accommodate peers that use the GO address in prov_disc_resp [IOP] |
20e8adb | P2P: Ignore PBC overlap in P2P provisioning [IOP] |
5f6bc58 | wpa_supplicant: declare 20/40 coex support [UPSTREAM] |
6b64367 | P2P: increase p2p go initial connection timeout [WORKAROUND] |
45a25ee | reload iface on ifdown/up and suspend/resume (INTERNAL) |
d818ecf | Smart config :provisioning solution |
1231b05 | ACS: don’t choose JP-only channel [ACS] |
badb9fa | ap: wps: avoid sending wps commands for each interface [AP AP] |
94594ef | acs: retry ACS scan on EBUSY return code [ACS] |
1e37781 | hostap: don’t check scan results in case of 20mhz [AP AP] |
ac061d6 | driver_nl80211: implement shared AP channel op [AP AP] |
a4c16c4 | hostapd: use new op to sync AP channels [AP AP] |
de8390a | acs: skip HT_SCAN on channel sync [ACS] |
3ea4f6b | acs: add additional dfs operating classes [ACS] |
3777dd4 | acs: Porting legacy ACS solution [ACS] |
2508508 | hostapd: sync channel on interface setup [AP AP] |
5a5cf33 | hostapd: add hostapd.conf param to force AP channel sync [AP AP] |
2f56fbd | P2P: dont consider p2p_ignore_shared_freq in case of running ap [INTERNAL, AP P2P] |
05ff2d5 | p2p: prefer shared freq for GO operation [INTERNAL, AP P2P] |
ab4728c | dfs: skip some channels [INTERNAL, REG] |
a3a9573 | ap: explicitly disable some channels from country IE [INTERNAL, REG] |
ea0ab60 | changes to default build config |