SimpleLink™ MSP432 WiFi Plugin SDK 1.30.00.03 Release Notes
Table of Contents
Introduction
This is version 1_30_00_03 of SimpleLink™ MSP432 WiFi Plugin.
SimpleLink™ SDK Plugins are designed to work in tandem to a microprocessor specific SDK. This plugin is designed to work alongside the SimpleLink MSP432 SDK 1.30.00.40 and relies on several core elements within this SDK. Without a prior installation of the SimpleLink MSP432 SDK 1.30.00.40, the SimpleLink MSP432 SDK WiFi Plugin will not work.
The SimpleLink™ Wi-Fi® CC3120 device is part of the new SimpleLink™ Wi-Fi® family that dramatically simplifies the implementation of Internet connectivity. The CC3120 device integrates all protocols for Wi-Fi and Internet, which greatly minimizes host MCU software requirements. With built-in security protocols, the CC3120 solution provides a robust and simple security experience.
The Wi-Fi network processor subsystem features a Wi-Fi Internet-on-a-Chip and contains an additional dedicated ARM MCU that completely offloads the host MCU. This subsystem includes an 802.11 b/g/n radio, baseband, and MAC with a powerful crypto engine for fast, secure Internet connections with 256-bit encryption. The CC3120 device supports Station, Access Point, and Wi-Fi Direct modes. The device also supports WPA2 personal and enterprise security and WPS 2.0. This subsystem includes embedded TCP/IP and TLS/SSL stacks, HTTP server, and multiple Internet protocols.
Content and Documentation
The SimpleLink CC3120 is comprised of several components that can be used together.
Component | Source Directory | Documentation |
---|---|---|
SimpleLink Wi-Fi host driver | source\ti\drivers\net\wifi |
API guide |
Release_Notes | ||
NWP Service Pack | tools\cc31xx_tools\servicepack-cc3x20 |
Release_Notes |
Root Certificate Catalog | tools\cc31xx_tools\certificate-catalog |
Readme |
Root Certificate Playground | tools\cc31xx_tools\certificate-playground |
Readme |
Networking demo applications
RTOS:
Demo | Source Directory | Documentation |
---|---|---|
Cloud OTA | examples\rtos\MSP_EXP432P401R\demos\cloud_ota |
Readme |
Local OTA | examples\rtos\MSP_EXP432P401R\demos\local_ota |
Readme |
Power measurement | examples\rtos\MSP_EXP432P401R\demos\power_measurement |
Readme |
Provisioning | examples\rtos\MSP_EXP432P401R\demos\provisioning |
Readme |
Network Terminal | examples\rtos\MSP_EXP432P401R\demos\network_terminal |
Readme |
- Peripherals drivers examples can be found under the core SDK (MSP432 SDK).
Documentation
What’s New
- Improved IAR user experience - Projects and Workspaces are provided for IAR examples in addition to project connections.
- IAR RTOS config is pre-built automatically when user builds an RTOS based IAR example.
- TI Resource Explorer support.
- Support for CCS 7.1
- Support for IAR EWARM 7.80.3
- Upgraded packaged XDCTools to 3.50.01.12
Updating service-pack
It is recommended to update the service-pack to the latest service-pack available. The service-pack can be found in <SDK_INSTALL_DIR>/tools/cc31xx_tools/servicepack-cc3x20
For more information please follow the instructions in the Quick start Guide
Upgrade and Compatibility Information
CC3120 SimpleLink Wi-Fi Network Processor and CC3220 SimpleLink Wireless MCU are the second generation devices in the SimpleLink Wi-Fi and Internet-of-Things family. The Migration Guide intends to guide users who already have experience with the CC3100/CC3200 devices and need to port their software to the new CC3120/CC3220 family of devices. The document describes the new SDK structure and highlights the software components that require attention including host driver, OS layers, board drivers, and external libraries.
Host Support
- Windows 7, Windows 8
- Ubuntu
- Mac OS X
Dependencies
This release requires the following other software components and tools.
- SimpleLink MSP432 SDK 1.30.00.40
- CCS 7.1.0 Release page
- XDCTools 3.50.01.12 or higher
- TI Code Generation Tools
- ARM version 16.9.1 LTS or later
- GNU Code Generation Tools
- ARM gcc-arm-none-eabi-4_9-2015q3 Release page
- IAR Code Generation Tools
- ARM 7.80.3 Release page
Validation Information
- Code Composer Studio 7.1.0 Release page
- ARM version 16.9.1 LTS
- XDCTools 3.50.01.12
- GNU Code Generation Tools
- ARM gcc-arm-none-eabi-4_9-2015q3 Release page
- IAR Code Generation Tools
- ARM 7.80.3 Release page
Fixed Issues
ID | Summary |
---|---|
None | None |
Known Issues
ID | Summary |
---|---|
None | None |
- When using FreeRTOS a patch is required:
- Download FreeRTOS official version 9 - www.freertos.org
- Install the software under
c:
- TI Resource Explorer integration is not supported.
Versioning
This product’s version follows a version format, M.mm.pp.bb, where M is a single digit Major number, mm is 2 digit minor number, pp is a 2 digit patch number, and b is an unrestricted set of digits used as an incrementing build counter.
Technical Support and Product Updates
- Visit the E2E Forum