Release Notes

Table of Contents

Introduction

This is a GA release of the Core SDK 4.40.00.03 for CC32xx devices.

Documentation

Open the documentation overview web page file in the SDK’s Doc folder for a full list of documentation.

What’s New

Upgrade and Compatibility Information

This release breaks compatibility with previous releases of the Core SDK in the following ways:

IAR RTOS plugin .dll

The ROV tool for IAR requires an update to work properly. If you are an ROV user, follow the instructions on this forum page: https://e2e.ti.com/support/processors/f/791/t/832561. If you don’t use ROV, you can proceed with the standard debugging sessions. The ROV tool does not affect any other funcationality.

Host Support

See the SDK release notes for a description of which host operating systems are supported in this release.

Dependencies

See the SDK release notes for a description of which components and tools are required to work with this product.

Device Support

See the SDK release notes for a list of TI devices that are supported in this product.

Validation Information

The Core SDK was validated with the following components:

Known Issues

ID Summary
TIDRIVERS-3636 I2C_transfer() occasionally fails when called from an interrupt context
TIDRIVERS-1806 CC32xx SD driver does not work reliability on some SD cards
TIDRIVERS-1642 NVSSPI25x driver does not work when using internal SPI CS

Versioning

This product’s version follows a version format, M.mm.pp.bb, where M is a single digit Major number, mm is 2 digit minor number, pp is a 2 digit patch number, and b is an unrestricted set of digits used as an incrementing build counter.

Prior Release Changes

A summary of changes made in previous releases of this product can be found in the product Change Log