TitleRelease Notes - SimpleLink Wi-Fi CC3235 service pack

Table of Contents

Introduction

The SimpleLink™ Wi-Fi® CC3235 device is a single-chip micro-controller (MCU) with built-in Wi-Fi connectivity, created for the Internet of Things (IoT). The CC3235 device is a wireless MCU that integrates a high-performance ARM® Cortex®-M4 MCU, allowing customers to develop an entire application with a single IC.

Content and Documentation

This release include the ServicePack binary image to be programmed into CC3135/CC3235 devices. ServicePack must be applied both in production and development stage of the CC3135/CC3235 devices

File Notes
sp_4.2.0.3_3.1.0.5_3.1.0.17.bin ServicePack binary for UniFlash
sp_4.2.0.3_3.1.0.5_3.1.0.17.ucf ServicePack UCF for host driver API
sp_4.2.0.3_3.1.0.5_3.1.0.17.ucf.signed.bin ServicePack UCF signature

Version information

Component Version
NWP 4.2.0.3
MAC 3.1.0.5
PHY 3.1.0.17

Note: Upon successful ServicePack programming, version can be retrieved using ‘sl_DeviceGet()’ API, with SL_DEVICE_GENERAL_VERSION option.

What’s New

Upgrade and Compatibility Information

The ServicePack can be programmed using UniFlash utility. Latest UniFlash utility can be downloaded from https://www.ti.com/tool/UniFlash.

The ServicePack can also be flushed using host driver API’s or OTA application (please refer for the SimpleLink CC32xx SDK for more information)

Dependencies

This release requires the following software components and tools:

Device Support

Evaluation Boards

Fixed Issues

ID Summary
SL_WIFI_R3-1222 In transceiver mode, the device might get stack when transmitting on different channels
SL_WIFI_R3-1221 MDNS updates to support homekit BCT 1.4 certification
SL_WIFI_R3-1158 When scanning in AP mode - WEP is identified as an OPEN network

Known Issues

ID Summary
SL_WIFI_R3-1245 DHCP Server - Might assign the device's IP address to a client if it is in the address range
SL_WIFI_R3-1232 Smart Config WEP with key set as ascii is not working (only hex)
SL_WIFI_R3-1216 Reg Domain SUT: When STA is set to ‘World Wide’ country, it doesn't perform scanning on channels 12 & 13.
SL_WIFI_R3-1209 Cannot configure (Scan) RSSI threashold for 5G, the 2.4 RSSI configuration override the results.
SL_WIFI_R3-1156 sl_WlanProfleUpdate() fails with enterprise when extended parameter supplied
SL_WIFI_R3-1154 Update profile: updating a profile from (WEP to Open) and (WPA to Open) doesn't work
SL_WIFI_R3-1145 RX filtering promiscuous mode: filter for IP header protocol field doesn't always work
SL_WIFI_R3-1124 HTTP webserver not correctly handling multi-TCP-segment POST requests with user tokens
SL_WIFI_R3-1102 P2P IOP: Could not establish connection with Google Pixel mobile phone
SL_WIFI_R3-1092 (APUT GUI) DHCP Server: If start address and last address are the same, the configuration doesn't apply
SL_WIFI_R3-1049 gethostbyname6(<“IPv6 address”>) with explicit IP address return error
SL_WIFI_R3-974 HTTP Server GUI: Ipv6 global stateless not show as expected
SL_WIFI_R3-695 Select: Setting unopened socket in SlFdSet_t rdListSet in select() does not return an error
SL_WIFI_R3-213 mDNS: NetAppDnsGetHostByService does not return service name, can be retrived from NetAppGetServiceList.

Versioning

This product’s version follows a version format, M.mm.pp.bb, where M is a single digit Major number, mm is 2 digit minor number, pp should be zero indicating official version and b is an unrestricted set of digits used as an incremented build counter.

Technical Support and Product Updates