Change Log
Table of Contents
- Core SDK 4.10.02 (Current Release)
- Core SDK 4.10.01 (Mar 5, 2019)
- Core SDK 4.10.00 (Feb 27, 2019)
- Core SDK 3.80.01 (Dec 19, 2018)
- Core SDK 3.80.00 (Nov 28 2018)
- Core SDK 3.70.00 (Aug 23 2018)
- Core SDK 3.60.01 (May 24 2018)
- Core SDK 3.60.00 (May 24 2018)
- Core SDK 3.50.00 (Feb 22 2018)
- Core SDK 3.40.00 (Nov 20 2017)
- Core SDK 3.30.00 (Aug 23 2017)
- Core SDK 3.20.02 (Jul 10 2017)
- Core SDK 3.20.00 (May 25 2017)
- Core SDK 3.10.02 (Mar 1 2017)
- Core SDK 3.10.01 (Feb 24 2017)
- Core SDK 3.10.00 (Feb 15 2017)
- Core SDK 3.01.01 (Dec 9 2016)
- Core SDK 3.01.00 (Nov 9 2016)
Core SDK 4.10.02 (Current Release)
New Features
| ID | Summary |
|---|---|
| None | None |
Bugs Resolved
| ID | Summary |
|---|---|
| TIDRIVERS-3651 | SysConfig/CC32xx error – Cannot read property ‘name’ of undefined |
Core SDK 4.10.01 (Mar 5, 2019)
New Features
| ID | Summary |
|---|---|
| None | None |
Bugs Resolved
| ID | Summary |
|---|---|
| TIRTOS-1894 | CCS TIRTOS kernel .projectspec files should use XDC 3.51 by default |
| TIDRIVERS-3622 | I2SCC32XX is not working when optimization is turned on |
Core SDK 4.10.00 (Feb 27, 2019)
New Features
| ID | Summary |
|---|---|
| TIRTOS-1842 | Add SysConfig notice to all example README files |
| TIRTOS-1778 | Move to FreeRTOS 10.1.1 |
| TIRTOS-1772 | Migrate to TI 18.12.1 LTS CGT |
| TIRTOS-1589 | Add JSON example |
| TIRTOS-1581 | Update IAR support to 8.32.2 |
| TIRTOS-1448 | Implement nanosleep() to replace deprecated usleep() |
| TIDRIVERS-3627 | Update GPIOCC32XX.h with Pin numbers for GPIO macros |
| TIDRIVERS-3620 | Remove deprecated definitions in Capture.h and Timer.h |
| TIDRIVERS-3541 | Update I2S Example for new API |
| TIDRIVERS-3438 | Update CC32xx I2S driver to match new I2S API |
| TIDRIVERS-3422 | Add generic random number generation utility |
| TIDRIVERS-3347 | Provide SPI Driver Examples with Higher Bit Rate and Show How to use Custom Power Levels |
| TIDRIVERS-1706 | Feature Request for CC32xx Power_shutdown() to use hardware interrupt without RTC |
| TIDRIVERS-1480 | Create top-level I2S driver |
Bugs Resolved
| ID | Summary |
|---|---|
| TIRTOS-1814 | pthread_create() adds guardsize to pre-allocated stack [SYS/BIOS] |
| TIDRIVERS-3424 | ClockPSysTick_nortos can remove clock from queue before timeout expires |
| TIDRIVERS-3406 | Swi execution can occur on Idle task stack vs interrupt stack |
| TIDRIVERS-3397 | IAR linker scripts do not properly reserve HEAP and CSTACK memory |
| TIDRIVERS-1809 | Clock timeout value is lost after first run of clock function [NoRTOS] |
| TIDRIVERS-1808 | UART_write() should return error if UART is still busy |
Core SDK 3.80.01 (Dec 19, 2018)
New Features
| ID | Summary |
|---|---|
| None | None |
Bugs Resolved
| ID | Summary |
|---|---|
| None | None |
Core SDK 3.80.00 (Nov 28 2018)
New Features
| ID | Summary |
|---|---|
| TIRTOS-1603 | Add support for the CC3235S and CC3235SF devices |
| TIRTOS-1584 | Updated examples to use Board_init() instead of Board_initGeneral() |
| TIRTOS-1572 | Add C11 aligned_alloc() to FreeRTOS memory support |
| TIRTOS-1453 | Watchdog example must not clear the watchdog in the ISR |
| TIRTOS-1326 | Update examples to use BASSENSORS BoosterPack instead of SENSORS-BOOSTXL |
| TIDRIVERS-3335 | use common attribute ((align(x))) syntax when alignment is needed |
| TIDRIVERS-1727 | Add function to PWM to set load and match in one call |
| TIDRIVERS-1723 | Remove SDSPI driver from build (has been deprecated for several quarters) |
| TIDRIVERS-1540 | NVSSPI25X should implement polling delay in doErase() to prevent CPU starvation |
| TIDRIVERS-650 | Improve External Flash erase time for NVSSPI25X driver |
Bugs Resolved
| ID | Summary |
|---|---|
| TIRTOS-1767 | usleep(n) should sleep “at least” n microseconds |
| TIRTOS-1607 | Get pthread priority incorrect after priority change [FreeRTOS] |
| TIRTOS-1527 | clock_settime should not discard tv_nsec |
| TIDRIVERS-3366 | The Display driver incorrectly sets the LCD SPI clock frequency to 4Mhz instead of the 1MHz rated value |
| TIDRIVERS-2069 | SPIFFS_unlock() improperly uses lock->count |
| TIDRIVERS-1814 | I2C drivers incorrectly handle error on last byte transmitted |
| TIDRIVERS-1797 | Assert always fails using DMA with SD host |
| TIDRIVERS-1682 | The CC3220 may not enter LPDS (Low Power Deep Sleep) after calling Watchdog_open() |
Core SDK 3.70.00 (Aug 23 2018)
New Features
| ID | Summary |
|---|---|
| TIRTOS-1543 | Update examples and board files to support Sharp128 Display as the default (was Sharp96) |
| TIRTOS-1430 | Call pthread_exit() in run stub to handle termination sequence |
| TIRTOS-1016 | examplesgen – revise the process of importing examples to IAR |
| TIDRIVERS-1667 | Update CC3220 Board files to reflect new silkscreen |
Bugs Resolved
| ID | Summary |
|---|---|
| TIRTOS-1550 | The main_tirtos.c file in many examples has flawed logic |
| TIRTOS-1528 | time() should be implemented in posix for FreeRTOS |
| TIRTOS-1522 | calloc() in FreeRTOS posix compiles into an infinite loop in GCC with -O2 |
| TIRTOS-1512 | pthread key data destructor never invoked [FreeRTOS] |
| TIDRIVERS-1805 | Calling clock_settime delayed from init in FreeRTOS can cause error when clock_gettime is used |
| TIDRIVERS-1696 | UART flow control not working for MSP432E4 and CC32XX |
| TIDRIVERS-1681 | NVSSPI25X_close() does not wait for the external flash to be ready |
| TIDRIVERS-1649 | UART driver has a race condition in callback mode |
| TIDRIVERS-1612 | SDHostCC32XX driver does not work correctly with all DMA channel options |
| TIDRIVERS-1604 | Clock timeout value lost after first run of clock function [FreeRTOS] |
Core SDK 3.60.01 (May 24 2018)
Bugs Resolved
| ID | Summary |
|---|---|
| TIDRIVERS-1623 | Clock tick resync problem with PowerCC32XX_sleepPolicy |
Core SDK 3.60.00 (May 24 2018)
New Features
| ID | Summary |
|---|---|
| TIRTOS-1493 | Add ENFILE to errno |
Bugs Resolved
| ID | Summary |
|---|---|
| TIRTOS-1508 | Align default pthread stack size for all kernels |
| TIRTOS-1436 | Thread handle set too late in pthread_create() [FreeRTOS] |
| TIRTOS-1433 | Clock period ignored when calling ClockP_create() [FreeRTOS] |
| TIRTOS-1432 | Clock start flag and period are ignored when calling ClockP_create() |
| TIRTOS-1429 | Deadlock risk in _pthread_removeThreadKeys() [SYS/BIOS] |
| TIDRIVERS-1591 | UART drivers stack usage in callback mode |
| TIDRIVERS-1565 | ClockP_create() for FreeRTOS does not support a period of 0 |
| TIDRIVERS-1485 | The scheduler cannot be called from inside a HwiP_disable in a task context |
| TIDRIVERS-1475 | Period calculation in PWM drivers (CC32XX, MSP432, MSP432E4) are off by 1 |
| TIDRIVERS-1456 | No GPIO driver support for GPIO 26 & GPIO 27 (ANTSEL1 & ANTSEL2) |
| TIDRIVERS-1441 | ClockP_usleep() for FreeRTOS calculates delay incorrectly |
Core SDK 3.50.00 (Feb 22 2018)
New Features
| ID | Summary |
|---|---|
| TIRTOS-1421 | Update FreeRTOSConfig.h assorted files to use v10 license |
| TIRTOS-1377 | Update Core SDK products to use FreeRTOS version 10 |
| TIRTOS-1368 | FreeRTOS/POSIX clock_gettime() needs to be updated for FreeRTOS v10.0 |
| TIDRIVERS-1296 | Add SPI master and slave examples to demo SPI usage as both master and slave |
| TIDRIVERS-1206 | Create TI driver function to reset the watchdog by PRCM reset function |
| TIDRIVERS-591 | TI-DRIVERS should upgrade to FatFs v0.13a |
| TIDRIVERS-441 | Add SPIFFS, a lightweight file system that uses NVS to interface with on-chip or off-chip FLASH |
Bugs Resolved
| ID | Summary |
|---|---|
| TIRTOS-1346 | Incorrect thread protection in removeThreadKeys() [FreeRTOS] |
| TIRTOS-1337 | Dereference of freed memory in pthread_join() [FreeRTOS] |
| TIRTOS-1336 | pthread_detach() needs thread protection [FreeRTOS] |
| TIRTOS-1335 | Memory leak in pthread_create() on FreeRTOS |
| TIRTOS-1319 | Incorrect thread protection in mq_open() |
| TIRTOS-1275 | CC32XX startup needs to initialize stack for FreeRTOS IAR |
| TIRTOS-1023 | pthread_exit-related memory leak |
| TIDRIVERS-1414 | ClockP_start() (used internally by host driver) has a race condition in NORTOS implementation |
| TIDRIVERS-1371 | ADCBufCC26XX: Move DMA reload into hwi context. |
| TIDRIVERS-1337 | uartechodma project does not appear to use DMA configuration |
Core SDK 3.40.00 (Nov 20 2017)
New Features
| ID | Summary |
|---|---|
| TIRTOS-1312 | Update POSIX pthread support to show ‘fxn’ in UIA execution graph |
| TIDRIVERS-1280 | UART drivers should have error function in HwAttrs |
| TIDRIVERS-1183 | Improve RAM footprint of No-RTOS HwiP dispatch table |
| TIDRIVERS-704 | Convert SDSPI implementations to use SDFatFS interface |
Bugs Resolved
| ID | Summary |
|---|---|
| TIRTOS-1345 | Timed functions expecting abstime on CLOCK_REALTIME are broken |
| TIRTOS-1280 | POSIX barrier broken on FreeRTOS |
| TIDRIVERS-1295 | CC32XX SPI + DMA transfer does not work in Slave Mode |
| TIDRIVERS-1284 | NoRTOS SemaphoreP_post can permanently disable power policy |
| TIDRIVERS-1225 | NVS drivers pre-erase 2 sectors when write is equal to sector size |
Core SDK 3.30.00 (Aug 23 2017)
New Features
| ID | Summary |
|---|---|
| TIDRIVERS-1155 | NVS sections in GCC linker files should only set alignment |
| TIDRIVERS-1110 | Provide an NVS driver for RAM (NVSRAM) |
| TIDRIVERS-1075 | Make Power_idleFunc() the default idleCallback in NoRTOS module |
Bugs Resolved
| ID | Summary |
|---|---|
| TIRTOS-1193 | No-RTOS Display_printf “%%” problem in SystemP_nortos.c |
| TIRTOS-1163 | Display_print3 does not print out % in FreeRTOS based examples |
| TIDRIVERS-1182 | Race condition in No-RTOS HwiP_dispatch for CC3220, CC13xx and CC26xx |
| TIDRIVERS-1177 | Remove usage of shutdown disallow constraints by drivers |
| TIDRIVERS-1151 | When entering hibernate after LPDS serial flash may not be powered down |
| TIDRIVERS-1147 | SPI drivers should support transfer timeout |
| TIDRIVERS-1136 | NoRTOS SemaphoreP_pend should use local ClockP structure |
| TIDRIVERS-1106 | POSIX clock_gettime() for FreeRTOS needs to be more accurate |
| TIDRIVERS-1098 | UARTCC32XX CTS and RTS pins for UART0 need to be enabled |
Core SDK 3.20.02 (Jul 10 2017)
New Features
None
Bugs Resolved
| ID | Summary |
|---|---|
| TIDRIVERS-1136 | NoRTOS SemaphoreP_pend should use local ClockP structure |
Core SDK 3.20.00 (May 25 2017)
New Features
| ID | Summary |
|---|---|
| TIRTOS-1066 | Set configUSE_TIME_SLICING to ‘0’ in all FreeRTOSConfig.h files |
| TIRTOS-1036 | Supply Portable example with native RTOS APIs |
| TIRTOS-1009 | Add examples for NVS for internal and external SPI FLASH when available |
| TIRTOS-991 | Optimize DPL for size |
| TIRTOS-988 | Provide all single-task driver examples also for Non-RTOS |
| TIRTOS-948 | pthread_cond_timedwait should support CLOCK_MONOTONIC |
| TIRTOS-939 | Add Capture Driver for CC32XX device |
| TIRTOS-644 | Redundant FreeRTOS C stack definitions |
| TIRTOS-615 | Create example for UARTMon module |
| TIDRIVERS-1008 | Need Posix sleep and usleep for NoRTOS |
| TIDRIVERS-971 | Provide NVS driver for SPI FLASH |
| TIDRIVERS-963 | UARTCC32XX readTaskBlocking() timeout optimization |
| TIDRIVERS-916 | Board.html should specify pin functions for communication buses |
| TIDRIVERS-900 | Various driver pin encodings need to be explained better |
| TIDRIVERS-891 | Rename ADC_convertRawToMicroVolts to ADC_convertToMicroVolts |
| TIDRIVERS-887 | Capture Driver top level implementation review and fix |
| TIDRIVERS-881 | Construct and destruct APIs for DPL |
| TIDRIVERS-488 | Review TI-RTOS SemaphoreP implementation with goal to reduce stack usage |
Bugs Resolved
| ID | Summary |
|---|---|
| TIRTOS-1031 | FreeRTOS mq_getattr() should not disable scheduler |
| TIRTOS-954 | Update ADC examples to show microvolt values |
| TIRTOS-927 | In CC3220SF device CC3200_PIN_19 cannot assign PWM configure |
| TIDRIVERS-1078 | I2S read/write callback is invoked improperly |
| TIDRIVERS-1054 | Correct the IEEE RX command definition |
| TIDRIVERS-1027 | SemaphoreP_pend for FreeRTOS does not work with tick rate less than 1 msec |
| TIDRIVERS-1013 | FreeRTOS posix mqueue.h mode_t needs to be uint32_t |
| TIDRIVERS-1005 | SemaphoreP_Params_init() should set mode to COUNTING |
| TIDRIVERS-985 | I2CCC32XX_open should reset I2C and clear interrupt at NVIC |
| TIDRIVERS-964 | nortos DPL ClockP ISR should check for equality, not less-than-equal |
| TIDRIVERS-934 | Timeouts for Posix FreeRTOS need to handle wrapping |
| TIDRIVERS-842 | Driver close() should undo pin mux and restore pins to their reset states |
Core SDK 3.10.02 (Mar 1 2017)
New Features
None
Bugs Resolved
| ID | Summary |
|---|---|
| TIRTOS-992 | FreeRTOS POSIX mq_send and mq_receive should be callable from ISR context |
Core SDK 3.10.01 (Feb 24 2017)
New Features
None
Bugs Resolved
| ID | Summary |
|---|---|
| TIDRIVERS-924 | CC32XX GPIO driver pin GPIO_28 is misconfigured |
Core SDK 3.10.00 (Feb 15 2017)
New Features
| ID | Summary |
|---|---|
| TIRTOS-946 | Release.cfg should use policyMin instead of policySpin |
| TIRTOS-925 | IAR Examples.html should reference .eww and not .ipcf files any longer |
| TIRTOS-849 | Capture example needs to be replaced by CapturePWM |
| TIRTOS-842 | Need Mailbox example in the product |
| TIRTOS-750 | The CoreSDK is carrying around unnecessary files/directories |
| TIDRIVERS-888 | Update PWM Driver to use Allocate APIs for CC32XX |
| TIDRIVERS-820 | PowerCC32XX should retake the GPIO semaphore bits upon wake from LPDS, and this should be removed from GPIOCC32XX |
| TIDRIVERS-809 | CC32XX drivers should dynamically specify pin parking states as the device is opened |
| TIDRIVERS-747 | Add TimerCC32XX |
Bugs Resolved
| ID | Summary |
|---|---|
| TIRTOS-945 | pthread_setschedparam not supported in Freertos POSIX |
| TIRTOS-933 | CCS platform warning with TI-RTOS examples |
| TIRTOS-903 | Inconsistent declaration for timer_create, TI-RTOS and FreeRTOS |
| TIRTOS-900 | Display driver not printing float values |
| TIRTOS-897 | Makefile for FreeRTOS kernel has bad error message if FREERTOS_INSTALL_DIR is not set |
| TIRTOS-891 | RTOS build in IAR should be an .ewp and preferably a dependent project like in CCS |
| TIRTOS-823 | Update CC32XX LAUNCHXL Power section |
| TIRTOS-785 | Board_ADCBUFCHANNEL0 should be changed to Board_ADCBUF0CHANNEL0 for consistency |
| TIRTOS-776 | Posix usleep() function implemented in millisecond and not in microseconds |
| TIRTOS-749 | C++ constructors on FreeRTOS with GCC are not called |
| TIRTOS-709 | RTOS config projects are available only in makefile for IAR |
| TIRTOS-415 | IAR tools must be installed in non-default location to work with gmake |
| TIDRIVERS-890 | exit() support is missing in gcc libraries for FreeRTOS |
| TIDRIVERS-877 | ADC driver for CC3220 gives spurious values |
| TIDRIVERS-838 | Can't configure HW Flow control pins on the UART Driver |
| TIDRIVERS-837 | FreeRTOS Posix timer APIs need to check if in an ISR |
| TIDRIVERS-745 | Change reverse() in source\ti\mw\lcd\SharpGrLib.c to SharpGrLib_reverse() |
| TIDRIVERS-405 | UART_write returns before all data has been transmitted |
Core SDK 3.01.01 (Dec 9 2016)
New Features
| ID | Summary |
|---|---|
| TIRTOS-838 | Update the IAR/Arm compiler tools to version 7.80.x |
| TIRTOS-832 | kernel examples should get stack size from linker.cmd files like driver examples |
| TIRTOS-821 | remove ‘eclipse’ directory from the product, CCSv7 needs only .metadata folder |
| TIDRIVERS-810 | Add nortos support files for CC32xx |
Bugs Resolved
| ID | Summary |
|---|---|
| TIRTOS-823 | Update CC32XX LAUNCHXL Power section |
| TIRTOS-814 | Update primary_heap size logic in TI and GCC linker .cmd files |
| TIRTOS-606 | Makefiles should support tools directory names that contain spaces |
| TIDRIVERS-796 | Display_getType compile error for Display_DISABLE_ALL |
Core SDK 3.01.00 (Nov 9 2016)
New Features
| ID | Summary |
|---|---|
| TIRTOS-779 | FreeRTOS POSIX: sem_post() cannot be called from an ISR |
| TIRTOS-764 | CC32XXWARE is defined for the CC32xx examples |
| TIRTOS-763 | Move resetISR from projectSpec to linker command file |
| TIRTOS-759 | Update TI tools to 16.9.0 to be ready for CCSv7.0 |
| TIRTOS-756 | Update examples to use Display_printf instead of print0, etc. |
| TIRTOS-745 | Display_Type_UART should disable RX to allow power savings |
| TIRTOS-723 | Remove os/tirtos/builds/custom from CORE-SDK |
| TIRTOS-719 | Change ‘os’ directory to ‘kernel’ and ‘rtos’ in the CORESDK directory tree |
| TIRTOS-705 | Power Management doc needs updating for CoreSDK |
| TIRTOS-664 | Need to generate binary files in IAR .ipcf files |
| TIRTOS-543 | Update all Drivers examples with Display module usage as necessary |
| TIRTOS-248 | Move TI-RTOS driver documentation out of the user guide and into doxygen |
| TIDRIVERS-738 | Deprecate ti.drivers.Config as apps should supply libs on command line |
| TIDRIVERS-735 | Remove instrumented driver libraries and provide only release libraries |
| TIDRIVERS-695 | Remove the AWAKE_LDPS registration/notification in CryptoCC3200 |
| TIDRIVERS-601 | Update Power APIs for MISRA compliance |
| TIDRIVERS-569 | Update UART Display driver to function like an LCD |
Bugs Resolved
| ID | Summary |
|---|---|
| TIRTOS-687 | Insufficient thread stack size to run CC32xx cryptoHmac example |
| TIRTOS-586 | FreeRTOS build warnings (related to TI's CC3200/portsasm.h) |
| TIRTOS-552 | Spiloopback example master/slave needs synchronization |
| TIRTOS-230 | SD examples for CC32xx do not work for some SD cards |
| TIDRIVERS-688 | CC3220S Board file's ADC pins should NOT use PIN57 as this conflicts with the UART pins |
| TIDRIVERS-407 | OOB I2S Example for CC32xx does not work at 44.1KHz or above |