Sysconfig Standalone User Guide
Table of Contents
Using SysConfig with IAR Workbench
If you are using the IAR toolchain, you can use SysConfig as a standalone desktop tool to generate the configuration files to be compiled and linked with your application.
The steps that follow use the SysConfig v1.0.646 standalone installer and IAR-EWARM 8.32.2. The figures use the CC32XX SDK as an example, but other SimpleLink SDKs follow the same procedure. These steps assume the TI Code Generation Tools are installed in the default location.
Install SysConfig as a standalone tool (download here) within the default location (
C:\ti
).Open IAR and follow these steps to configure it to use the correct viewer for *.syscfg files:
a. Choose Tools > Configure Viewers from the menus, and then click Import. (Possible with IAR EWARM 8.32.2 or higher)
[](./sysconfig_standalone_iar_images/image001.png " Configure Viewers“)
b. Navigate to the SDK installation directory
<SDK_INSTALL_DIR>\tools\iar\
and select the filesysconfig_iar_setup.xml
like in the image shown below.[](./sysconfig_standalone_iar_images/image002.png " Configure Viewers“)
c. Alternatavily you can add the configuration manually by pressing the New button:
- Choose Tools > Configure Viewers from the menus, and then click New.
- Type .syscfg in the File name extensions field.*
- Select the Command line option and type the following into the field:
$SYSCONFIG_ROOT$\nw\nw.exe $SYSCONFIG_ROOT$ --compiler iar --product $SIMPLELINK_CC32XX_SDK_INSTALL_DIR$\.metadata\product.json --output $PROJ_DIR$ $FILE_PATH$
Follow these steps to import custom argument variables into IAR:
a. Choose Tools > Configure Custom Argument Variables from the menus.
b. Choose the Workspace or Global tab depending on how you want to apply the variables.
c. Click the Import button and browse to
\tools\iar
within your SDK installation. Select the*.custom_argvars
file provided there and click OK.d. Click the Edit Variable button and change the path of
SYSCONFIG_ROOT
according to the location of your SysConfig installation.If you have not done so already, create a new IAR workspace.
Follow these steps to add a project from one of the examples in the SDK’s
\examples\sysconfig_preview
folder.a. Choose Project > Add Existing Project from the menus.
b. Within your SDK installation, for this example browse to
\examples\syscfg_preview\rtos\CC3235S_LAUNCHXL\demos\power_measurement\freertos\iar
c. Add the
power_measurement.ewp
file.Rebuild the project to perform the custom build step, which uses SysConfig to generate additional files.
Double click on the *.syscfg file in your project.
This shall open SysConfig and offers you to adapt drivers, IO Pins and other settings.
NOTE: You can view the custom build configuration by choosing Project > Options from the menus and selecting the Custom Build category.