SimpleLink™ CC32xx SDK 2.40.01.01 Release Notes

Introduction

The SimpleLink™ Wi-Fi® CC32xx device is a single-chip microcontroller (MCU) with built-in Wi-Fi connectivity, created for the Internet of Things (IoT). The CC32xx device is a wireless MCU that integrates a high-performance ARM® Cortex®-M4 MCU, allowing customers to develop an entire application with a single IC.

The Texas Instruments royalty-free CC32xx Embedded Wi-Fi foundation software development kit (SDK) is a complete software platform for developing Wi-Fi applications. It is based on the CC3220 and cc3235 devices, a complete Wi-Fi SoC (System-on-Chip) solution. The CC32xx family of devices comes in following variants:

The SimpleLink™ Wi-Fi® CC32xx SDK contains drivers, libraries, example code for the CC32xx programmable MCU and documentation needed to use the solution. It also contains the flash programmer, a command line tool for flashing software, configuring network and software parameters (SSID, access point channel, network profile, etc.), system files, and user files (certificates, web pages, etc). This SDK can be used with TI’s SimpleLink Wi-Fi CC32xx LaunchPads.

The CC32xx solution combines a 2.4-GHz and 5-Ghz Wi-Fi PHY/MAC and TCP/IP networking engine with a microcontroller, up to 256-kB on-chip RAM, 1-MB internal flash (for CC32xx SF), and a comprehensive range of peripherals.

The SimpleLink™ MCU portfolio offers a single development environment that delivers flexible hardware, software and tool options for customers developing wired and wireless applications. With 100 percent code reuse across host MCUs, Wi-Fi™, Bluetooth® low energy, Sub-1GHz devices and more, choose the MCU or connectivity standard that fits your design. A one-time investment with the SimpleLink software development kit (SDK) allows you to reuse often, opening the door to create unlimited applications. For more information, visit www.ti.com/simplelink.

This is version 2_40_01_01 of the SimpleLink CC32xx SDK.

Documentation

What’s New

Code example:

   _u32 enable;
    enable = 1;
    sl_SetSockOpt(SockID,SL_SOL_SOCKET,SL_SO_SECURE_ENABLE_OCSP,&enable,sizeof(_u32));

Updating service-pack

It is recommended to update the service pack to the latest available, which can be found in the following path:
CC3220 Service pack - <SDK_INSTALL_DIR>/tools/cc32xx_tools/servicepack-cc3x20
CC3235 Service pack - <SDK_INSTALL_DIR>/tools/cc32xx_tools/servicepack-cc3x35
CC3220 NWP Service Pack Release Notes.
CC3235 NWP Service Pack Release Notes.

For more information please follow the instructions in the Quick start Guide.

Upgrade and Compatibility Information

The Migration Guide intends to guide users who already have experience with CC3200 devices and need to port their software to CC3220x/CC3235x family of devices. The document describes the SDK structure and highlights the software components that require attention including host driver, OS layers, board drivers, and external libraries.

Operating Systems Support

Dependencies

This release was validated with the following components:

Device Support

Known Issues

ID Summary
CC3X20SDK-1642 Signal spawn from IRQ context does not call the correct function
CC3X20SDK-1613 [provisioning] SC_KEY_ENABLE feature does not works as expected
CC3X20SDK-1600 Network terminal - Radio tool, Can be set gen2 on 5G channels.
CC3X20SDK-1569 Calling sl_Stop during sl_Select may cause assert
CC3X20SDK-1548 GPIO 11 doesn't wake device from hibernate when configured through PowerCC32XX_config
CC3X20SDK-1528 HttpClient: Connection to HTTPS web server through Proxy fails
CC3X20SDK-1527 AT Commands: Http client read response body command with length larger than 900 bytes might cause memory allocation fault
CC3X20SDK-1525 MQTT Client: connection with user name and without password is not functional
CC3X20SDK-1514 Cloud OTA :OTA TAR with name larger than 109 characters stops the OTA process without an error
CC3X20SDK-1450 OTA Lib: wrong handling of fragmented HTTP response
CC3X20SDK-1423 AT Commands: MDNS service is not advertised when flag is IPV6_IPV4_ONLY used, need to add IS_UNIQUE_BIT flag in order to make it advertise
CC3X20SDK-601 Rarely the MQTT Server internal bridging does not work from server to client
CC3X20SDK-156 Rarely the progress bar get stuck during OTA procedure
CC3X20SDK-116 Progress bar on Windows FireFox browser doesn't update process status on the fly

Versioning

This product’s version follows a version format, M.mm.pp.bb, where M is a single digit Major number, mm is 2 digit minor number, pp is a 2 digit patch number, and b is an unrestricted set of digits used as an incrementing build counter.

M - Is incremented for the first release every year. 1 -> 2017, 2 -> 2018, and so on..

mm - indicates the specific quarter of the year the SDK was released. 10 -> Q1; 20 -> Q2; 30 -> Q3; 40 -> Q4

Prior Releases

Technical Support and Product Updates