SL_WIFI_R2-1459 |
STA doesn't poll packets after beacon indicates both broadcast and unicast data exist for the STA |
SL_WIFI_R2-1431 |
sl_Start() calls to return SL_API_ABORTED rather than SL_ERROR_FS_ALERT_ERR when device is locked |
CC3X20SDK-1530 |
Doc: Add cc3120 programmers guide link to the documentation overview |
CC3X20SDK-1488 |
CSR example: remove serial number input from user interface as it is not valid input for CSR |
CC3X20SDK-1443 |
Sl Start which resolve in data abort cannot be followed by sl_stop |
CC3X20SDK-1316 |
AT Command: all AT commands that send data in binary mode would fail if containing LF, CR or backspace |