Cloud Ota
Table of Contents
Example Summary
This example demonstrate the Over the Air (OTA) update from remote servers on CC32xx devices. The OTA update is a bundle of files packed in archive tar file and may include: - Service pack for the NWP - New MCU image - Other user files
Peripherals Exercised
Board_LED0 (red LED)
- Indicates that the board was initialized withinmain()
and while blinking, indicates that the board is trying to connect to AP.LaunchPad board button
- Stop Pings Start the OTA update process, can be disabled by defining DISABLE_OTA_SWITCH_TRIGGER in cloud_ota.c (5 Pings and then OTA process)
Example Usage
Downloads and Installations.
Make sure you have Uniflash installed and Code Composer Studio or IAR IDE.
- !! IMPORTANT NOTE!!
- User must add access token (Dropbox, Github or custum) and define the OTA_VENDOR_TOKEN in otauser.h
#define OTA_VENDOR_TOKEN "<access token>"
- User must add access token (Dropbox, Github or custum) and define the OTA_VENDOR_TOKEN in otauser.h
- Checklist of required elements.
- Uniflash projects according to device flavor.
- Certificate artifacts, ca_in_cert_store, cert-good.der certificate and cert-good-key.der private key.
- Certificate for dropbox and github: DigCert_High_Assurance_CA.der, GoDaddy_class2_CA.der .
- Simple link provisioning application on your mobile device
- archive tar file for device update should be placed in the Dropbox or Github servers.
Build the setup.
Make sure you have the a local AP.
Build the project and flash it by using the SimpleLink Uniflash utility.
The example could be executed from the debugger as well but since it involves platform reset at the end (so the new OTA image can be tested and committed),the debugger would get disconnected. The example could be downloaded by the ImageCreator, make sure that all the certificates file are there
Open a serial session (e.g.
HyperTerminal
,puTTY
, etc.) to the appropriate COM port.The COM port can be determined via Device Manager in Windows or via
ls /dev/tty*
in Linux.
The connection should have the following settings
Baud-rate: 115200
Data bits: 8
Stop bits: 1
Parity: None
Flow Control: None
Run the example by pressing the reset button. The example should start running automatically when programming via Uniflash is done.
- The example will start connection by the provisioning process
- Follow provisioning application instructions in order to connect to your local AP
- The example will start pinging external server
- The example will start connection by the provisioning process
At this point, local OTA is enabled and may be triggered by pressing the LaunchPad button
The procedure to update a new version is as follows:
OTA process will connect the Dropbox/Github CDN server to get the archive tar file
The Dropbox/Github account and directory is configured from otauser.h file
OTA will save all archive files in the NWP SFLASH OTA, on download done, will call sl_Stop() and reset the MCU in order to move the new update into ‘TESTING’ mode OTA, after reset, will run the new update and on succefull ping (system check is ok) will commit the new update OTA will try agin to doanload only newer update from the CDN server
Application Design Details
This example demonstrates remote Over-the-Air update experience with CC32xx LaunchPad development kit. Over-the-Air update demonstrates an update of a full image over a secured channel. OTA service enables in-system update of the MCU application, CC32xx firmware releases (a.k.a. Service Pack) made available by Texas Instruments and other vendor files. An update procedure executed in a full system integrity fashion, i.e. failure in upgrading any of the image components would lead to rolling back to the previous valid version.
Please install the latest CC32xx Service Pack.
References
- For full detailed user guide see CC3220-CC3120 OTA Application document or open the following website: