95 #ifndef ti_drivers_watchdog_WatchdogCC32XX__include 96 #define ti_drivers_watchdog_WatchdogCC32XX__include 138 #define WatchdogCC32XX_CMD_IS_TIMER_ENABLE (Watchdog_CMD_RESERVED + 0) 148 #define WatchdogCC32XX_CMD_GET_TIMER_VALUE (Watchdog_CMD_RESERVED + 1) 159 #define WatchdogCC32XX_CMD_IS_TIMER_LOCKED (Watchdog_CMD_RESERVED + 2) 170 #define WatchdogCC32XX_CMD_GET_TIMER_RELOAD_VALUE (Watchdog_CMD_RESERVED + 3) unsigned int intPriority
Definition: WatchdogCC32XX.h:194
uint32_t reloadValue
Definition: WatchdogCC32XX.h:195
Watchdog driver interface.
Watchdog Object for CC32XX.
Definition: WatchdogCC32XX.h:203
struct WatchdogCC32XX_HWAttrs WatchdogCC32XX_HWAttrs
Watchdog hardware attributes for CC32XX.
Watchdog hardware attributes for CC32XX.
Definition: WatchdogCC32XX.h:191
unsigned int baseAddr
Definition: WatchdogCC32XX.h:192
const Watchdog_FxnTable WatchdogCC32XX_fxnTable
Watchdog function table for CC32XX.
The definition of a Watchdog function table that contains the required set of functions to control a ...
Definition: Watchdog.h:346
struct WatchdogCC32XX_Object WatchdogCC32XX_Object
Watchdog Object for CC32XX.
unsigned int intNum
Definition: WatchdogCC32XX.h:193
bool isOpen
Definition: WatchdogCC32XX.h:204