90 #ifndef ti_drivers_uart_UARTCC32XX__include 91 #define ti_drivers_uart_UARTCC32XX__include 100 #include <ti/drivers/dpl/ClockP.h> 101 #include <ti/drivers/dpl/HwiP.h> 102 #include <ti/drivers/dpl/SemaphoreP.h> 115 #define UARTCC32XX_PIN_UNASSIGNED 0xFFF 117 #define UARTCC32XX_PIN_01_UART1_TX 0x700 118 #define UARTCC32XX_PIN_02_UART1_RX 0x701 119 #define UARTCC32XX_PIN_03_UART0_TX 0x702 120 #define UARTCC32XX_PIN_04_UART0_RX 0x703 121 #define UARTCC32XX_PIN_07_UART1_TX 0x506 122 #define UARTCC32XX_PIN_08_UART1_RX 0x507 123 #define UARTCC32XX_PIN_16_UART1_TX 0x20F 124 #define UARTCC32XX_PIN_17_UART1_RX 0x210 125 #define UARTCC32XX_PIN_45_UART0_RX 0x92C 126 #define UARTCC32XX_PIN_45_UART1_RX 0x22C 127 #define UARTCC32XX_PIN_53_UART0_TX 0x934 128 #define UARTCC32XX_PIN_55_UART0_TX 0x336 129 #define UARTCC32XX_PIN_55_UART1_TX 0x636 130 #define UARTCC32XX_PIN_57_UART0_RX 0x338 131 #define UARTCC32XX_PIN_57_UART1_RX 0x638 132 #define UARTCC32XX_PIN_58_UART1_TX 0x639 133 #define UARTCC32XX_PIN_59_UART1_RX 0x63A 134 #define UARTCC32XX_PIN_62_UART0_TX 0xB3D 143 #define UARTCC32XX_PIN_50_UART1_RTS 0xA31 147 #define UARTCC32XX_PIN_61_UART1_CTS 0x33C 149 #define UARTCC32XX_PIN_62_UART1_RTS 0x33D 154 #define UARTCC32XX_FLOWCTRL_NONE 0 159 #define UARTCC32XX_FLOWCTRL_HARDWARE 1 193 #define UARTCC32XX_CMD_IS_BUSY (UART_CMD_RESERVED + 0) 204 #define UARTCC32XX_CMD_IS_RX_DATA_AVAILABLE (UART_CMD_RESERVED + 1) 215 #define UARTCC32XX_CMD_IS_TX_SPACE_AVAILABLE (UART_CMD_RESERVED + 2) const unsigned char * writeBuf
Definition: UARTCC32XX.h:379
enum UART_Echo_ UART_Echo
UART echo settings.
unsigned int powerMgrId
Definition: UARTCC32XX.h:390
uint16_t txPin
Definition: UARTCC32XX.h:317
uint32_t baudRate
Definition: UARTCC32XX.h:362
const UART_FxnTable UARTCC32XX_fxnTable
Power_NotifyObj postNotify
Definition: UARTCC32XX.h:389
uint32_t flowControl
Definition: UARTCC32XX.h:309
unsigned int intNum
Definition: UARTCC32XX.h:305
UARTCC32XX Object.
Definition: UARTCC32XX.h:329
uint16_t txPin
Definition: UARTCC32XX.h:392
enum UART_PAR_ UART_PAR
UART parity type settings.
SemaphoreP_Handle readSem
Definition: UARTCC32XX.h:374
enum UART_LEN_ UART_LEN
UART data length settings.
struct UARTCC32XX_Object * UARTCC32XX_Handle
enum UART_Mode_ UART_Mode
UART mode settings.
Power notify object structure.
Definition: Power.h:113
unsigned int baseAddr
Definition: UARTCC32XX.h:303
uint16_t rtsPin
Definition: UARTCC32XX.h:321
PowerCC32XX_ParkState prevParkTX
Definition: UARTCC32XX.h:391
UART Global configuration.
Definition: UART.h:695
size_t readCount
Definition: UARTCC32XX.h:373
struct UARTCC32XX_HWAttrsV1 UARTCC32XX_HWAttrsV1
UARTCC32XX Hardware attributes.
uint16_t ctsPin
Definition: UARTCC32XX.h:319
UART_LEN dataLength
Definition: UARTCC32XX.h:363
Power manager interface for the CC32XX.
struct UARTCC32XX_FxnSet UARTCC32XX_FxnSet
Complement set of read functions to be used by the UART ISR and UARTCC32XX_read(). Internal use only.
ClockP_Handle txFifoEmptyClk
Definition: UARTCC32XX.h:388
size_t readSize
Definition: UARTCC32XX.h:372
UART_Callback writeCallback
Definition: UARTCC32XX.h:384
unsigned int writeEmptyClkTimeout
Definition: UARTCC32XX.h:385
The definition of a UART function table that contains the required set of functions to control a spec...
Definition: UART.h:652
Complement set of read functions to be used by the UART ISR and UARTCC32XX_read(). Internal use only.
Definition: UARTCC32XX.h:244
unsigned int intPriority
Definition: UARTCC32XX.h:307
unsigned int writeTimeout
Definition: UARTCC32XX.h:383
HwiP_Handle hwiHandle
Definition: UARTCC32XX.h:360
UARTCC32XX Hardware attributes.
Definition: UARTCC32XX.h:301
uint16_t rtsPin
Definition: UARTCC32XX.h:394
struct UARTCC32XX_Object UARTCC32XX_Object
UARTCC32XX Object.
enum UART_STOP_ UART_STOP
UART stop bit settings.
enum UART_ReturnMode_ UART_ReturnMode
UART return mode settings.
UART_PAR parityType
Definition: UARTCC32XX.h:365
UART_Callback readCallback
Definition: UARTCC32XX.h:376
unsigned char * ringBufPtr
Definition: UARTCC32XX.h:311
int(* readTaskFxn)(UART_Handle handle)
Definition: UARTCC32XX.h:246
SemaphoreP_Handle writeSem
Definition: UARTCC32XX.h:382
unsigned int readTimeout
Definition: UARTCC32XX.h:375
RingBuf_Object ringBuffer
Definition: UARTCC32XX.h:368
PowerCC32XX_ParkState prevParkRTS
Definition: UARTCC32XX.h:393
UARTCC32XX_FxnSet readFxns
Definition: UARTCC32XX.h:370
size_t ringBufSize
Definition: UARTCC32XX.h:313
unsigned char * readBuf
Definition: UARTCC32XX.h:371
ClockP_Handle timeoutClk
Definition: UARTCC32XX.h:361
uint16_t rxPin
Definition: UARTCC32XX.h:315
UART_STOP stopBits
Definition: UARTCC32XX.h:364
size_t writeSize
Definition: UARTCC32XX.h:380
void(* UART_Callback)(UART_Handle handle, void *buf, size_t count)
The definition of a callback function used by the UART driver when used in UART_MODE_CALLBACK The cal...
Definition: UART.h:438
size_t writeCount
Definition: UARTCC32XX.h:381
bool(* readIsrFxn)(UART_Handle handle)
Definition: UARTCC32XX.h:245
enum UART_DataMode_ UART_DataMode
UART data mode settings.
PowerCC32XX_ParkState
Enumeration of states a pin can be parked in.
Definition: PowerCC32XX.h:385