55 #ifndef ti_drivers_Power__include 56 #define ti_drivers_Power__include 66 #define Power_TOTAL (1U) 67 #define Power_RESUME (2U) 70 #define Power_NOTIFYDONE (0) 71 #define Power_NOTIFYERROR (-1) 75 #define Power_EFAIL (-1) 76 #define Power_EINVALIDINPUT (-2) 77 #define Power_EINVALIDPOINTER (-3) 78 #define Power_ECHANGE_NOT_ALLOWED (-4) 79 #define Power_EBUSY (-5) 82 #define Power_ACTIVE (1U) 83 #define Power_ENTERING_SLEEP (2U) 84 #define Power_EXITING_SLEEP (3U) 85 #define Power_ENTERING_SHUTDOWN (4U) 86 #define Power_CHANGING_PERF_LEVEL (5U) 92 typedef void (*Power_PolicyInitFxn)(void); 103 uintptr_t eventArg, uintptr_t clientArg);
556 uint_fast32_t shutdownTime);
577 int_fast16_t
Power_sleep(uint_fast16_t sleepState);
uint_fast32_t Power_getTransitionLatency(uint_fast16_t sleepState, uint_fast16_t type)
Get the hardware transition latency for a sleep state.
int_fast16_t Power_getDependencyCount(uint_fast16_t resourceId)
Get the current dependency count for a resource.
uintptr_t clientArg
Definition: Power.h:117
int_fast16_t Power_sleep(uint_fast16_t sleepState)
Transition the device into a sleep state.
int_fast16_t Power_init(void)
Power initialization function.
Power notify object structure.
Definition: Power.h:113
int_fast16_t(* Power_NotifyFxn)(uint_fast16_t eventType, uintptr_t eventArg, uintptr_t clientArg)
Power notify function pointer.
Definition: Power.h:102
int_fast16_t Power_setPerformanceLevel(uint_fast16_t level)
Set the MCU performance level.
int_fast16_t Power_setConstraint(uint_fast16_t constraintId)
Declare an operational constraint.
int_fast16_t Power_registerNotify(Power_NotifyObj *pNotifyObj, uint_fast16_t eventTypes, Power_NotifyFxn notifyFxn, uintptr_t clientArg)
Register a function to be called upon a specific power event.
void(* Power_PolicyFxn)(void)
Power policy function pointer.
Definition: Power.h:97
int_fast16_t Power_shutdown(uint_fast16_t shutdownState, uint_fast32_t shutdownTime)
Put the device into a shutdown state.
uint_fast16_t Power_getPerformanceLevel(void)
Get the current performance level.
void Power_setPolicy(Power_PolicyFxn policy)
Set a new Power policy.
struct Power_NotifyObj_ Power_NotifyObj
Power notify object structure.
int_fast16_t Power_releaseDependency(uint_fast16_t resourceId)
Release a previously declared dependency.
void Power_unregisterNotify(Power_NotifyObj *pNotifyObj)
Unregister previously registered notifications.
uint_fast32_t Power_getConstraintMask(void)
Get the constraints that have been declared with Power.
void Power_disablePolicy(void)
Disable the configured power policy from running when the CPU is idle.
uint_fast16_t Power_getTransitionState(void)
Get the current transition state of the Power manager.
List_Elem link
Definition: Power.h:114
int_fast16_t Power_releaseConstraint(uint_fast16_t constraintId)
Release a previously declared constraint.
int_fast16_t Power_setDependency(uint_fast16_t resourceId)
Declare a dependency upon a resource.
void Power_enablePolicy(void)
Enable the configured power policy to run when the CPU is idle.
void Power_idleFunc(void)
Power function to be added to the application idle loop.
Power_NotifyFxn notifyFxn
Definition: Power.h:116
uint_fast16_t eventTypes
Definition: Power.h:115
Linked List interface for use in drivers.