This example introduce the user to the MQTT Client Library.
Secured socket In order to activate the secured example, SECURE_CLIENET should be enabled ( certificates should be programmed )
Subscribed topics The Client will connect to remote broker Subscribed to the topics “/Broker/To/cc32xx” - General topic that will print the data on the uart
“/cc3200/ToggleLEDCmdL1” - toggle LED0
“/cc3200/ToggleLEDCmdL2” - toggle LED1
“/cc3200/ToggleLEDCmdL3” - toggle LED2
Published topics the topic will be published by pressing SW2 on the board