SimpleLink™ Certification Reports 2.30.00.00 Release Notes
Introduction
The SimpleLink™ certification reports are provided to customers as reference material and customers should always consult with their regulatory test house on the re-use of any test reports and/or applying modular results to their product. Please read this USE AGREEMENT carefully. If you do not agree, do not use the TI Services and TI Materials, as such terms are defined in the Agreement.
What’s New
- The following module certificatoin reports where added:
- CC3100MOD Certification reports for FCC, ISED, CE, China, & Japan
- CC3120MOD Certification reports for FCC, ISED, CE, China & Japan
- CC3200MOD Certification reports for FCC, ISED, CE, China & Japan
- CC3220MOD Certification reports for FCC, ISED, CE, Chian & Japan
- The following EVM certificatoin reporst where added (NOTE: EVM certificatoin reports are for reference only and do not hold modular certification and thus the customer is resposible for certificatoin using the IC version of the device):
- CC3100MODBOOST Certification reports for FCC, IC & CE
- CC3200MODLAUNCHXL Certification reports for FCC, IC & CE
- BOOSTXL-CC3120MOD Certification reports for FCC, IC & CE
- LAUNCHCC3220MODASF Certification reports for FCC, IC & CE
- CC3100BOOST Certificatoin reports for FCC, IC & CE
- CC32000-LAUNCHXL Certification reports for FCC, IC & CE
- CC3120BOOST Certification reports for FCC, IC & CE
- CC3220x-LAUNCHXL Certification reports for FCC, IC & CE
Versioning
The certification version follows the following format, M.mm.pp.bb, where:
M - Is incremented for the first release every year. 1 -> 2017, 2 -> 2018, and so on.
mm - indicates the specific quarter of the year the certificatoin report was released on TI.com. 10 -> Q1; 20 -> Q2; 30 -> Q3; 40 -> Q4
pp - indicated if an udpated certification document was released in the same quarter.
M - is an unrestricted set of digits used for minor report updates released within the same quarter.
Prior Releases
This is the first release