CC3200 SDK 1.4.0 Release Notes
Table of Contents
Introduction
The SimpleLink™ Wi-Fi® CC3200 device is a single-chip microcontroller (MCU) with built-in Wi-Fi connectivity. The CC3200 device is a wireless MCU that integrates a high-performance ARM® Cortex®-M4 MCU, allowing customers to develop an entire application with a single IC.
For more information, visit www.ti.com/simplelink.
This is version 1.4.0 of the CC3200 SDK.
Getting Started
To get started using the CC3200 LaunchPad with the Out of Box experience, please see the CC3200 Quick Start Guide.
To get started with your project development, please see the CC3200 Getting Started Guide.
What’s New
- Bug fixes
- Example maintenance and updates
- Updated all CCS projects to .projectspec files
- CCS and IAR examples use debug SimpleLink library builds by default
Updating the servicepack
It is recommended to update the service pack to the latest available, which can be downloaded from the CC3200 SDK download page.
For more information, see the CC3100 & CC3200 UniFlash Guide.
Dependencies
This release was validated with the following components:
- Code Composer Studio 8.3
- Compiler TI 18.1.4.LTS
- IAR Code Generation Tools
- SimpleLink host driver 1.0.1.13
- CC3100/CC3200_ServicePack 1.0.1.13-2.11.0.1
- TI-RTOS 2.16.01.14
- FreeRTOS 10.0.1
Device Support
- CC3200R1 [ES1.33 Chip Id : 0x4000010]
- CC3200-LAUNCHXL Rev3.2 onwards
Directory Structure
| Directory Name | Content |
|---|---|
| Docs | Quick Start Guide for LaunchPad Out of Box Experience Getting Started Guide for application development SimpleLink Host Driver Programmer’s API Guide (simplelink_api folder) CC3200 TI-RTOS User’s Guide Power Management Framework Guide OTA Update Application Note SimpleLink OTA Extlib API Guide CC3200 Peripheral Driver Library API Guide API Guides for MQTT and HTTP libraries (netapps folder) |
| Driverlib | Peripheral driver library source files. driverlib.a is provided in CCS, GCC and IAR directories. |
| Examples | Example applications in source code |
| Inc | Register definition header files |
| Middleware | Power Management Framework providing an easy-to-use infrastructure for low power solutions |
| Netapps | HTTP client library source files HTTP server library source files (webserver) JSON parser library source files MQTT client library source files MQTT client-server library source files SMTP client library source files TFTP client library source files XMPP client library source files |
| Oslib | Interface file to configure Free-RTOS or TI-RTOS |
| SimpleLink | The SimpleLink Network Processor host driver code. Pre-built simplelink library (simplelink.a) for OS, NON_OS, PM_framework and NON_OS_PM are available in CCS and IAR directories, plus debug versions of these libraries. For GCC compiler, libsimplelink.a and libsimplelink_nonos.a are available in gcc folder. |
| SimpleLink Ext Libraries | FLC library source files OTA library source files Provisioning library source files |
| Third Party | FATFS library source files FreeRTOS library source files |
| TI-RTOS | Abstraction layer files for TI-RTOS |
| Tools | ccs_patch – Files required for CCS-FTDI-LP connection gcc_scripts – Script files required for GCC compiler ftdi - Contains CC3200 FTDI-USB driver for Windows iar_patch – Files required for IAR-FTDI-LP connection |
Examples
Networking Applications
| Example | Description | OS Support | Documentation |
|---|---|---|---|
| Antenna Selection | Antenna Selection is the method by which users can configure the WLAN RF antenna on the CC3200 device to improve radio performance. | TI-RTOS | antenna_selection README |
| Connection Policy | Demonstrates the connection policies which determine how the CC3200 connects to an AP. | Non-OS | connection_policy README |
| Demonstrates how to send emails via SMTP on a hardware interrupt. | TI-RTOS | email README | |
| Enterprise Security | Demonstrates the connection to an enterprise network using the flashed certificate. Certificate is flashed onto the serial flash. | Non-OS | ent_wlan README |
| File Download | Demonstrates how to connect to a server to download a file and save it on the serial flash. | Non-OS | file_download README |
| File Operations | Demonstrates the file operations on the serial flash. | Non-OS | file_operations README |
| Get Time | Connects to a SNTP server and requests time information. | FreeRTOS | get_time README |
| Get Weather | Connects to a weather service website and requests weather data. | FreeRTOS | get_weather README |
| Getting Started with WLAN AP | Demonstrates device capability to behave as an AP in a typical networking system. | TI-RTOS | getting_started_with_wlan_ap README |
| Getting Started with WLAN Station | Demonstrates device capability to behave as a station in a typical networking system. | TI-RTOS | getting_started_with_wlan_station README |
| Hibernate | Showcases hibernate mode as a power-saving tool in a networking context, demonstrated as a UDP client. | FreeRTOS | hib README |
| HTTP Client Demo | Demonstrates the HTTP Client library to enable the device as an HTTP Client. | Non-OS | http_client_demo README |
| HTTP Server | Demonstrates the internal HTTP Server hosted on the CC3200. | FreeRTOS | httpserver README |
| Idle Profile (Non OS) | Demonstrates a low power mode (LPDS) using the Power Management Framework in a Non-OS environment. | Non-OS | idle_profile_nonos README |
| Idle Profile | Demonstrates a low power mode (LPDS) using the Power Management Framework. | FreeRTOS | idle_profile README |
| mDNS | Demonstrates mDNS functionality in CC3200. This application showcases “mDNS advertise” and “mDNS listen” functionality. | Non-OS | mdns README |
| Mode Configuration | Configure the device either to a station or an Access Point. | Non-OS | mode_config README |
| MQTT Client | Showcases the device acting as a MQTT client in a fully functional MQTT network. | TI-RTOS/FreeRTOS | mqtt_client README |
| MQTT Server | Showcases the device acting as an MQTT Server managing multiple local clients and allowing local clients to communicate with remote MQTT clients. | FreeRTOS | mqtt_server README |
| NWP Filter | Demonstrates the RX filtering feature on the CC3200. | Non-OS | nwp_filter README |
| OTA Update | Showcases Over-The-Air (OTA) firmware update including MCU image, service pack, and additional user files. | FreeRTOS/Non-OS | OTA Application Note |
| Out of Box | Demonstrates the Out of Box Experience with the CC3200 Launch Pad. | FreeRTOS | out_of_box README |
| P2P (Wi-Fi Direct) | Demonstrates Wi-Fi direct (Peer to Peer) feature on the CC3200. | Non-OS | p2p README |
| Power Measurement | Provides users the ability to configure the device in various low power modes and profiles for power measurements. | Non-OS | power_measurement README |
| Provisioning AP | Demonstrates the AP provisioning feature. AP Provisioning is the method by which users can configure AP information on the CC3200 device from a web browser. | Non-OS | provisioning_ap README |
| Provisioning SmartConfig | Demonstrates the SmartConfig provisioning feature. TI SmartConfig is the proprietary method where users can use a Wi-Fi enabled device to configure the CC3200 to an AP on the fly. | Non-OS | provisioning_smartconfig README |
| Provisioning WPS | Demonstrates how to use WPS for Wi-Fi provisioning. | Non-OS | provisioning_wps README |
| Scan Policy | Demonstrates how to set the scan policy and enables the scan. | Non-OS | scan_policy README |
| Sensor Profile | Demonstrates a low power mode (hibernate) using the Power Management Framework. | FreeRTOS | sensor_profile README |
| Serial Wi-Fi | Serial Wi-Fi is a capability designed to provide easy, self-contained terminal access behavior over a UART interface. | FreeRTOS | serial_wifi README |
| SSL | Showcases SSL implementation on the CC3200. | Non-OS | ssl README |
| TCP Socket | Demonstrates device communication over a network using TCP protocol. | Non-OS | tcp_socket README |
| TFTP Client | Demonstrates how a client application can read/write a file from/to the TFTP server running on a network. | FreeRTOS | tftp_client README |
| Transceiver Mode | The RX Statistics feature is used to inspect the medium in terms of congestion, distance, and validate the RF hardware. Using the RSSI information it can help position the CC3200 in an ideal location. | Non-OS | transceiver_mode README |
| UDP Socket | Demonstrates device communication over a network using UDP protocol. | Non-OS | udp_socket README |
| Watchdog System | Demonstrates the use of a watchdog timer (WDT) in a complete system with MCU and networking subsystem. | Non-OS | watchdog_system_demo README |
| WebSock Simple | Demonstrates the real-time streaming capability of websocket protocol. | FreeRTOS | websocket_simple README |
| Wi-Fi Audio | Demonstrates audio streaming on the CC3200. Device can act as a speaker or microphone. | FreeRTOS | wifi_audio_app README |
| XMPP | Demonstrates the connection and communication via a XMPP server. | TI-RTOS | xmpp README |
MCU Only Applications
| Example | Description | OS Support | Documentation |
|---|---|---|---|
| ADC | Demonstrates the functionality of the CC3200 ADC module using driverlib APIs. | Non-OS | adc README |
| AES | Demonstrates the AES encryption feature on the CC3200. | Non-OS | aes README |
| Application Bootloader | Demonstrates the secondary bootloader operations to manage updates to application image. | Non-OS | application_bootloader README |
| Blinky | Demonstrates the GPIOs using driverlib APIs to control LEDs on the CC3200. LaunchPad. | Non-OS | blinky README |
| CRC | Demonstrates the functionality of the CC3200 CRC module using driverlib APIs. | Non-OS | crc README |
| DES | Demonstrates the DES encryption feature on the CC3200. | Non-OS | des README |
| Dynamic Library Loader | Demonstrates dynamic loading of an application binary from non-volatile memory while the program is being executed. | FreeRTOS | dynamic_lib_loader README |
| FreeRTOS Demo | Showcases FreeRTOS functionality like task creation and inter-task communication using message queues. | FreeRTOS | freertos_demo README |
| I2C | Demonstrates the functionality of the CC3200 ADC module using driverlib APIs. | Non-OS | i2c_demo README |
| Interrupt | Demonstrates interrupt preemption and tail-chaining capabilities. | Non-OS | interrupt README |
| MCU Sleep | Demonstrates the sleep mode of the MCU. | Non-OS | sleep README |
| Pulse Width Modulation (PWM) | Demonstrates the functionality of the CC3200 PWM module using driverlib APIs. | Non-OS | pwm README |
| SDHost | Demonstrates the functionality of the CC3200 SDHost module using driverlib APIs. | Non-OS | sdhost README |
| SDHost FatFS | Demonstrates the functionality of the CC3200 SDHost FATFS module using driverlib APIs to provide the block level read/write access to the SD card. | Non-OS | sdhost_fatfs README |
| SHA-MD5 | Demonstrates the SHA-MD5 Hash Algorithm on the CC3200. | Non-OS | shamd5 README |
| SPI | Demonstrates the functionality of the CC3200 SPI module using driverlib APIs. | Non-OS | spi_demo README |
| Timer | Demonstrates the usage of 16 bit timers to generate interrupts that toggle GPIOs. | Non-OS | timer README |
| Timer Count Capture | Demonstrates the timer count capture feature to measure the frequency of an external signal. | Non-OS | timer_cc README |
| UART | Demonstrates the functionality of the CC3200 UART module using driverlib APIs. | Non-OS | uart_demo README |
| UART DMA | Demonstrates UART using driverlib APIs with uDMA and interrupts. | Non-OS | uart_dma README |
| uDMA | Demonstrates different DMA modes of transfer. | Non-OS | udma README |
| Watchdog Demo Application | Demonstrates the watchdog timer functionality to reset the system whenever the system fails. | Non-OS | watchdog README |
Fixed Issues
SDK
| ID | Summary |
|---|---|
| SLWIFICSR-427 | Move all example READMEs to markdown/HTML |
| SLWIFICSR-424 | Pin 55 & 57 pin mode check in PRCMCC3200MCUInit() |
| SLWIFICSR-421 | File_download example update server |
| SLWIFICSR-385 | Extend URL length in OTA example and library |
| SLWIFICSR-360 | Change websock_camera to websock_simple |
| SLWIFICSR-333 | PSIRT-9 Simplelink memory corruption vulnerability webserver |
| SLWIFICSR-307 | Email example update security methods |
| SLWIFICSR-306 | Move example and netapps libraries to CCS projectspec files |
| SLWIFICSR-256 | HTTP Client parsing is case-sensitive |
| SLWIFICSR-253 | SSL example update cipher suites for server |
| SLWIFICSR-238 | Add provisionlib CCS configuration for os and nonos |
| SLWIFICSR-214 | Get_weather update APIs |
| SLWIFICSR-213 | Get_time update default SNTP server |
| SLWIFICSR-204 | Wrong value for FreeRTOS configMAX_SYSCALL_INTERRUPT_PRIORITY |
| SLWIFICSR-191 | Scan_policy example should init terminal and print scan list |
| SLWIFICSR-185 | SSL example should use SlDateTime_t definition from device.h |
| SLWIFICSR-156 | Timer_cc timer overflow |
| SLWIFICSR-149 | Tcp_socket includes print statement that doesn't check pointer value before printing |
| SLWIFICSR-148 | Out of Box locks up without error message when I2C jumpers are not placed |
| SLWIFICSR-147 | SSL example update instructions to generate root CA |
| SLWIFICSR-146 | SSL example assigns incorrect values to time structure |
| SLWIFICSR-145 | Wifi_audio_app GPIO configuration |
| SLWIFICSR-143 | Httpserver UniFlash file has incorrect path to mcuimg |
| SLWIFICSR-142 | Build examples correctly with NOTERM symbol undefined |
| SLWIFICSR-130 | MQTT client update server defaults |
| SLWIFICSR-98 | Uart_hal.c generates extra callback |
| SLWIFICSR-44 | Xmpp_client update server defaults |
Host Driver
| ID | Summary |
|---|---|
| SLWIFICSR-229 | Request x509 serial number to be exposed via getsockopts |
| CC3X00SDK-203 | Add host driver macro to disable WPA enterprise server authentication |
Known Issues
SDK
| ID | Summary |
|---|---|
| SLWIFICSR-425 | HTTPCli_getResponseStatus does not timeout in file_download example |
| SLWIFICSR-420 | Memory leak in webserver library when receiving data (WSCore_DataRecv) |
Network Processor / Host Driver
| ID | Title | Description | Impact | Workaround |
|---|---|---|---|---|
| SL_WIFI_R1-400 | WiFi Security: CC3100 and CC3200 Supports only WEP with Key Index 0 (==> AP Key index 1) | When using WEP security – only WEP index 0 is supported | Can’t use more than one key in WEP security | None |
| SL_WIFI_R1-149 | WiFi Security: Traffic Stop while WPA EAP-TLS Enterprise and Reauthentication enabled | In WPA EAP-TLS security the traffic stopped when Reauthentication packet is received | Traffic stopped | Disable reauthentication or set it to a very long time |
| SL_WIFI_R1-1258 | Scan: Results list contain duplicate networks | Device might returns duplicate networks when the network list is not totally filled and the get scan results ask for fewer entries than what was actually found. | Duplicate networks in Scan results list | Read the maximum entries at once (20 entries) or to read one by one starting from the end to the beginning and check for duplicates. Once a duplicate was found the list is completed |
| SL_WIFI_R1-747 | sl_NetAppDnsGetHostByName return with no answer in high traffic | In high Rx traffic some DNS packets can get lost | No answer on request | Run API again |
| SL_WIFI_R1-808 | UDP/RAW socket data payload is limited to MTU size | Tx IP Fragmentation is not supported for UDP and RAW Tx | Packet bigger than MTU size will lead that portion of the packet will be discard | Use packet size <= MTU size |
| SL_WIFI_R1-934 | DHCP: SL continues using its previous IP address if an invalid IP in the DHCPACK (before lease time expired) | DHCPACK arrives to SL with invalid address in the DHCPACK params address field but also the IP destination is the same invalid address (MAC address is the valid SL address). SL does not listen to other IPs address as destination but his own therefore this DHCPACK is not processed and SL continue to use his old address until the lease time expires | The device will continue to use the previous IP address | N/A |
| SL_WIFI_R1-1016 | NS: SL device should discard ICMP Req datagram with problem in IP Header | According to the RFC – if the gateway or host processing a ICMP Req datagram and finds a problem with the header parameters such that it cannot complete processing the datagram it must discard the datagram | Low impact - The SL device sends ICMP reply message | N/A |
| SL_WIFI_R1-1313 | NS: Error -105 when trying to open 4 TCP server sockets while the internal HTTP server is running | While the HTTP server is running one of the TCP server is been used and limit the number of user TCP Servers. Error -105 - SL_ENOBUFS [No buffer space available] | Only 3 TCP servers can be used while the HTTP is running | Disable the internal HTTP Server if 4 TCP Server need to be used |
| SL_WIFI_R1-1347 | NS: blocking accept on secure socket doesn’t return | Procedure: open secured socket, bind, listen, select on socket. Select will not return when other side is connected | Select doesn’t return | Don’t use select method for accept on secure socket |
| SL_WIFI_R1-1320 | Transceiver mode: Can’t configuring the channel of a RAW Socket if it’s already open | Changing the channel while a RAW socket is open to receive by using SetSockOpt command can halt the Host. The command response on SetSockOpt doesn’t return. As a result, the host is might get stuck if it configured to blocking mode. | Host might get stuck | Close the socket and open it again with the correct channel |
| CC3x00SDK-69 | WPS PIN Connect might fail if pin code is not null-terminated | If the PIN code from the HOST is not null terminated the string can be wrongly used and in some cases the connection doesn’t succeed | Connection doesn’t succeed | Add null termination to the PIN code string |
| CC3x00SDK-166 | Host: Set/Get time is limited up to year 2038 | time.h (standard time library) is limiting the structure to a signed 32-bit integer, and this number is interpreted as the number of seconds since 00:00:00 UTC on 1 January 1970 | Low impact – Certifications that are bounded by date will expire after year 2038 | N/A |
| SL_WIFI_R1-930 | In Enterprise network the device will Frequently Wakeup due to IPV4 BRDCST Rx frames | On enterprise network there a lot of BRDCST packets | Increase in power consumption | Add a filter to block the broadcast packets. Filter is specific to the enterprise network. |
Notes for CC3200 Application Developers
SimpleLink library build: Release vs. Development
A core reset from the debugger will only reset the applications MCU and leave the networking subsystem active. This means while using the debugger on the CC3200 LaunchPad, the developer would have to manually reset the LaunchPad after every debug session before loading the new application image.
To improve the developer’s experience, the following was added to the implementation of sl_Start:
sl_DeviceEnablePreambledefined asNwpPowerOnPreamblein cc_pal.c resets the networking services- Delay in
sl_DeviceEnabledefined asNwpPowerOnintroduced for proper operation - With these changes, the networking engine has to be gracefully stopped and started again for the next debug session. This includes some additional delays which result in greater overall current consumption. As these additional steps and delays are required only for debug purposes, they should not be a part of deployment applications.
For ease of use, the latest CC3200 SDK provides separate configurations of the SimpleLink library for development (debug) and deployment scenarios.
Release libraries
- NON_OS – SimpleLink for NON-OS environment
- OS – SimpleLink for OS environment
- PM_Framework – SimpleLink with Power Management Framework for OS environment
- NON_OS_PM – SimpleLink with Power Management Framework hook
Development libraries
- NON_OS_debug – SimpleLink for NON-OS environment with debug support
- OS_debug – SimpleLink for NON-OS environment with debug support
- PM_Framework_debug – SimpleLink with Power Management Framework for OS environment with debug support
- NON_OS_PM_debug – SimpleLink with Power Management Framework hook with debug support
All the above configurations are pre-built in the SDK package along with their generated output library.
Note that the debug builds will result in overall greater current consumption. Developers should link to the release library builds for deployment by updating the library path to simplelink.a in their IDE.
Updating SimpleLink spawn task stack size
By default, the SimpleLink spawn task stack size is set to 2048 bytes. While this size is sufficient for the applications available in the SDK, this value may need to be changed depending on the callback implementation/call flows. In order to change the stack size, the oslib library must be rebuilt with the macro SPAWN_TASK_STACK set to the optimum stack size value (for example -DSPAWN_TASK_STACK=3072).
Implementation of osi.h is shown below:
#ifndef SPAWN_TASK_STACK
#define STACK_LEN (2048) /*Stack Size*/
#else
#define STACK_LEN (SPAWN_TASK_STACK)
#endifPost-LPDS settings
PRCMCC3200MCUInit API must be called after coming out of LPDS. If this API is not called post-LPDS, then the interrupts and DMA requests for GPIO and I2C modules would not work since their initial configuration is lost after LPDS. PRCMCC3200MCUInit has these settings and will reconfigure these modules.
The Idle Profile example demonstrates this from the lp3p0_restore_soc_data implementation.
Default GPIO settings
All GPIO pins default to Mode 1 on power-up, unless programmed by the MCU. Set all unused pins except the serial flash SPI (pins 11, 12, 13, 14) and JTAG (pin 16, 17, 19, 20) to Mode 0 to prevent any bus contention.
Add following code snippet to void PinMuxConfig(void):
PinModeSet(PIN_X,PIN_MODE_0);For example, by default I2C is muxed to pins 1 and 2. If the application assigns other pins to the I2C module, this would cause contention. To resolve contention on I2C lines, add following code snippet to void PinMuxConfig(void):
PinModeSet(PIN_01,PIN_MODE_0);
PinModeSet(PIN_02,PIN_MODE_0);