Release Notes
Table of Contents
Introduction
The SimpleLink™ Wi-Fi® CC3200/3100 device family is a single-chip with built-in Wi-Fi connectivity, created for Internet of Things (IoT) purposes. The CC3100 device integrates all protocols for Wi-Fi and Internet, which greatly minimizes host MCU software requirements.
The Texas Instruments royalty-free SimpleLink host driver provides a complete software library, made especially for developing Wi-Fi® applications for the CC3100 network processor.
This document describes the Software Development Kit (SDK) version 1.3.0 for use with the CC3100 SimpleLink Wi-Fi Network Processor device mounted on the CC3100 BoosterPack development platform.
Getting Started
Please follow the on-line CC3100 Quick Start Guide to start using the CC3100 BoosterPack development platform.
Please download the CC3100 Getting Started Guide to get started with your project development.
Procedure to Upgrade from SDK 1.2.0 to SDK 1.3.0
To upgrade from SDK 1.2.0 to SDK 1.3.0, ensure servicepack 1.0.1.11-2.10.0.0 (or newer) is flashed on CC3100. The servicepack 1.0.1.11-2.10.0.0 is available at the SDK download page. Please refer to the UNIFLASH Quick Start Guide for details on flashing the service pack.
What’s New
Host Driver fixes and code optimizations
Please refer to the Host Driver Release Notes for the changes to the Host Driver.
SDK Content
| SDK Version | Updates from previous version |
|---|---|
| 1.3.0 | MSP430Ware_3_80_03_07TivaWare_C_Series-2.1.4.178STM32Cube_FW_F4_V1.19.0 |
Release Content
| Item | Version | Type |
|---|---|---|
| Device | CC3100R ES1.33 Chip Id : 0x4000000 | Production device |
| Development boards | CC3100BOOST Rev3.3 onwards with CC31XXEMUBOOST Board Rev3.0 | Orderable from TI |
| SDK Installer | CC3100SDK-1.3.0-windows-installer.exe for Windows 7 | Provided with a click wrap license |
| Firmware | 2.10.0.0.31.1.5.0.2.1.0.3.37 | Download servicepack_1.0.1.11-2.10.0.0 |
| Reference host platform | MSP430F5529 Launchpad MSP430FR5969 Launchpad TM4C123GH6PM Launchpad TM4C1294NCPDT Launchpad STM32F407VG Discovery Kit |
Orderable from TI (except for Discovery Kit) |
| Network Processor Host driver | Version 1.0.1.11 | Source code |
| Supported IDE | IAR version 7.11 for MSP430 IAR version 8.20 for TM4C + STM32 CCS version 7.4 MS Visual Studio Express 2010 for PC & SimpleLink Studio Eclipse 4.3.0 for PC and SimpleLink Studio |
Delivered separately |
| Demo | Embedded HTML web-site | Pre-flashed on Booster Pack and source code provided |
| User guides | CC3100 Getting started guide CC3100 BoosterPack User Guide SimpleLink Host Driver Programmer’s Guide |
PDF Doxygen HTML |
| Tools | USB Drivers for CC31XXEMUBOOST board for Windows | Executable |
Directory Structure of SDK
Double-Click on the package to copy the directories (and files) to the preferred location. The first level directory structure is as shown in the table below.
| Directory Name | Content |
|---|---|
| Docs | Getting Started Guide for application development Boards User Guide SimpleLink Host Driver Programmer’s Guide Application notes for sample applications MQTT library API document HTTP client library API document Simplelink OTA Extlib API document |
| Examples | Example application in source code |
| Netapps | HTTP client library source code, MQTT library source code |
| Oslib | Interface file to configure Free-RTOS |
| Platform | MSP430F5529lp |
| SimpleLink | The SimpleLink Network Processor host driver code template_user.h file to be modified by the user for porting the driver to any host platform |
| Simplelink_extlib | OTA (over the air) library source code, Provisioning library |
| Third_party | Free-RTOS source code |
| Tools | cc31xx_board_drivers: USB Drivers for Windows 7 to enable application development on a PC using SimpleLink Studio for CC3100 |
Networking
Package Quality
Interoperability - IOP
- STA mode was tested for connection, traffic and power consumption with more than 200 AP
- AP mode was tested for connection and traffic with more than 50 STA
Robustness
- Use cases were tests for 1000 of cycles – for example:
- Connect/Disconnect
- On/Off
- Connect, Send Packet, Disconnect
Stability
- STA was kept running at different traffic scenarios in open AIR for long durations.
- Green Dot - STA was stopped after a set time
- The Failure tests (red dot) is representing TCP Tx with 163Byte payload in congested environment, the test fail due to socket disconnect after 67Hours (3 other instances passed >70hours)
Features
Wi-Fi
| Standards | 802.11b/g/n Station and Wi-Fi Direct Client |
|---|---|
| Supported Channels | 1-13 The default regulatory domain is US (1-11) |
| Personal Security | WEP, WPA and WPA2 |
| Enterprise Security | WPA-2 Enterprise EAP Fast EAP PEAPv0 MSCHAPv2 EAP PEAPv0 TLS EAP PEAPv1 TLS EAP TLS EAP TTLS TLS EAP TTLS MSCHAPv2 |
| Provisioning | SmartConfigTM technology Wi-Fi Protected Setup (WPS2) Access Point mode with internal HTTP Web Server |
| Standards | 802.11b/g Access Point and Wi-Fi Direct Group Owner |
| Clients | 1 |
| Personal Security | WEP, WPA and WPA2 |
Networking protocols
| IP | IPv4 |
|---|---|
| Transport | UDP TCP RAW ICMP |
| Cross-Layer | DHCP ARP DNS |
| Application | mDNS DNS-SD HTTP 1.0 web server |
| Transport Layer Security | SSLV3 SSL_RSA_WITH_RC4_128_SHA SSLV3 SSL_RSA_WITH_RC4_128_MD5 TLSV1 TLS_RSA_WITH_RC4_128_SHA TLSV1 TLS_RSA_WITH_RC4_128_MD5 TLSV1 TLS_RSA_WITH_AES_256_CBC_SHA TLSV1 TLS_DHE_RSA_WITH_AES_256_CBC_SHA TLSV1 TLS_ECDHE_RSA_WITH_RC4_128_SHA TLSV1 TLS_ECDHE_RSA_WITH_AES_256_CBC_SHA TLSV1_1 TLS_RSA_WITH_RC4_128_SHA TLSV1_1 TLS_RSA_WITH_RC4_128_MD5 TLSV1_1 TLS_RSA_WITH_AES_256_CBC_SHA TLSV1_1 TLS_DHE_RSA_WITH_AES_256_CBC_SHA TLSV1_1 TLS_ECDHE_RSA_WITH_RC4_128_SHA TLSV1_1 LS_ECDHE_RSA_WITH_AES_256_CBC_SHA TLSV1_2 TLS_RSA_WITH_RC4_128_SHA TLSV1_2 TLS_RSA_WITH_RC4_128_MD5 TLSV1_2 TLS_RSA_WITH_AES_256_CBC_SHA TLSV1_2 TLS_DHE_RSA_WITH_AES_256_CBC_SHA TLSV1_2 TLS_ECDHE_RSA_WITH_RC4_128_SHA TLSV1_2 TLS_ECDHE_RSA_WITH_AES_256_CBC_SHA TLSV1_2 TLS_RSA_WITH_AES_128_CBC_SHA256* TLSV1_2 TLS_RSA_WITH_AES_256_CBC_SHA256* TLSV1_2 TLS_ECDHE_RSA_WITH_AES_128_CBC_SHA256* TLSV1_2 TLS_ECDHE_ECDSA_WITH_AES_128_CBC_SHA256* *client mode |
| User application sockets | Up to 8 open sockets Up to 2 secured application sockets: |
Advanced Features
| 802.11 Transceiver | Transmit and Receive raw Wi-Fi packets with full control over payload. Wi-Fi disconnect mode. Can be used for general-purpose applications (e.g. tags, sniffer, RF tests) |
| Traffic Filters | Embedded filters to reduce power consumption and Wake-on-LAN trigger packets (IP and MAC layer) |
Interfaces
| SPI | Standard SPI up to 20MHz on production device and up to 14MHz on Pre-Production device |
| UART | 4 wire UART up to 3MHz |
Power Modes
| Low Power mode | Uses 802.11 Power Save and Device Deep Sleep Power with three user configurable policies |
| Configurable Power Policies | Normal (Default)– Best tradeoff between traffic delivery time and power performance Low power–- Used only for Transceiver mode application (Disconnect mode) Long Sleep Interval–- Wakes up for the next DTIM after a configurable sleep interval, up to 2 seconds. This policy is only applicable for client socket mode |
Advanced Information
System/Software Capabilities
- Host SPI interface max speed: 20MHz (production device)
- Stability in all traffic scenarios was tested for at least 12 hours (major use cases were tested for at least 24hours) – User may rarely experience:
- Traffic Stops
- System freeze
- Robustness tests
- Start/Stop with WiFi Connect/Disconnect and data Tx burst was tested for 5000 cycles and found to be stable
- WiFi Connect/Disconnect without data was tested for 5000 cycles and found stable
- SSL
- Elliptic-curve based ciphers (e.g. ECDH) implies a longer connection time
- Network Stack
- TCP Window size: 32KB (Production device)
- The memory resources are divided among all user sockets and the TCP windows size might change accordingly
- IP Fragmentation is not supported for Tx UDP and RAW sockets
- In connection mode Tx and Rx traffic should be done after IP is acquired
- File System
- Up to 100 user files
- File Size is limited to ~1Mbyte [1,040,384byte] (No Error if trying to create a larger size)
- SPI Interface
- Little/Big Endian Hosts are supported
- 8/16/32bit modes are supported
- Big Endian auto detection is supported
- UART Interface
- Little Endian Hosts are supported
- HTTP Server
- Support HTTP 1.0
- Built-in ROM WEB Pages
- Additional WEB pages can be stored on the File System
- Dynamic content through proprietary Token mechanism (limited to 64 Characters)
- WEP
- WEP open using ASCII pre shared key
- Small code can be used in the Host and HTTP Web page to support HEX format (more details and code example included in the programmer’s guide)
- WPS
- Delay of up to 4Sec can be seen between association and EAPOL-Start when using WPS connection
- Default State - With no other configuration the default state of the device is as follows:
- STA mode
- Regulatory domain is US (channel 1-11)
- Connection policy – AutoStart and AutoSmartConfig
- DHCP - Enable
Product Constraints
- SSL
- Supported modes
- Up to one Server (Listen Socket and Accept Socket) + Client (Data socket)
- Up to Two clients (Data socket)
- CA Certificates must be installed if server authentication is required
- Client mode –
- Signature authentication check – must be less or equal to 2048
- Key exchange and challenge – must be less or equal to 2048
- Client authentication – must be less or equal to 2048
- Server mode –
- Signature authentication check – must be less or equal to 2048
- Key exchange and challenge – must be less or equal to 2048
- Client authentication – must be less or equal to 2048
- Packets will be truncated above 1386Bytes (two TCP packets will be transmitted)
- Supported modes
- SmartConfig
- Not supported with 5GHz AP (802.11a/n/ac)
- Not supported for MIMO-capable configuration devices
- Not supported with non-standard proprietary modulation schemes
- Only Group 0 is supported in auto start mode
- In Auto Start Mode the key is transferred not encrypted
- Enterprise Security
- WPA2-TLS connection is not supported with v3 certificates
- Connection is successful with expired date certificates
- Tx Power
- Tx power in AP mode takes effect only after reset
- WiFi Direct
- When the WiFi Direct is set to be Group Owner (GO) the recommendation will be to set FAST connection policy to TRUE
- Rx Filters
- BSSID can’t be filtered while STA is connected (If filtered will cause disconnection)
- Power Management
- The device will remain in active after init until the host will read all events
- HTTP internal WEB Pages – main limitations
- Values entered are not validated – for example:
- Adding longer/short key in password fields (will be accepted)
- Typing letters in DHCP lease time (instead of numbers)
- WPA password is requested to be entered in Hex format when it should be ASCII
- The length of the AP SSID field is limited to 15 characters (instead of 32)
- The length of the AP Password field is limited to 24 characters (instead 63)
- The length of the Device name is limited to 15 characters (instead of 32)
- Adding/configuring Hidden SSID is not supported
- HTTP authentication (user name and password) should be disabled in order not to get into a lock state
- Values entered are not validated – for example:
- Network Stack
- Max Tx payload for Raw packet with IP header is 1460 bytes
- Max Tx payload for Raw Transceiver (disconnect mode) is 1476 bytes (including Data and Header)
- Min Tx payload for Raw Transceiver (disconnect mode) is 14 bytes (including Data and Header)
- Closing socket should be done in a proper way (for example not to close a socket while there is blocking receive command on it) - a timeout can be used in this scenarios
- TCP socket keep alive timeout is set to 5 min (non configurable)
- Host
- The Host driver is assuming that a Char value is equal to 1 Byte. MCU (like CC2000) that support different configuration won’t work with the Host Driver as is. The only option is to port the driver manually to the MCU architecture
- Setting device Mode
- Changing the device role (STA<->AP<->P2P) requires to reset the device
- Setting network configurations after setting the device role (without reset) can lead to system halt
- If SetRole to station was issued during AP mode it won’t accept connected STA (See first bolt, reset is required)
- Setting the device mode is persistent and SFLASH endurance must be considered on use cases that requires switching between roles
- Network configuration is applicable to the current role of the device
- Supported SFLASH
- The product supports JEDEC specification (to read manufacture ID by JEDEC standard) – the below list are the main SFLASH that were verified.
- Micron N25Q128- A13BSE40 - 128Mbit
- Spansion S25FL208K - 8Mbit
- Winbond W25Q16V - 16Mbit
- Adesto AT25DF081A - 8Mbit
- Macronix MX25L12835F-M2 - 128Mbit
- Macronix MX25R6435 – 64Mbit
- ISSI IS25LQ016 - 16Mbit
- Updated list and more recommendation can be found in: CC3100 & CC3200 Serial Flash Guide
- The product supports JEDEC specification (to read manufacture ID by JEDEC standard) – the below list are the main SFLASH that were verified.
Sample Applications
The release package includes sample applications created for the MSP430F5529 Launchpad including:
- Application Notes explaining the functionality usage
- Project file for IAR and CCS
- Smartphone application as needed
Some of the sample applications are also provided for MSP430FR5969, TM4C123GH6PM, TM4C1294NCPDT and SimpleLink Studio on a PC environment. All the applications can be easily ported to other MCUs and host processors. The default speed of SPI clock for MSP430F5529 is 12 MHz and can be increased to 20 MHz. Only debug configuration is provided for CCS and Visual Studio projects.
Antenna Selection
This is a reference implementation for antenna-selection scheme running on the host MCU, to enable improved radio performance inside buildings
Connection Policies
This application demonstrates the usage of the CC3100 profiles and connection-policies.
Send Email
This application sends an email using SMTP to a user-configurable email address at the push of a button.
Enterprise Network Connection
This application demonstrates the procedure for connecting the CC3100 to an enterprise network.
File System
This application demonstrates the use of the file system API to read and write files from the serial Flash.
Get Time
This application connects to an SNTP cloud server and receives the accurate time.
Get Weather
This application connects to ‘Open Weather Map’ cloud service and receives weather data.
Getting Started in AP Mode
This application configures the CC3100 in AP mode. It verifies the connection by pinging the connected client.
Getting Started in STA Mode
This application configures the CC3100 in STA mode. It verifies the connection by pinging the connected Access Point.
HTTP Client
This application demonstrates the use of HTTP client library API for HTTP based application development.
HTTP Server
This application demonstrates using the on-chip HTTP Server APIs to enable static and dynamic web page content.
IP Configuration
This application demonstrates how to enable static IP configuration instead of using DHCP.
MDNS
This application registers the service for broadcasting and attempts to get the service by the name broadcasted by another device.
Mode Configuration
This application demonstrates switching between STA and AP modes.
MQTT Client
This application showcase the use of MQTT library API to connect to an IBM MQTT broker and communicate using appropriate topic names.
NWP Filters
This application demonstrates the configuration of Rx-filtering to reduce the amount of traffic transferred to the host, and to achieve lower power consumption.
NWP Power Policy
This application shows how to enable different power policies to reduce power consumption based on use case in the station mode.
Out-of-box
This application demonstrates Out-of-Box experience with CC3100 Booster Pack
OTA sample application
This application focuses on showcasing CC3100’s ability to receive firmware update and/or any related files over the internet enabled wifi interface. This example uses the Dropbox API app platform to store and distribute the OTA update files.
Wi-Fi Direct
This application configures the device in Wi-Fi Direct (P2P) mode and demonstrates how to communicate with a remote peer device.
Provisioning with WPS
This application demonstrates the usage of WPS Wi-Fi provisioning with CC3100.
Scan Policy
The application demonstrates the scan-policy settings in CC3100.
SPI Diagnostics Tool
This is a diagnostics application for troubleshooting the host SPI configuration.
SSL/TLS
The application demonstrates the usage of certificates with SSL/TLS for application traffic privacy and device or user authentication
TCP Socket
The application demonstrates simple connection with TCP traffic.
Transceiver Mode
The application demonstrates the CC3100 transceiver mode of operation.
UDP Socket
The application demonstrates simple connection with UDP traffic.
XMPP Client
The application demonstrates instant messaging using a cloud based XMPP server.
Errata
The following section covers known issues and performance limitations with CC3100 production and pre-production devices.
Hardware
Pre-regulated 3.3v to Pin 47
For preproduction devices connect an external pre-regulated 3.3v +/- 5% supply to pin 47 (VDD_ANA2). This adds 12mA average current and up to 100mA peak current over 20uSec to the total system current at 3.3V.
The CC3100 BoosterPack version 3.3 already includes the correct supply configuration for the pre-production device and also adds a 10uF capacitor to filter the peak currents. No further action is required.
The external 3.3V supply is not required in the CC3100 production device in which case pin 47 should be left not connected.
Power consumption increase
Power consumption of the CC3100 pre-production device in all active modes is 1-2 mA higher compared to the CC3100 production devices
Performance
| Item | Production Devices |
|---|---|
| Maximum SPI clock speed | 20 MHz |
| Init time from hibernate until device ready | 75 mSec |
| Init time from hibernate until WPA2 connection | 120 mSec |
| Maximum UDP throughput, open socket | 16 Mbps |
| Maximum TCP throughput, open socket | 13 Mbps |
| Maximum TLS/SSL throughput with RC4_128 cipher | 9 Mbps |
| Maximum TLS/SSL throughput with AES_256 cipher | 12 Mbps |
| Minimum TLS/SLL connection time with ECC cipher | 1.3 Sec |
| Minimum TLS/SSL connection time with RSA cipher | 130 mSec |
Software
Wi-Fi Known Issues
| ID | MCS00123349 |
| Title | WiFi Security: CC3100 and CC3200 Supports only WEP with Key Index 0 (==> AP Key index 1) |
| Description | When using WEP security – only WEP index 0 is supported |
| Impact | Can’t use more than one key in WEP security |
| Workaround | None |
| ********** | ****************************************************************************************************************************************** |
| ID | MCS00106970 |
| Title | WiFi Security: Traffic Stop while WPA EAP-TLS Enterprise and Reauthentication enabled |
| Description | In WPA EAP-TLS security the traffic stopped when Reauthentication packet is received |
| Impact | Traffic stopped |
| Workaround | Disabled Reauthentication or set it to a very long time |
| ********** | ****************************************************************************************************************************************** |
| ID | MCS00130040 |
| Title | WiFi Direct Reliability: 65% Success rate when Peer device is initiator of connection |
| Description | Negotiation with other peer not always successful at first chance |
| Impact | The first connection doesn’t success |
| Workaround | Try to connect again |
| ********** | ****************************************************************************************************************************************** |
| ID | MCS00131174 |
| Title | Scan: Results list contain duplicate networks |
| Description | The SimpleLink might returns duplicate networks when the network list is not totally filled and the get scan results ask for fewer entries than what was actually found. |
| Impact | duplicate networks in Scan results list |
| Workaround | Read the maximum entries at once (20 entries) or to read one by one starting from the end to the beginning and check for duplicates. Once a duplicate was found the list is completed |
| ********** | ****************************************************************************************************************************************** |
Networking Known Issues
| ID | MCS00127876 |
| Title | sl_NetAppDnsGetHostByName return with no answer in high traffic |
| Description | In high Rx traffic some DNS packets can get lost |
| Impact | No answer on request |
| Workaround | Run the API again |
| ********** | ****************************************************************************************************************************************** |
| ID | MCS00128353 |
| Title | UDP/RAW socket data payload is limited to MTU size |
| Description | Tx IP Fragmentation is not supported for UDP and RAW Tx |
| Impact | Packet bigger than MTU size will lead that portion of the packet will be discard |
| Workaround | Use packet size <= MTU size |
| ********** | ****************************************************************************************************************************************** |
| ID | MCS00128959 |
| Title | DHCP: SL continues using its previous IP address if an invalid IP in the DHCPACK (before lease time expired) |
| Description | DHCPACK arrives to SL with invalid address in the DHCPACK params address field but also the IP destination is the same invalid address (MAC address is the valid SL address) SL does not listen to other IPs address as destination but his own therefore this DHCPACK is not processed and SL continue to use his old address until the lease time expires |
| Impact | The device will continue to use the previous IP address |
| Workaround | N/A |
| ********** | ****************************************************************************************************************************************** |
| ID | MCS00129407 |
| Title | NS: SL device should discard ICMP Req datagram with problem in IP Header |
| Description | According to the RFC – if the gateway or host processing a ICMP Req datagram and finds a problem with the header parameters such that it cannot complete processing the datagram it must discard the datagram |
| Impact | Low impact – The SL device sends ICMP reply message |
| Workaround | N/A |
| ********** | ****************************************************************************************************************************************** |
| ID | MCS00131564 |
| Title | NS: Error -105 when trying to open 4 TCP server sockets while the internal HTTP server is running |
| Description | While the HTTP server is running one of the TCP server is been used and limit the number of user TCP Servers Error -105 - SL_ENOBUFS [No buffer space available] |
| Impact | Med impact – Only 3 TCP servers can be used while the HTTP is running |
| Workaround | Disable the internal HTTP Server if 4 TCP Server need to be used |
| ********** | ****************************************************************************************************************************************** |
| ID | MCS00131966 |
| Title | NS: blocking accept on secure socket doesn’t return |
| Description | procedure: |
| Impact | High impact – Select doesn’t return |
| Workaround | Don’t use select method for accept on secure socket |
| ********** | ****************************************************************************************************************************************** |
| ID | MCS00131612 |
| Title | Transceiver mode: Can’t configuring the channel of a RAW Socket if it’s already open |
| Description | Changing the channel while a RAW socket is open to receive by using SetSockOpt command can halt the Host. The command response on SetSockOpt doesn’t return. As a result, the host is might get stuck if it configured to blocking mode |
| Impact | Host might get stuck |
| Workaround | Close the socket and open it again with the correct channel |
| ********** | ****************************************************************************************************************************************** |
| ID | MCS00135767 |
| Title | Command sl_WlanSet is not working on Big Endian systems |
| Description | The command is not working well on Big Endian systems and will return an documented error. The command is used to set Tx power, Scan parameters, regulatory domain |
| Impact | Undocumented error and the command is not taking any affect |
| Workaround | Program the setting in the image (Uniflash) and avoid using the API |
| Remarks | Fix is expected in the next service pack release |
Host Known Issues
| ID | MCS00127283 |
| Title | Free RTOS OS is not stable when running UDP traffic and Ping |
| Description | Known issue with free RTOS that can cause deadlock |
| Impact | Deadlock in OS |
| Workaround | Use TI RTOS |
| ********** | ****************************************************************************************************************************************** |
| ID | MCS00130291 |
| Title | WPS PIN Connect might fail if pin code is not null-terminated |
| Description | If the PIN code from the HOST is not null terminated the string can be wrongly used and in some cases the connection doesn’t succeed |
| Impact | Connection doesn’t succeed |
| Workaround | Add null termination to the PIN code string |
| ********** | ****************************************************************************************************************************************** |
| ID | MCS00131563 |
| Title | Host: Set/Get time is limited up to year 2038 |
| Description | time.h (standard time library) is limiting the structure to a signed 32-bit integer, and this number is interpreted as the number of seconds since 00:00:00 UTC on 1 January 1970 |
| Impact | Low impact – Certifications that are bounded by date will expire after year 2038 |
| Workaround | N/A |
| ********** | ****************************************************************************************************************************************** |
| ID | MCU00015994 |
| Title | Reset observed when the APPS MCU enters LPDS after the nwp is shutdown |
| Description | A new API sl_Stop_WithNwpLpdsPoll was added to support a special use case of LPDS. This special use case is when the Networking sub-system has to be stopped before the APPS MCU enters LDPS. Note that the existing/standard sl_Stop API should not be used for this special use case. However, with this new API, there is issue observed. Issue: At times, reset of device is observed when the device enters LPDS. |
| Impact | Application which shuts down the NWP before entering LPDS |
| Workaround | N/A |
| ********** | ****************************************************************************************************************************************** |
| ID | CC3X20SDK-355 |
| Title | Host Driver - ‘Tiny’ mode not functional |
Power Management Known Issues
| ID | MCS00128947 |
| Title | In Enterprise network the device will Frequently Wakeup due to IPV4 BRDCST Rx frames |
| Description | On enterprise network there a lot of BRDCST packets |
| Impact | Increase in power consumption |
| Workaround | Add a filter to block the broadcast packets (will be different for each enterprise network) |
| Remarks | Fix is Not expected – the filter is specific to the network |
| ********** | ****************************************************************************************************************************************** |
Application Known Issues
| ID | MCS00128652 |
| Title | HTTP Server: When entering the internal web page with Huawei phone, GUI is zoomed in |
| Impact | Web page displayed incorrectly |
| Workaround | N/A |
| ********** | ****************************************************************************************************************************************** |
| ID | MCS00128658 |
| Title | HTTP Server: GUI is only displayed correctly after refresh in Nexus one phone |
| Impact | Web page displayed incorrectly |
| Workaround | N/A |
| ********** | ****************************************************************************************************************************************** |
| ID | MCS00128130 |
| Title | HTTP Server: With In Dolphin web application cursor is sometimes seen on two rows simultaneously |
| Impact | Double cursor |
| Workaround | N/A |
| ********** | ****************************************************************************************************************************************** |
| ID | MCS00128425 |
| Title | HTTP Server: Default Galaxy Tablet browser shows wrong authentication GUI |
| Impact | Wrong GUI is displayed |
| Workaround | Use different browser or disable authentication option |
| ********** | ****************************************************************************************************************************************** |
| ID | MCS00129384 |
| Title | HTTP Server: GUI - In IE7 browser, GUI boarder is truncated |
| Impact | Web page displayed incorrectly |
| Workaround | Use different browser |
| Remarks | Fix is Not Expected due to browser issue |
| ********** | ****************************************************************************************************************************************** |
| ID | MCS00129385 |
| Title | HTTP Server: On some mobile devices, “WiFi Connectivity” & “Profile Settings” are seen in two lines |
| Impact | Web page displayed incorrectly |
| Workaround | Use different browser |
| Remarks | Fix is Not Expected due to browser issue |
| ********** | ****************************************************************************************************************************************** |
| ID | MCS00129390 |
| Title | HTTP Server: On some mobile devices “some parameters were changed, System may require reset” is seen in two lines |
| Impact | Web page displayed incorrectly |
| Workaround | Use different browser |
| Remarks | Fix is Not Expected due to browser issue |
| ********** | ****************************************************************************************************************************************** |
| ID | MCS00129392 |
| Title | HTTP Server: On some mobile devices all tabs are merged together in browser |
| Impact | Web page displayed incorrectly |
| Workaround | Use different browser |
| Remarks | Fix is Not Expected due to browser issue |
| ********** | ****************************************************************************************************************************************** |
| ID | MCS00129393, MCS00129394, MCS00129397, MCS00129399, MCS00129401 |
| Title | HTTP Server: On some mobile devices lines and tabs are displayed incorrectly |
| Impact | Web page displayed incorrectly |
| Workaround | Use different browser |
| Remarks | Fix is Not Expected due to browser issue |
| ********** | ****************************************************************************************************************************************** |
| ID | MCS00130155 |
| Title | HTTP Server: Can’t configure the Default Gateway from the HTTP Server pages (with default tokens) |
| Impact | When working with default HTTP server pages, only default gateway can be used (192.168.1.xxx) |
| Workaround | Add proprietary token to modify the default Gateway for user pages |
| ********** | ****************************************************************************************************************************************** |
| ID | MCS00130240 |
| Title | DNS Server: In AP mode the internal DNS Server can’t be disabled |
| Impact | Can’t disabled the internal DNS server – can’t use external DNS server in AP mode |
| Workaround | DNS server in AP mode can’t be disabled – It can be bypassed using IP UDP Raw socket and disable the DHCP server |
| ********** | ****************************************************************************************************************************************** |
| ID | MCS00130241 |
| Title | HTTP Server: ‘AnyP2P’ and ‘Auto smart config’ policies can be changed only in station or P2P mode |
| Impact | Can’t change these specific configurations from the HTTP server in AP mode |
| Workaround | Change the configurations in STA mode |
| ********** | ****************************************************************************************************************************************** |
| ID | MCS00131120 |
| Title | HTTP Server: The System Up Time will get reset after 49Days |
| Impact | The displayed system up time won’t be accurate after 49days |
| Workaround | Get Time from sl_DevGet SL_DEVICE_GENERAL_CONFIGURATION_DATE_TIME |
| ********** | ****************************************************************************************************************************************** |
| ID | MCS00132268 |
| Title | NetApp: the Ping response is sent to the Host only on timeout |
| Description | The Ping response is sent to the Host only on timeout and not when the response was actually received |
| Impact | Med impact – The Ping reply received very fast but the Host will have to wait few seconds until it will know that it received correctly |
| Workaround | Set pingCommand.Flags = 1 - this will return response for every ping |
| ********** | ****************************************************************************************************************************************** |
| ID | MCS00131570 |
| Title | HTTP Server: Version number displayed in hexadecimal instead of decimal |
| Description | The HTTP Pages display the SW version number in hexadecimal instead of decimal |
| Impact | Low impact – SW version is not displayed correctly |
| Workaround | Convert the version numbers to Dec in the HTTP page (user files) |
| ********** | ****************************************************************************************************************************************** |
| ID | MCS00132159 |
| Title | DHCP Server: Same address is provided if pool is full |
| Description | When all of the addresses in the DHCP server pool are assigned, it will continue to offer and assign the last address in the pool to new connected station |
| Impact | Low impact – The DHCP lease time is not kept for the last disconnected STA. Since only one client can connect at a time to the AP the STA will still get an IP and connect |
| Workaround | N/A |
| ********** | ****************************************************************************************************************************************** |
| ID | MCS00132200 |
| Title | HTTP Server: SSID is limited to 16 characters |
| Description | From the HTTP web pages only the SSID string is limited to 16 characters instead of 32 characters |
| Impact | Med impact – Can’t add a SSID string longer than 16 characters from the HTTP using the device tokens |
| Workaround | Only the device tokens are limited – implementing user tokens for this field can overcome the issue |
| ********** | ****************************************************************************************************************************************** |
| ID | MCS00132203 |
| Title | HTTP Server: Password key is limited to 32 characters |
| Description | From the HTTP web pages only the password key is limited to 32 characters instead of 63 alphanumeric characters |
| Impact | Med impact – Can’t add a password key longer than 32 characters from the HTTP using the device tokens |
| Workaround | Only the device tokens are limited – implementing user tokens for this field can overcome the issue |
| ********** | ****************************************************************************************************************************************** |
| ID | MCS00132206 |
| Title | HTTP Server: Sending a page with no checkbox return “HTTP- No Content Length” message appears |
| Description | The internal web pages of the device returns “HTTP- No Content Length” if no checkbox is set |
| Impact | Low impact – HTTP pages design |
| Workaround | Insuring that the form will never be empty by adding to the HTML form (that is sent via an HTTP POST) an additional input (can be set with type=hidden) |
Driver Library Compatibility Known Issues
Version TivaWare_C_Series-2.1.4.178
| Title | IAR Compiler version 8.10 and later will generate linker warnings for pre-compiled driverlib.a library inside TivaWare version TivaWare_C_Series-2.1.4.178 |
| Description | The precompiled driverlib.a library was compiled using an EWARM IAR version of 7.80 or earlier in which the size of wchar_t datatype does not match the size in later IAR versions. See the IAR information Center for ARM for additional details. |
| Impact | Please refer to the IAR information Center for ARM for impact details |
| Resolution | To avoid any impact on the user application, the developer should recompile driverlib.a as a static library with a newer version (8.11 or later) in IAR. |
| ********** | ****************************************************************************************************************************************** |
Migrating from Host Driver Version 1.0.1.6 to Version 1.0.1.11
The new Host driver checks the host tick count to internally determine certain timeouts and error detection. To support the entire error handing mechanism, accurate timestamp service should be implemented in the Host application. For non-os applications, it is mandatory to support this option in the builds. This section describes the minimal changes required in order to use the new Host driver.
Event Handler
Ensure sl_GeneralEvtHdlr is registered. This handler will enable the application to be notified on general/fatal driver errors and therefore it is mandatory. If the application already registered to this handler the handler should check for the new errors.
System Time
The Host driver calls sl_GetSystemtime to get the current tick count. In addition, the macros: SL_TIMESTAMP_TICKS_IN_10_MILLISECONDS and SL_TIMESTAMP_MAX_VALUE must be defined in order for the internal host driver logic to trigger a timeout.