XDAIS
dais-x04
|
Defines the input arguments for all IVIDENC2 instance process function. More...
#include <ividenc2.h>
Data Fields | |
XDAS_Int32 | size |
XDAS_Int32 | inputID |
XDAS_Int32 | control |
Defines the input arguments for all IVIDENC2 instance process function.
size
parameter. size
field must be correctly set by the caller. See https://processors.wiki.ti.com/index.php/Extending_data_structures_in_XDM for more details.XDAS_Int32 IVIDENC2_InArgs::size |
Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.
XDAS_Int32 IVIDENC2_InArgs::inputID |
Identifier to attach with the corresponding input frames to be encoded.
XDAS_Int32 IVIDENC2_InArgs::control |
Encoder control operations