XDAIS
dais-x04
|
Defines the input arguments for all IVIDENC1 instance process function. More...
#include <ividenc1.h>
Data Fields | |
XDAS_Int32 | size |
XDAS_Int32 | inputID |
XDAS_Int32 | topFieldFirstFlag |
Defines the input arguments for all IVIDENC1 instance process function.
size
parameter. size
field must be correctly set by the caller. See https://processors.wiki.ti.com/index.php/Extending_data_structures_in_XDM for more details.XDAS_Int32 IVIDENC1_InArgs::size |
Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.
XDAS_Int32 IVIDENC1_InArgs::inputID |
Identifier to attach with the corresponding encoded bitstream frames.
XDAS_Int32 IVIDENC1_InArgs::topFieldFirstFlag |
Flag to indicate the field order in interlaced content.