XDAIS
dais-x04
|
This structure defines the algorithm parameters that can be modified after creation via IVIDDEC3_Fxns.control() calls. More...
#include <ividdec3.h>
Data Fields | |
XDAS_Int32 | size |
XDAS_Int32 | decodeHeader |
Decode entire access unit or only header. | |
XDAS_Int32 | displayWidth |
XDAS_Int32 | frameSkipMode |
Video frame skip features for video decoder. | |
XDAS_Int32 | newFrameFlag |
XDM_DataSyncPutFxn | putDataFxn |
XDM_DataSyncHandle | putDataHandle |
XDM_DataSyncGetFxn | getDataFxn |
XDM_DataSyncHandle | getDataHandle |
XDM_DataSyncPutBufferFxn | putBufferFxn |
XDM_DataSyncHandle | putBufferHandle |
XDAS_Int32 | lateAcquireArg |
This structure defines the algorithm parameters that can be modified after creation via IVIDDEC3_Fxns.control() calls.
size
parameter. size
field must be correctly set by the caller. See https://processors.wiki.ti.com/index.php/Extending_data_structures_in_XDM for more details.XDAS_Int32 IVIDDEC3_DynamicParams::size |
Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.
XDAS_Int32 IVIDDEC3_DynamicParams::decodeHeader |
Decode entire access unit or only header.
XDAS_Int32 IVIDDEC3_DynamicParams::displayWidth |
Pitch. If set to zero, use the decoded image width. Else, use given display width in pixels. Display width has to be greater than or equal to image width.
XDAS_Int32 IVIDDEC3_DynamicParams::frameSkipMode |
Video frame skip features for video decoder.
XDAS_Int32 IVIDDEC3_DynamicParams::newFrameFlag |
Flag to indicate that the algorithm should start a new frame.
XDM_DataSyncPutFxn IVIDDEC3_DynamicParams::putDataFxn |
Optional datasync "put data" function.
XDM_DataSyncHandle IVIDDEC3_DynamicParams::putDataHandle |
Datasync "put data" handle
XDM_DataSyncGetFxn IVIDDEC3_DynamicParams::getDataFxn |
Datasync "get data" function.
XDM_DataSyncHandle IVIDDEC3_DynamicParams::getDataHandle |
Datasync "get data" handle
getDataFxn
.XDM_DataSyncPutBufferFxn IVIDDEC3_DynamicParams::putBufferFxn |
Datasync "put buffer" function.
XDM_DataSyncHandle IVIDDEC3_DynamicParams::putBufferHandle |
Datasync "put buffer" handle
XDAS_Int32 IVIDDEC3_DynamicParams::lateAcquireArg |
Argument used during late acquire.
lateAcquireArg
value when requesting resources (i.e. during their call to acquire() when requesting the resource).