XDAIS  dais-x04
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Groups Pages
Data Fields
IVIDANALYTICS_InArgs Struct Reference

Defines the input arguments for all IVIDANALYTICS instance process function. More...

#include <ividanalytics.h>

Collaboration diagram for IVIDANALYTICS_InArgs:
Collaboration graph

Data Fields

XDAS_Int32 size
XDM_Date date

Detailed Description

Defines the input arguments for all IVIDANALYTICS instance process function.

Remarks:
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See https://processors.wiki.ti.com/index.php/Extending_data_structures_in_XDM for more details.
See also:
IVIDANALYTICS_Fxns::process()

Field Documentation

XDAS_Int32 IVIDANALYTICS_InArgs::size

Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.

XDM_Date IVIDANALYTICS_InArgs::date

Set the current time.


The documentation for this struct was generated from the following file:
Copyright 2013, Texas Instruments Incorporated