XDAIS
dais-x04
|
Defines the run time output arguments for all ISPHENC1 instance objects. More...
#include <isphenc1.h>
Data Fields | |
XDAS_Int16 | size |
XDAS_Int16 | frameType |
XDAS_Int32 | extendedError |
Extended error information. |
Defines the run time output arguments for all ISPHENC1 instance objects.
size
parameter. size
field must be correctly set by the caller. See https://processors.wiki.ti.com/index.php/Extending_data_structures_in_XDM for more details.XDAS_Int16 ISPHENC1_OutArgs::size |
Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.
XDAS_Int16 ISPHENC1_OutArgs::frameType |
Encoder frame types.
XDAS_Int32 ISPHENC1_OutArgs::extendedError |
Extended error information.