XDAIS
dais-x04
|
Defines the run time output arguments for all ISPHDEC instance objects. More...
#include <isphdec.h>
Data Fields | |
XDAS_Int32 | size |
XDAS_Int32 | mode |
Defines the run time output arguments for all ISPHDEC instance objects.
size
parameter. size
field must be correctly set by the caller. See https://processors.wiki.ti.com/index.php/Extending_data_structures_in_XDM for more details.XDAS_Int32 ISPHDEC_OutArgs::size |
Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.
XDAS_Int32 ISPHDEC_OutArgs::mode |
Speech voice mode. See ISPEECH_VoiceMode.