XDAIS
dais-x04
|
Defines the creation time parameters for all IAUDENC1 instance objects. More...
#include <iaudenc1.h>
Defines the creation time parameters for all IAUDENC1 instance objects.
size
parameter. size
field must be correctly set by the caller. See https://processors.wiki.ti.com/index.php/Extending_data_structures_in_XDM for more details. XDAS_Int32 IAUDENC1_Params::size |
Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.
XDAS_Int32 IAUDENC1_Params::sampleRate |
Sampling Frequency in Hz. For example, if the sampling frequency is 44.1 kHz, this field will be 44100.
XDAS_Int32 IAUDENC1_Params::bitRate |
Average bit rate, in bits per second.
XDAS_Int32 IAUDENC1_Params::channelMode |
Input Channel Mode.
XDAS_Int32 IAUDENC1_Params::dataEndianness |
Endianness of input data.
XDAS_Int32 IAUDENC1_Params::encMode |
Encoding mode.
XDAS_Int32 IAUDENC1_Params::inputFormat |
Input format block/interleaved.
XDAS_Int32 IAUDENC1_Params::inputBitsPerSample |
Number of input bits per output sample. For example, if there are 16 bits per PCM input sample, this should be set to 16.
XDAS_Int32 IAUDENC1_Params::maxBitRate |
Maximum bit rate in case of VBR. Some of the encoders allow you to specify max bit rate in case of VBR mode
XDAS_Int32 IAUDENC1_Params::dualMonoMode |
Mode to indicate type of Dual Mono. Applicable only if channelMode is dualMono
XDAS_Int32 IAUDENC1_Params::crcFlag |
Flag indicating whether the encoder should insert CRC bits into the bitstream or not.
Valid values for this field are XDAS_TRUE and XDAS_FALSE.
XDAS_Int32 IAUDENC1_Params::ancFlag |
Ancillary Data Flag.
Valid values for this field are XDAS_TRUE and XDAS_FALSE.
XDAS_Int32 IAUDENC1_Params::lfeFlag |
Flag indicating whether LFE channel data is present or not in the input.
Valid values for this field are XDAS_TRUE and XDAS_FALSE.