XDAIS
dais-x04
|
Defines instance status parameters (read-only). More...
#include <iauddec1.h>
Defines instance status parameters (read-only).
size
parameter. size
field must be correctly set by the caller. See https://processors.wiki.ti.com/index.php/Extending_data_structures_in_XDM for more details.XDAS_Int32 IAUDDEC1_Status::size |
Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.
XDAS_Int32 IAUDDEC1_Status::extendedError |
Extended error information.
XDM1_SingleBufDesc IAUDDEC1_Status::data |
Buffer descriptor for data passing.
XDAS_Int32 IAUDDEC1_Status::validFlag |
Reflects the validity of this status structure.
XDAS_Int32 IAUDDEC1_Status::lfeFlag |
Flag indicating the presence of LFE channel in the output. When the LFE channel is not in the output, this is set to XDAS_FALSE.
Valid values for this field are XDAS_TRUE and XDAS_FALSE.
XDAS_Int32 IAUDDEC1_Status::bitRate |
Average bit rate, in bits per second.
XDAS_Int32 IAUDDEC1_Status::sampleRate |
Sampling frequency, in Hz. For example, if the sampling frequency is 44.1 kHz, this field will be 44100.
XDAS_Int32 IAUDDEC1_Status::channelMode |
Output Channel Configuration.
XDAS_Int32 IAUDDEC1_Status::pcmFormat |
Output PCM Format Block/Interleaved.
XDAS_Int32 IAUDDEC1_Status::numSamples |
Number of samples in the output.
XDAS_Int32 IAUDDEC1_Status::outputBitsPerSample |
Number of bits per output sample. For example, if the value of the field is 16, there are 16 output bits per PCM sample.
XDM_AlgBufInfo IAUDDEC1_Status::bufInfo |
Input and output buffer information.
XDAS_Int32 IAUDDEC1_Status::dualMonoMode |
Mode to indicate type of Dual Mono. Only used in case of Dual Mono Output.