XDAIS
dais-x04
|
IRES Resource Protocol Definitions - IRES Resource.
#include "ialg.h"
Go to the source code of this file.
Data Structures | |
struct | IRES_ProtocolRevision |
Protocol revision type. Used to ensure the given 'protocol' revision can be validated. More... | |
struct | IRES_ProtocolArgs |
Abstract Protocol Arguments structure definition. Actual arguments passed by the algorithm to request a resource from a specific IRES Protocol will extend and supply the concrete definitions. More... | |
struct | IRES_ResourceDescriptor |
Descriptor to Logical Resource. More... | |
struct | IRES_Properties |
Abstract Resource Properties structure/pointer definition. Actual resource protocol will supply the concrete property definitions. The list of attributes for the actual resource will expose the relevant features that needs to be known to a client to use the resource, such as: resource register base addresses and offsets, critical register and memory region addresses, ... More... | |
struct | IRES_Obj |
IRES_Obj holds the private state associated with each logical resource. More... | |
enum | IRES_Status { IRES_OK = 0, IRES_EALG = 1, IRES_EEXISTS = 2, IRES_EFAIL = 3, IRES_EINIT = 4, IRES_ENOINIT = 5, IRES_ENOMEM = 6, IRES_ENORESOURCE = 7, IRES_ENOTFOUND = 8 } |
IRES_Status defines the standard error and success codes returned by IRES APIs. More... | |
enum | IRES_RequestMode { IRES_SCRATCH, IRES_PERSISTENT, IRES_LATEACQUIRE } |
Mode in which resources can be requested. More... | |
typedef enum IRES_Status | IRES_Status |
IRES_Status defines the standard error and success codes returned by IRES APIs. | |
typedef struct IRES_ProtocolRevision | IRES_ProtocolRevision |
Protocol revision type. Used to ensure the given 'protocol' revision can be validated. | |
typedef enum IRES_RequestMode | IRES_RequestMode |
Mode in which resources can be requested. | |
typedef struct IRES_ProtocolArgs | IRES_ProtocolArgs |
Abstract Protocol Arguments structure definition. Actual arguments passed by the algorithm to request a resource from a specific IRES Protocol will extend and supply the concrete definitions. | |
typedef struct IRES_ResourceDescriptor | IRES_ResourceDescriptor |
Descriptor to Logical Resource. | |
typedef struct IRES_Properties | IRES_Properties |
Abstract Resource Properties structure/pointer definition. Actual resource protocol will supply the concrete property definitions. The list of attributes for the actual resource will expose the relevant features that needs to be known to a client to use the resource, such as: resource register base addresses and offsets, critical register and memory region addresses, ... | |
typedef struct IRES_Obj | IRES_Obj |
IRES_Obj holds the private state associated with each logical resource. | |
typedef struct IRES_Obj * | IRES_Handle |
Handle to "logical" resource. |