XDAIS  dais-x04
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Groups Pages
Enumerations
ISPEECH1_ILBC - XDM Speech Interface (iLBC)

Enumerations

enum  ISPEECH1_ILBC_CodecSelect {
  ISPEECH1_ILBC_CODECSELECT_20MS = 0,
  ISPEECH1_ILBC_CODECSELECT_30MS = 1,
  ISPEECH1_ILBC_CODECSELECT_DEFAULT = ISPEECH1_ILBC_CODECSELECT_20MS
}
 Codec selection. More...

Detailed Description

This is the XDM speech interface shared between the various iLBC codecs.


Enumeration Type Documentation

Codec selection.

Remarks:
This parameter is used to select 20ms/30ms frame size for iLBC
Enumerator:
ISPEECH1_ILBC_CODECSELECT_20MS 

20MS frame size

ISPEECH1_ILBC_CODECSELECT_30MS 

30MS frame size

ISPEECH1_ILBC_CODECSELECT_DEFAULT 

Default setting.

Copyright 2013, Texas Instruments Incorporated