XDAIS  dais-x04
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Groups Pages
Data Structures | Macros | Typedefs
IAUDDEC1 - XDM Audio Decoder Interface

Data Structures

struct  IAUDDEC1_Obj
 This must be the first field of all IAUDDEC1 instance objects. More...
struct  IAUDDEC1_Params
 Defines the creation time parameters for all IAUDDEC1 instance objects. More...
struct  IAUDDEC1_DynamicParams
 This structure defines the codec parameters that can be modified after creation via control() calls. More...
struct  IAUDDEC1_InArgs
 Defines the input arguments for all IAUDDEC1 instance process function. More...
struct  IAUDDEC1_Status
 Defines instance status parameters (read-only). More...
struct  IAUDDEC1_OutArgs
 Defines the run time output arguments for all IAUDDEC1 instance objects. More...
struct  IAUDDEC1_Fxns
 Defines all of the operations on IAUDDEC1 objects. More...

Macros

#define IAUDDEC1_EOK   XDM_EOK
 
#define IAUDDEC1_EFAIL   XDM_EFAIL
 
#define IAUDDEC1_EUNSUPPORTED   XDM_EUNSUPPORTED
 

Typedefs

typedef struct IAUDDEC1_Obj IAUDDEC1_Obj
 This must be the first field of all IAUDDEC1 instance objects.
typedef struct IAUDDEC1_ObjIAUDDEC1_Handle
 Opaque handle to an IAUDDEC1 objects.
typedef struct IAUDDEC1_Params IAUDDEC1_Params
 Defines the creation time parameters for all IAUDDEC1 instance objects.
typedef struct
IAUDDEC1_DynamicParams 
IAUDDEC1_DynamicParams
 This structure defines the codec parameters that can be modified after creation via control() calls.
typedef struct IAUDDEC1_InArgs IAUDDEC1_InArgs
 Defines the input arguments for all IAUDDEC1 instance process function.
typedef struct IAUDDEC1_Status IAUDDEC1_Status
 Defines instance status parameters (read-only).
typedef struct IAUDDEC1_OutArgs IAUDDEC1_OutArgs
 Defines the run time output arguments for all IAUDDEC1 instance objects.
typedef IALG_Cmd IAUDDEC1_Cmd
 Defines the control commands for the IAUDDEC1 module.
typedef struct IAUDDEC1_Fxns IAUDDEC1_Fxns
 Defines all of the operations on IAUDDEC1 objects.

Detailed Description

This is the XDM IAUDDEC1 Audio Decoder Interface.


Macro Definition Documentation

#define IAUDDEC1_EOK   XDM_EOK

Success.

#define IAUDDEC1_EFAIL   XDM_EFAIL

General failure.

#define IAUDDEC1_EUNSUPPORTED   XDM_EUNSUPPORTED

Request is unsupported.


Typedef Documentation

typedef struct IAUDDEC1_Obj IAUDDEC1_Obj

This must be the first field of all IAUDDEC1 instance objects.

typedef struct IAUDDEC1_Obj* IAUDDEC1_Handle

Opaque handle to an IAUDDEC1 objects.

Defines the creation time parameters for all IAUDDEC1 instance objects.

Remarks:
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See https://processors.wiki.ti.com/index.php/Extending_data_structures_in_XDM for more details.

This structure defines the codec parameters that can be modified after creation via control() calls.

Remarks:
It is not necessary that a given implementation support all dynamic parameters to be configurable at run time. If a particular algorithm does not support run-time updates to a parameter that the application is attempting to change at runtime, it may indicate this as an error.
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See https://processors.wiki.ti.com/index.php/Extending_data_structures_in_XDM for more details.
See also:
IAUDDEC1_Fxns::control()

Defines the input arguments for all IAUDDEC1 instance process function.

Remarks:
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See https://processors.wiki.ti.com/index.php/Extending_data_structures_in_XDM for more details.
See also:
IAUDDEC1_Fxns::process()

Defines instance status parameters (read-only).

Remarks:
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See https://processors.wiki.ti.com/index.php/Extending_data_structures_in_XDM for more details.
See also:
IAUDDEC1_Fxns::control()

Defines the run time output arguments for all IAUDDEC1 instance objects.

Remarks:
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See https://processors.wiki.ti.com/index.php/Extending_data_structures_in_XDM for more details.
See also:
IAUDDEC1_Fxns::process()

Defines the control commands for the IAUDDEC1 module.

Remarks:
This ID can be extended in IMOD interface for additional controls.
See also:
XDM_CmdId
IAUDDEC1_Fxns::control()
typedef struct IAUDDEC1_Fxns IAUDDEC1_Fxns

Defines all of the operations on IAUDDEC1 objects.

Copyright 2013, Texas Instruments Incorporated