isphdec1.h File Reference


Detailed Description

This header defines all types, constants, and functions shared by all implementations of the speech decoder algorithms.

#include <ti/xdais/ialg.h>
#include <ti/xdais/xdas.h>
#include "xdm.h"
#include "ispeech1.h"
Include dependency graph for isphdec1.h:

Go to the source code of this file.

Data Structures

struct  ISPHDEC1_Obj
 This must be the first field of all ISPHDEC1 instance objects. More...
struct  ISPHDEC1_Params
 Defines the creation time parameters for all ISPHDEC1 instance objects. More...
struct  ISPHDEC1_DynamicParams
 This structure defines the codec parameters that can be modified after creation via ISPHDEC1_Fxns.control(). More...
struct  ISPHDEC1_InArgs
 Defines the input arguments for all ISPHDEC1 instance process function. More...
struct  ISPHDEC1_Status
 Defines instance status parameters. More...
struct  ISPHDEC1_OutArgs
 Defines the run time output arguments for all ISPHDEC1 instance objects. More...
struct  ISPHDEC1_Fxns
 Defines all of the operations on ISPHDEC1 objects. More...

Defines

#define ISPHDEC1_EOK   XDM_EOK
#define ISPHDEC1_EFAIL   XDM_EFAIL
#define ISPHDEC1_EUNSUPPORTED   XDM_EUNSUPPORTED

Typedefs

typedef struct ISPHDEC1_ObjISPHDEC1_Handle
 Opaque handle to an ISPHDEC1 objects.
typedef IALG_Cmd ISPHDEC1_Cmd
 Defines the control commands for the ISPHDEC1 module.

Enumerations

enum  ISPHDEC1_FrameType {
  ISPHDEC1_FTYPE_SPEECHGOOD = 0,
  ISPHDEC1_FTYPE_SIDUPDATE = 1,
  ISPHDEC1_FTYPE_NODATA = 2,
  ISPHDEC1_FTYPE_SPEECHLOST = 3,
  ISPHDEC1_FTYPE_DEGRADED = 4,
  ISPHDEC1_FTYPE_BAD = 5,
  ISPHDEC1_FTYPE_SIDFIRST = 6,
  ISPHDEC1_FTYPE_SIDBAD = 7,
  ISPHDEC1_FTYPE_ONSET = 8
}
 

Decoder frame types.

More...
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2010, Texas Instruments Incorporated