Introduction, Documentation, What's New, Upgrade Info, Compatibility Information, Validation Info, Known Issues, Examples, Version Information, Technical Support.
This XDAIS product contains the DSP Algorithm Interface Standard specification and related documentation and examples.
The following packages are included in this release:
In addition several example packages are also provided.
The following documentation is available:
In addition, users are encouraged to monitor (and contribute to!) the TI Embedded Processors Wiki.
Release notes from previous releases are also available in the relnotes_archive directory.
The following significant changes have been made since 5.00
ID | Headline |
SDOCM00067036 | ti/xdais/qualiti/README.txt file refers to non-existent scripts |
ID | Headline |
SDOCM00068904 | Update GenAlg's templates based on IUNIVERSAL users feedback |
ID | Headline |
SDOCM00064152 | GenAlg Wizard must check xdctools version |
ID | Headline |
SDOCM00064248 | Add com.ti.dvt.tools.menu addition to xdais eclipse plugin |
SDOCM00064018 | Remove grep from QualiTI (to reduce size and simplify licensing) |
ID | Headline |
ID | Headline |
SDOCM00061294 | Allow QualiTI to use relative paths (relative to the .qti file) to set basedir field |
SDOCM00046986 | IALG::algInit status/return codes should be well-specified and allow extensions of error or success codes |
SDOCM00062286 | Create a wizard to generate XDM algorithm packages |
SDOCM00061326 | Add ".econst" and ".ebss" to QualiTI's Rule 13-based list of approved section names |
SDOCM00061304 | IRES_RequestMode should also support the IRES_LATEACQUIRE mode for acquiring resources. |
ID | Headline |
ID | Headline |
ID | Headline |
SDOCM00053259 | chm API Reference Guide search doesn't work |
SDOCM00054295 | QualiTI fails on Windows if the tool paths contain spaces |
ID | Headline |
SDOCM00054214 | Add 674 target support to QualiTI |
SDOCM00054216 | Add QualiTI -g option to support launching GUI with a given filename |
ID | Headline |
SDSCM00050966 | Add more Chroma format enums |
ID | Headline |
SDOCM00049826 | Change Licensing to BSD |
SDOCM00050452 | Add the ability for extending XDM-defined enums |
ID | Headline |
SDSCM00024690 | QualiTI doesn't catch not-an-archive Rule 15 if in an XDC package |
SDSCM00025188 | QualiTI needs to handle _IALG symbols when they're const |
SDSCM00025559 | viddec2_copy example has incorrect symbol in header |
ID | Headline |
SDSCM00024172 | Examples which use package.bld should have explicit Build and Pkg assignments |
SDSCM00025558 | IVIDDEC2 spec should state that valid bufs can be returned when non-fatal EFAIL is returned from process() |
SDSCM00026170 | Add IUNIVERSAL to XDM spec |
ID | Headline |
SDSCM00014553 | Remove dependency on BIOS types in idma3.h |
SDSCM00013817 | Deprecate XDM_ERUNTIME for XDM 1.00 |
SDSCM00013698 | Add bitrate fields to several speech1 structs and more frame types |
SDSCM00013621 | XDM 1.0 speech inArgs should have "size" field for extensibility |
SDSCM00013568 | XDM user guide needs to discuss extension of parameter ad argument structions |
SDSCM00013537 | ISPHENC1_FrameType enums have inconsistant prefix |
SDSCM00011273 | When including public header files in XDAIS, one needs to use "full qualified package path" |
SDSCM00005724 | XDAIS Documentation needs to be update to support IDMA3 |
The XDAIS packages are available in the "packages/" subdirectory of the product. If you have a previous release of the XDAIS product, you can install this release next to it, and modify your builds to use this newer release.
If you're using the DVEVM, this can be done by setting the XDAIS_INSTALL_DIR variable in the Rules.make file at the top of the DVEVM distribution directory.
None
Note, if you're upgrading from a release earlier than XDAIS 6.24, be sure to review the Upgrade section for each of the releases between your current XDAIS release and this one. Previous release notes are available in the relnotes_archive directory.
The details provided below describe each package's compatibility with the previous release (6.24).
If migrating from a release prior to XDAIS 6.24, consult previous releases available in the relnotes_archive directory.
Compatibility keys are intentionally independent of Marketing product numbers and are intended to:
Compatibility keys are composed of 3 comma-delimited numbers - M,S,R - where:
This release was validated against using the following components:
See the MFP Known Issues wiki article for issues found after these release notes were compiled.
XDAIS examples and instructions are located in the "examples" directory.
This product's version follows a version format, M.mm.pp.bb, where M is a single digit Major number, mm is 2 digit minor number, pp is a 2 digit patch number, and b is an unrestricted set of digits used as an incrementing build counter.
To support multiple side-by-side installations of the product, the product version is encoded in the top level directory, ex. xdais_6_25_02_11.
Subsequent releases of patch upgrades will be identified by the patch number, ex. XDAIS 6.25.01 with directory xdais_6_25_01_XX. Typically, these patches only include critical bug fixes.
For technical support, contact softwaresupport@ti.com
Check the following web site for updates: https://software-dl.ti.com/dsps/dsps_public_sw/sdo_sb/targetcontent/xdais/index.html
Last updated: May 4, 2010