129 #ifndef ti_drivers_spi_SPIEUSCIADMA__include
130 #define ti_drivers_spi_SPIEUSCIADMA__include
139 #include <ti/sysbios/knl/Semaphore.h>
uint8_t rxDMASourceTrigger
Definition: SPIEUSCIADMA.h:221
void(* SPI_CallbackFxn)(SPI_Handle handle, SPI_Transaction *transaction)
The definition of a callback function used by the SPI driver when used in SPI_MODE_CALLBACK.
Definition: SPI.h:282
SPI_Transaction * transaction
Definition: SPIEUSCIADMA.h:241
SPIEUSCIADMA Hardware attributes.
Definition: SPIEUSCIADMA.h:204
uint32_t dmaBaseAddr
Definition: SPIEUSCIADMA.h:217
SPI_TransferMode
SPI transfer mode determines the whether the SPI controller operates synchronously or asynchronously...
Definition: SPI.h:316
Semaphore_Struct transferComplete
Definition: SPIEUSCIADMA.h:236
uint8_t defaultTxBufValue
Definition: SPIEUSCIADMA.h:214
SPI_CallbackFxn transferCallbackFxn
Definition: SPIEUSCIADMA.h:239
The definition of a SPI function table that contains the required set of functions to control a speci...
Definition: SPI.h:402
uint32_t baseAddr
Definition: SPIEUSCIADMA.h:206
uint16_t bitOrder
Definition: SPIEUSCIADMA.h:210
bool isOpen
Definition: SPIEUSCIADMA.h:234
uint8_t txDMASourceTrigger
Definition: SPIEUSCIADMA.h:225
struct SPIEUSCIADMA_Object SPIEUSCIADMA_Object
SPIEUSCIADMA Object.
A SPI_Transaction data structure is used with SPI_transfer(). It indicates how many SPI_FrameFormat f...
Definition: SPI.h:262
uint8_t clockSource
Definition: SPIEUSCIADMA.h:208
struct SPIEUSCIADMA_Object * SPIEUSCIADMA_Handle
SPI_TransferMode transferMode
Definition: SPIEUSCIADMA.h:238
const SPI_FxnTable SPIEUSCIADMA_fxnTable
uint8_t * scratchBufPtr
Definition: SPIEUSCIADMA.h:212
uint8_t rxDMAChannelIndex
Definition: SPIEUSCIADMA.h:219
uint8_t txDMAChannelIndex
Definition: SPIEUSCIADMA.h:223
struct SPIEUSCIADMA_HWAttrs SPIEUSCIADMA_HWAttrs
SPIEUSCIADMA Hardware attributes.
SPIEUSCIADMA Object.
Definition: SPIEUSCIADMA.h:233