52 #ifndef ti_drivers_sdspi_SDSPITiva__include
53 #define ti_drivers_sdspi_SDSPITiva__include
uint32_t driveNumber
Definition: SDSPITiva.h:191
DSTATUS diskState
Definition: SDSPITiva.h:192
SDSPITiva Object.
Definition: SDSPITiva.h:190
SDSPIBaseAddrType baseAddr
Definition: SDSPITiva.h:162
SDSPITiva Hardware attributes.
Definition: SDSPITiva.h:160
uint32_t portCS
Definition: SDSPITiva.h:180
The definition of a SDSPI function table that contains the required set of functions to control a spe...
Definition: SDSPI.h:241
const SDSPI_FxnTable SDSPITiva_fxnTable
struct SDSPITiva_Object * SDSPITiva_Handle
unsigned long SDSPIBaseAddrType
Definition: SDSPITiva.h:98
SDSPITiva_CardType cardType
Definition: SDSPITiva.h:193
Definition: SDSPITiva.h:112
BYTE DSTATUS
Definition: diskio.h:19
Definition: SDSPITiva.h:109
struct SDSPITiva_Object SDSPITiva_Object
SDSPITiva Object.
uint32_t portMOSI
Definition: SDSPITiva.h:175
FATFS filesystem
Definition: SDSPITiva.h:195
uint32_t portSCK
Definition: SDSPITiva.h:165
struct SDSPITiva_HWAttrs SDSPITiva_HWAttrs
uint32_t pinMOSI
Definition: SDSPITiva.h:177
unsigned long SDSPIDataType
Definition: SDSPITiva.h:99
uint32_t portMISO
Definition: SDSPITiva.h:170
SDSPITiva_CardType
SD Card type inserted.
Definition: SDSPITiva.h:108
uint32_t pinCS
Definition: SDSPITiva.h:182
uint32_t pinSCK
Definition: SDSPITiva.h:167
Definition: SDSPITiva.h:110
uint32_t pinMISO
Definition: SDSPITiva.h:172
uint32_t bitRate
Definition: SDSPITiva.h:194
Definition: SDSPITiva.h:111