258 #ifndef ti_drivers_crypto_CryptoCC26XX__include
259 #define ti_drivers_crypto_CryptoCC26XX__include
268 #include <driverlib/crypto.h>
298 #define CRYPTOCC26XX_TIMEOUT 20
300 #define CRYPTOCC26XX_STATUS_SUCCESS 0
301 #define CRYPTOCC26XX_STATUS_ERROR -1
302 #define CRYPTOCC26XX_STATUS_UNDEFINEDCMD -2
304 #define CRYPTOCC26XX_OP_AES_CCM_ENCRYPT 0
305 #define CRYPTOCC26XX_OP_AES_CCM_ENCRYPT_AAD_ONLY 1
306 #define CRYPTOCC26XX_OP_AES_CCM_DECRYPT 2
307 #define CRYPTOCC26XX_OP_AES_CCM_DECRYPT_AAD_ONLY 3
308 #define CRYPTOCC26XX_OP_AES_ECB_ENCRYPT 4
309 #define CRYPTOCC26XX_OP_AES_ECB_DECRYPT 5
310 #define CRYPTOCC26XX_OP_AES_CBC_ENCRYPT 6
311 #define CRYPTOCC26XX_OP_AES_CBC_DECRYPT 7
314 #define CRYPTOCC26XX_OP_AES_CCM CRYPTOCC26XX_OP_AES_CCM_ENCRYPT
315 #define CRYPTOCC26XX_OP_AES_CCM_NOCRYPT CRYPTOCC26XX_OP_AES_CCM_ENCRYPT_AAD_ONLY
316 #define CRYPTOCC26XX_OP_AES_CCMINV CRYPTOCC26XX_OP_AES_CCM_DECRYPT
317 #define CRYPTOCC26XX_OP_AES_CCMINV_NOCRYPT CRYPTOCC26XX_OP_AES_CCM_DECRYPT_AAD_ONLY
318 #define CRYPTOCC26XX_OP_AES_ECB CRYPTOCC26XX_OP_AES_ECB_ENCRYPT
319 #define CRYPTOCC26XX_OP_AES_ECB_NOCRYPT CRYPTOCC26XX_OP_AES_ECB_DECRYPT
326 #define ti_sysbios_family_arm_m3_Hwi__nolocalnames
327 #include <ti/sysbios/family/arm/m3/Hwi.h>
328 #include <ti/sysbios/knl/Semaphore.h>
543 ti_sysbios_family_arm_m3_Hwi_Struct
hwi;
772 #undef ti_sysbios_family_arm_m3_Hwi__nolocalnames
int CryptoCC26XX_allocateKey(CryptoCC26XX_Handle handle, CryptoCC26XX_KeyLocation keyLocation, const uint32_t *keySrc)
Function that allocates key, writes key into key store RAM and returns a handle to CryptoCC26XX Key...
CryptoCC26XX Transaction.
Definition: CryptoCC26XX.h:413
Semaphore_Struct waitSem
Definition: CryptoCC26XX.h:545
CryptoCC26XX Global Configuration.
Definition: CryptoCC26XX.h:549
CryptoCC26XX_Transaction * currentTransact
Definition: CryptoCC26XX.h:533
void CryptoCC26XX_Params_init(CryptoCC26XX_Params *params)
Function to initialize the CryptoCC26XX_Params struct to its defaults.
CryptoCC26XX AES-CCM Transaction.
Definition: CryptoCC26XX.h:425
struct CryptoCC26XX_Object CryptoCC26XX_Object
CryptoCC26XX Object.
CryptoCC26XX_Operation opType
Definition: CryptoCC26XX.h:463
int CryptoCC26XX_close(CryptoCC26XX_Handle handle)
Function to closes a given CryptoCC26XX peripheral specified by the CryptoCC26XX handle.
void * msgOut
Definition: CryptoCC26XX.h:434
struct CryptoCC26XX_AESCCM_Transaction CryptoCC26XX_AESCCM_Transaction
CryptoCC26XX AES-CCM Transaction.
CryptoCC26XX_Transaction * tailPtr
Definition: CryptoCC26XX.h:537
CryptoCC26XX Parameters.
Definition: CryptoCC26XX.h:393
uint8_t keyIndex
Definition: CryptoCC26XX.h:465
void * msgIn
Definition: CryptoCC26XX.h:451
CryptoCC26XX_Operation opType
Definition: CryptoCC26XX.h:426
Definition: CryptoCC26XX.h:379
uint8_t CryptoCC26XX_Operation
CryptoCC26XX Operation Type.
Definition: CryptoCC26XX.h:369
uint8_t fieldLength
Definition: CryptoCC26XX.h:435
Definition: CryptoCC26XX.h:382
CryptoCC26XX_Operation opType
Definition: CryptoCC26XX.h:414
uint8_t data[]
Definition: CryptoCC26XX.h:416
Definition: CryptoCC26XX.h:346
CryptoCC26XX_Transaction * headPtr
Definition: CryptoCC26XX.h:536
CryptoCC26XX_Operation opType
Definition: CryptoCC26XX.h:447
int CryptoCC26XX_loadKey(CryptoCC26XX_Handle handle, int keyIndex, const uint32_t *keySrc)
Function that writes a given key into a key store.
void * msgOut
Definition: CryptoCC26XX.h:467
uint8_t keyIndex
Definition: CryptoCC26XX.h:428
char * nonce
Definition: CryptoCC26XX.h:431
void * msgOut
Definition: CryptoCC26XX.h:452
struct CryptoCC26XX_Config CryptoCC26XX_Config
CryptoCC26XX Global Configuration.
void CryptoCC26XX_Transac_init(CryptoCC26XX_Transaction *trans, CryptoCC26XX_Operation opType)
Function to initialize the CryptoCC26XX_Transaction struct to its defaults.
int CryptoCC26XX_releaseKey(CryptoCC26XX_Handle handle, int *keyIndex)
Function that releases the specified CryptoCC26XX Key.
Definition: CryptoCC26XX.h:385
char * header
Definition: CryptoCC26XX.h:433
CryptoCC26XX Hardware Attributes.
Definition: CryptoCC26XX.h:501
Power_NotifyObj cryptoNotiObj
Definition: CryptoCC26XX.h:540
int openCnt
Definition: CryptoCC26XX.h:530
ti_sysbios_family_arm_m3_Hwi_Struct hwi
Definition: CryptoCC26XX.h:543
Definition: CryptoCC26XX.h:384
void const * hwAttrs
Definition: CryptoCC26XX.h:554
uint16_t headerLength
Definition: CryptoCC26XX.h:437
Definition: CryptoCC26XX.h:352
uint16_t msgInLength
Definition: CryptoCC26XX.h:436
struct CryptoCC26XX_Params CryptoCC26XX_Params
CryptoCC26XX Parameters.
struct CryptoCC26XX_Config * CryptoCC26XX_Handle
A handle that is returned from a CryptoCC26XX_open() call.
Definition: CryptoCC26XX.h:333
void * msgIn
Definition: CryptoCC26XX.h:466
Power notify object structure.
Definition: Power.h:112
uint32_t timeout
Definition: CryptoCC26XX.h:531
Definition: CryptoCC26XX.h:386
CryptoCC26XX_Mode
CryptoCC26XX Mode Settings.
Definition: CryptoCC26XX.h:341
CryptoCC26XX AES-ECB Transaction.
Definition: CryptoCC26XX.h:462
char * msgIn
Definition: CryptoCC26XX.h:432
void CryptoCC26XX_init(void)
Function to initializes bios modules needed by CryptoCC26XX module.
uint8_t intPriority
Crypto Peripheral's interrupt priority.
Definition: CryptoCC26XX.h:520
int CryptoCC26XX_transact(CryptoCC26XX_Handle handle, CryptoCC26XX_Transaction *transaction)
Function to do a Crypto operation (encryption or decryption) in blocking mode.
CryptoCC26XX_Mode mode
Definition: CryptoCC26XX.h:448
CryptoCC26XX_KeyStore keyStore
Definition: CryptoCC26XX.h:532
uint8_t keyIndex
Definition: CryptoCC26XX.h:449
uint16_t msgInLength
Definition: CryptoCC26XX.h:453
int powerMngrId
Definition: CryptoCC26XX.h:505
void * object
Definition: CryptoCC26XX.h:551
Semaphore_Struct transSem
Definition: CryptoCC26XX.h:544
Definition: CryptoCC26XX.h:387
Definition: CryptoCC26XX.h:381
uint8_t CryptoCC26XX_KeyStore
CryptoCC26XX Key.
Definition: CryptoCC26XX.h:402
CryptoCC26XX_Handle CryptoCC26XX_open(unsigned int index, bool exclusiveAccess, CryptoCC26XX_Params *params)
Function to initialize a given CryptoCC26XX peripheral specified by the particular index value...
CryptoCC26XX_Mode mode
Definition: CryptoCC26XX.h:464
void * nonce
Definition: CryptoCC26XX.h:450
CryptoCC26XX_KeyLocation
CryptoCC26XX Key Store Location.
Definition: CryptoCC26XX.h:377
int intNum
Definition: CryptoCC26XX.h:507
struct CryptoCC26XX_HWAttrs CryptoCC26XX_HWAttrs
CryptoCC26XX Hardware Attributes.
CryptoCC26XX_Mode mode
Definition: CryptoCC26XX.h:415
Definition: CryptoCC26XX.h:383
struct CryptoCC26XX_Transaction CryptoCC26XX_Transaction
CryptoCC26XX Transaction.
uint32_t timeout
Definition: CryptoCC26XX.h:394
CryptoCC26XX Object.
Definition: CryptoCC26XX.h:528
CryptoCC26XX_Mode mode
Definition: CryptoCC26XX.h:427
uint32_t baseAddr
Definition: CryptoCC26XX.h:503
struct CryptoCC26XX_AESECB_Transaction CryptoCC26XX_AESECB_Transaction
CryptoCC26XX AES-ECB Transaction.
struct CryptoCC26XX_AESCBC_Transaction CryptoCC26XX_AESCBC_Transaction
CryptoCC26XX AES-CBC Transaction.
Definition: CryptoCC26XX.h:380
int CryptoCC26XX_transactPolling(CryptoCC26XX_Handle handle, CryptoCC26XX_Transaction *transaction)
Function to do a Crypto transaction operation (encryption or decryption) in polling mode...
int CryptoCC26XX_transactCallback(CryptoCC26XX_Handle handle, CryptoCC26XX_Transaction *transaction)
Function to do a Crypto transaction operation (encryption or decryption) in callback mode...
uint8_t authLength
Definition: CryptoCC26XX.h:429
CryptoCC26XX AES-CBC Transaction.
Definition: CryptoCC26XX.h:446
Definition: CryptoCC26XX.h:378