Texas Instruments

TI-RTOS CC13XX and CC26XX 2.18.00.03 Release Notes

Table of Contents

Introduction

TI-RTOS delivers components that enable engineers to develop applications on Texas Instruments micro-controller devices. The product is comprised of multiple software components and examples of how to use these components together. TI-RTOS gives developers a one-stop RTOS solution for developing applications for TI embedded microcontrollers. It provides an OS kernel, communications support, drivers, and more. It is tightly integrated with the Code Composer Studio development environment. In addition, examples are provided to demonstrate the use of each functional area and each supported device and as a starting point for your own projects.

Documentation

The following documentation is provided with this release.

NOTE: Please view the Device Specific driver implementations as they may contain or exclude certain features that are defined in the top level interfaces.

Products Included

Click on the links below to view the release notes for the different products.

Boards Supported

Examples are provided for the following boards:

What’s New

To see what has changed in the TI-RTOS Drivers, see the separate TI-Drivers release notes in [as installed]/products/tidrivers_M_mm_pp_bb.

Defects fixed in this release:

Key Summary
TIRTOS-500 Update RF examples generated settings to use RF Studio 2.4.0
TIRTOS-501 Import latest CC13xx/CC36xx ccware/driverlib with RF bug fixes

Upgrade and Compatibility Information

Host Support

Dependencies

This release requires the following other software components and tools.

Validation Information

Known Issues

IMPORTANT NOTICE ON CC1350 BLUETOOTH(R) SMART: This TI RTOS release contains a pre-release version of the Bluetooth Smart radio configuration for CC1350. The Bluetooth Smart settings/overrides in this release should not be used in production of CC1350-based products. The CC1350 production-ready Bluetooth Smart settings/overrides are in their final stages of verification, and it should be expected that some radio-specific timings and parameters can change in the production release. This notice does not apply to the Bluetooth Smart settings/overrides for CC2640/50.

Versioning

All releases have 4 digits (M.mm.pp.bb). This includes GA and engineering releases. Engineering releases are denoted with an _eng suffix (e.g., 2.00.00.15_eng)

This product’s version follows a version format, M.mm.pp.bb, where M is a single digit Major number, mm is 2 digit minor number, pp is a 2 digit patch number, and b is an unrestricted set of digits used as an incrementing build counter.

To support multiple side-by-side installations of the product, the product version is encoded in the top level directory (e.g. tirtos_2_00_00_16).

Subsequent releases of patch upgrades will be identified by the patch number, ex. TI-RTOS 1.00.01.68 with directory tirtos_1_00_01_68. Typically, these patches only include critical bug fixes.

Technical Support and Product Updates