This is a General Availability (GA) of TI-RTOS . This version of TI-RTOS requires CCS 5.5.
MSP430 support has been added into this release, however it is at a "beta" level. The next release (1.21) will have GA support for MSP430. While not expected, there may be breaks in backward compability for MSP430 from 1.20 to 1.21. All of the other components in this release of TI-RTOS are at a GA level.The following documentation is available:
Release notes from previous releases are also available in the release notes archive directory.ID | Headline |
SDOCM00083850 | SD (SSI) Driver restrictions (one peripheral and one SSI slave select pin) |
SDOCM00094054 | tcpEcho does not handle more than two connections well |
SDOCM00097571 | Add docs for "Adding System Analyzer via USB CDC" |
SDOCM00100711 | select() should be removed from WiFi example when CC3000 is patched |
SDOCM00101013 | TI-RTOS module has work-around for platform issue with launchpad |
SDOCM00101241 | Need to be consistent on giving names to enums |
SDOCM00101243 | Document that SysFlex is deprecated (use xdc.runtime.SysCallback instead) |
SDOCM00101254 | TI-RTOS release notes should have pointers to sub-component docs (or release notes which point to docs) |
SDOCM00101371 | __EKS_LM4F232_H should be __EK_TM4C123GXL_H in EK_TM4C123GXL.h |
SDOCM00101494 | Getting Started Guide needs section on adding TI-RTOS to TI Resource Explorer |
SDOCM00101542 | USB serial and composite mouse/serial examples do not retrieve data correctly from the USB rxBuffer |
SDOCM00101590 | Change max payload size for WiFi driver grace page |
SDOCM00101857 | In Watchdog driver a few Void functions have return statements |
SDOCM00101998 | SPIMessageQTransport needs a valid errFxn function |
SDOCM00102004 | TI-RTOS Ethernet driver needs API for determining link status |
SDOCM00102576 | Race condition in WiFi driver |
SDOCM00103029 | Add EK-LM4F120XL board and examples back in |
SDOCM00103074 | Add I2C_config[] structure in Stellaris/Tiva launchpad board files. |
SDOCM00103106 | TI-RTOS examples should use ti.platforms.tiva instead of ti.platforms.stellaris |
SDOCM00103392 | Add DK_TM4C123G (renamed EKS_LM4F232 board) |
SDOCM00103573 | TI-RTOS drivers should offer zero-memory allocation option |
SDOCM00103901 | TI-RTOS should ship smaller footprint examples |
SDOCM00104272 | UARTTiva returns incorrect datapointer in callback fucntion when in UART_DATA_TEXT mode. |
SDOCM00104684 | USBMSCHFatFs's servicePriority param should default to highest not a hard-coded 15 |
This release requires the following other software components and tools versions to successfully function:
ID | Headline |
SDOCM00088081 | SD Card driver lacks CRC support |
SDOCM00093268 | Add parity and error checking for UART driver |
SDOCM00093967 | TI-RTOS Windows install will fail if installed in multiple or single directory that contains more than 38 characters in path |
SDOCM00094053 | TI-RTOS sub-products (e.g. UIA, IPC) are not linked into CCS Help |
SDOCM00097626 | Giving Priorities to Hwis from TI-RTOS Drivers |
SDOCM00098063 | UART driver needs to support DMA |
SDOCM00099017 | TI-RTOS needs to make sub-products examples accessible |
SDOCM00099460 | ping flood causes Concerto board to stop receiving interrupts |
SDOCM00099858 | Stellaris launchpad doesn't detect a USB disconnect event |
SDOCM00100494 | SPI driver was not tested in Slave Open Drain mode |
SDOCM00100864 | Multithreaded CC3000 Host Driver does not work properly |
SDOCM00100865 | TI-RTOS drivers should have top-level enable and disable APIs |
SDOCM00100945 | Make TCP/UDP Echo for CC3000 examples more like NDK TCP/UDP Echo examples |
SDOCM00101155 | Intermittent spin lock in USB library's USBHCDPipeRead() for LM4F232 |
SDOCM00101176 | SPIMessageQTransport does not support static creates |
SDOCM00101229 | HTTP demo doesn't show the current SD Card logging state |
SDOCM00101240 | Coverity for WiFi driver reports several defects in the CC3000 Host Driver |
SDOCM00102477 | I2CTiva driver get's stuck at a Semaphore_pend() when I2C bus arbitration was lost |
SDOCM00102563 | WiFi driver should not create Hwi instance |
SDOCM00103028 | Add USB Host examples to EK_TM4C123GXL |
SDOCM00103637 | MSP430 UART[USCIA] LibType_Instrumented is not recommended at baudrates > 9600 |
SDOCM00104253 | MSP430 Launchpad ez-FET UART emulation issue at buadrate > 28.8kbps |
SDOCM00104686 | UART in Stellaris launchpad not working above 9600 baud when used with windows apps that use rxtxSerial.dll driver |
SDOCM00104691 | USBMSCHFatFsTiva_open requires a heap since no task stack is provided to the Task_construct |
SDOCM00104772 | Support for USB in a MSP430 Empty project wizard |
SDOCM00104883 | improve stack usage in UARTTiva_open() and other XYZ_open() functions |
SDOCM00105002 | TI-RTOS examples with no heap get an error if they call BIOS_exit |
SDOCM00105005 | The EMACSnow driver needs a new name |
SDOCM00105047 | ROV for I2C for MSP430 does not work |
All releases have 4 digits (M.mm.pp.bb). This includes GA and pre-releases (engineering, EA, beta, etc.). Pre-releases are denoted with a suffix (e.g. 1.01.00.15_eng or 1.01.00.21-beta).
This product's version follows a version format, M.mm.pp.bb, where M is a single digit Major number, mm is 2 digit minor number, pp is a 2 digit patch number, and b is an unrestricted set of digits used as an incrementing build counter.
To support multiple side-by-side installations of the product, the product version is encoded in the top level directory, ex. tirtos_1_00_01_11.
Subsequent releases of patch upgrades will be identified by the patch number, ex. TI-RTOS 1.00.00.68 with directory tirtos_1_00_01_70. Typically, these patches only include critical bug fixes.
Please note that version numbers and compatibility keys are NOT the same. For an explanation of compatibility keys, please refer to the 'Upgrade and Compatibility Information' section.
For technical support, please refer to the Texas Instruments E2E BIOS Support Forum http://e2e.ti.com/support/embedded/bios/default.aspx or other forums in http://e2e.ti.com/ as needed.
Last updated: November 11, 2013