1 /*
2 * Copyright (c) 2013, Texas Instruments Incorporated
3 * All rights reserved.
4 *
5 * Redistribution and use in source and binary forms, with or without
6 * modification, are permitted provided that the following conditions
7 * are met:
8 *
9 * * Redistributions of source code must retain the above copyright
10 * notice, this list of conditions and the following disclaimer.
11 *
12 * * Redistributions in binary form must reproduce the above copyright
13 * notice, this list of conditions and the following disclaimer in the
14 * documentation and/or other materials provided with the distribution.
15 *
16 * * Neither the name of Texas Instruments Incorporated nor the names of
17 * its contributors may be used to endorse or promote products derived
18 * from this software without specific prior written permission.
19 *
20 * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
21 * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
22 * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
23 * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
24 * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
25 * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
26 * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
27 * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
28 * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
29 * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
30 * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
31 */
32 /*
33 * ======== Idle.xdc ========
34 *
35 */
36 package ti.sysbios.knl;
37
38 import xdc.rov.ViewInfo;
39
40 /*!
41 * ======== Idle ========
42 * Idle Thread Manager.
43 *
44 * The Idle module is used to specify a list of functions to be called
45 * when no other tasks are running in the system.
46 *
47 * If tasking is enabled (ie {@link ti.sysbios.BIOS#taskEnabled
48 * BIOS.taskEnabled} = true), then the Task module will create an "Idle task"
49 * with the lowest possible priority. When no other tasks are running, this
50 * idle task runs in an infinite loop, calling the list of functions
51 * specified by the Idle module.
52 *
53 * If tasking is disabled (ie {@link ti.sysbios.BIOS#taskEnabled
54 * BIOS.taskEnabled} = false), then the idle functions are called in an
55 * infinite loop within the {@link ti.sysbios.BIOS#start BIOS_start}
56 * function called within main().
57 *
58 * The list of idle functions is only statically configurable; it cannot be
59 * modified at runtime.
60 *
61 */
62
63 @DirectCall
64 module Idle
65 {
66 /*! Idle function type definition. */
67 typedef Void (*FuncPtr)();
68
69 metaonlystruct ModuleView {
70 UInt index;
71 UInt coreId;
72 String fxn;
73 }
74
75 /*! @_nodoc */
76 @Facet
77 metaonlyconfig ViewInfo.Instance rovViewInfo =
78 xdc.rov.ViewInfo.create({
79 viewMap: [
80 ['Idle.funcList',
81 {
82 type: ViewInfo.MODULE_DATA,
83 viewInitFxn: 'viewInitModule',
84 structName: 'ModuleView'
85 }
86 ]
87 ]
88 });
89
90 /*!
91 * ======== funcList ========
92 * @_nodoc 93 * The array of functions to be called when no other Tasks are running.
94 */
95 config FuncPtr funcList[length] = [];
96
97 /*!
98 * ======== coreList ========
99 * @_nodoc 100 * The array of coreIds associated with Idle funcList[]
101 */
102 config UInt coreList[length] = [];
103
104 /*!
105 * ======== idleFxns ========
106 * Functions to be called when no other Tasks are running
107 *
108 * Functions added to the Idle.idleFxns[] array, as well as those
109 * added via the Idle.addFunc() API will be run by the Idle loop.
110 *
111 * @a(NOTE) 112 * This array is intended for use by the GUI config tool.
113 *
114 * Config script authors are encourged to use the
115 * {@link #addFunc Idle.addFunc()} API to add idle functions
116 * to their applications.
117 */
118 metaonlyconfig FuncPtr idleFxns[length] = [
119 null, null, null, null, /* slots for GUI */
120 null, null, null, null
121 ];
122
123 /*!
124 * ======== addFunc ========
125 * Statically add a function to the Idle function list.
126 *
127 * Functions added to the Idle function list are
128 * called repeatedly by the Idle task function.
129 *
130 * @see Idle#run
131 *
132 * Usage example:
133 *
134 * @p(code) 135 * var Idle = xdc.useModule('ti.sysbios.knl.Idle');
136 * Idle.addFunc('&myIdleFunc'); // add myIdleFunc()
137 * @p 138 *
139 * @a(NOTE) 140 * Idle functions have the following signature:
141 * @p(code) 142 * Void func(Void);
143 * @p 144 */
145 metaonly Void addFunc(FuncPtr func);
146
147 /*!
148 * ======== addCoreFunc ========
149 * Statically add a core-unique function to the Idle function list.
150 */
151 metaonly Void addCoreFunc(FuncPtr func, UInt coreId);
152
153 /*!
154 * ======== loop ========
155 * @_nodoc 156 * Idle loop which calls the idle functions in an infinite loop.
157 *
158 * This function is called internally and is not normally intended
159 * to be called by the client.
160 *
161 * When tasking is enabled, the Task module creates an Idle task which
162 * simply calls this function. If tasking is disabled, then this function
163 * is called after main and any module startup functions.
164 *
165 * The body of this function is an infinite loop that calls the "run"
166 * function.
167 */
168 Void loop(UArg arg1, UArg arg2);
169
170 /*!
171 * ======== run ========
172 * Make one pass through idle functions
173 *
174 * This function is called repeatedly by the Idle task when
175 * the Idle task has been enabled in the Task module
176 * (see {@link Task#enableIdleTask}).
177 *
178 * This function makes one pass through an internal static array
179 * of functions made up of functions added using the
180 * {@link #addFunc Idle.addFunc()} API as well as any functions
181 * defined in the GUI tool's {@link #idleFxns Idle.idleFxns[]} array.
182 *
183 * This function returns after all functions have been executed one
184 * time.
185 *
186 * @see Idle#addFunc
187 * @see Task#enableIdleTask
188 * @see Task#allBlockedFunc
189 */
190 Void run();
191
192 }