1    /* 
     2     *  Copyright (c) 2008 Texas Instruments. All rights reserved.
     3     *  This program and the accompanying materials are made available under the
     4     *  terms of the Eclipse Public License v1.0 and Eclipse Distribution License
     5     *  v. 1.0 which accompanies this distribution. The Eclipse Public License is
     6     *  available at http://www.eclipse.org/legal/epl-v10.html and the Eclipse
     7     *  Distribution License is available at
     8     *  http://www.eclipse.org/org/documents/edl-v10.php.
     9     *
    10     *  Contributors:
    11     *      Texas Instruments - initial implementation
    12     * */
    13    /*
    14     *  ======== Error.xdc ========
    15     */
    16    
    17    /*!
    18     *  ======== Error ========
    19     *  Runtime error manager
    20     *
    21     *  The `Error` module provides mechanisms for raising, checking, and
    22     *  handling errors in a program. You can configure it via the
    23     *  `{@link Error#policy Error.policy}` and
    24     *  `{@link Error#raiseHook Error.raiseHook}` configuration parameters.
    25     *
    26     *  Modules may define specific error types and reference these when
    27     *  raising an error. Each error type has a custom error message and
    28     *  can be parameterized with up to `{@link #NUMARGS}` arguments. A
    29     *  generic error type is provided for raising errors when not in a module.
    30     *
    31     *  Use the `{@link #check Error_check()}` function to determine if an
    32     *  error has been raised. It is important to understand that it is the
    33     *  caller's responsibility to check the error block after calling a
    34     *  function that takes an error block as an argument. Otherwise, a raised
    35     *  error may go undetected, which could compromise the integrity of the
    36     *  system. For example:
    37     *
    38     *  @p(code)
    39     *  Task_create(..., &eb);
    40     *
    41     *  if (Error_check(&eb)) {
    42     *      ...an error has been raised...
    43     *  }
    44     *  @p
    45     *
    46     *  The `{@link #raiseHook Error.raiseHook}` configuration parameter allows
    47     *  a configured function to be invoked when any error is raised. This
    48     *  function is passed a pointer to the error's error block and makes it
    49     *  easy to manage all errors from a common point. For example, you can
    50     *  trap any error (fatal or not) by simply setting a breakpoint in this
    51     *  function. You can use the following functions to extract information
    52     *  from an error block.
    53     *
    54     *  @p(blist)
    55     *  - `{@link #getData Error_getData()}`
    56     *  - `{@link #getCode Error_getCode()}`
    57     *  - `{@link #getId Error_getId()}`
    58     *  - `{@link #getMsg Error_getMsg()}`
    59     *  - `{@link #getSite Error_getSite()}`
    60     *  @p
    61     *
    62     *  The Error module provides facilities for handling errors, but the Log
    63     *  module also provides features for logging error events. These are separate
    64     *  concepts; however, to ensure that users do not have to both raise and log
    65     *  an error, the Error module will automatically log an error event when one
    66     *  is raised. The Error module logs the standard {@link Log#L_error} event,
    67     *  passing it the error message and arguments.
    68     *
    69     *  The error event is logged to the Error module's logger using the Error
    70     *  module's diags mask. Logging of errors is enabled by default in the diags
    71     *  mask, but the event will not be logged unless a logger is configured for
    72     *  the Error module as well.
    73     *
    74     *  To make the error event appear as though it is coming from the module which
    75     *  called Error_raise, the event is logged with the caller's module id and
    76     *  with the caller's call site information.
    77     *
    78     *  @a(Examples)
    79     *  Example 1: The following example shows how a module, named ModA,
    80     *  defines a custom error type and shows how this error is raised by
    81     *  the module. The module defines an `Id` of `E_notEven` in its module
    82     *  specification file (in this case, `ModA.xdc`). The error's message
    83     *  string takes only one argument. The module also defines a `mayFail()`
    84     *  function that takes an error block. In the module's C source file,
    85     *  the function checks for the error condition and raises the error if
    86     *  needed.
    87     *
    88     *  This is part of ModA's XDC specification file for the module:
    89     *
    90     *  @p(code)
    91     *  config xdc.runtime.Error.Id E_notEven = {
    92     *      msg: "expected an even number (%d)"
    93     *  };
    94     *
    95     *  Void mayFail(Int x, xdc.runtime.Error.Block *eb);
    96     *  @p
    97     *
    98     *  This is part of the C code for the module:
    99     *
   100     *  @p(code)
   101     *  Void ModA_mayFail(Int x, Error_Block *eb)
   102     *  {
   103     *      if ((x % 2) != 0) {
   104     *          Error_raise(eb, ModA_E_notEven, x, 0);
   105     *          ...add error handling code here...
   106     *          return;
   107     *      }
   108     *      ...
   109     *  }
   110     *  @p
   111     *
   112     *  @p(html)
   113     *  <hr />
   114     *  @p
   115     *
   116     *  Example 2: The following C code supplies an error block to a function
   117     *  that requires one and tests the error block to see if the function
   118     *  raised an error. Note that an error block must be initialized before
   119     *  it can be used and same error block may be passed to several functions.
   120     *
   121     *  @p(code)
   122     *  #include <xdc/runtime/Error.h>
   123     *  #include <ti/sysbios/knl/Task.h>
   124     *  Error_Block eb;
   125     *  Task_Handle tsk;
   126     *
   127     *  Error_init(&eb);
   128     *  tsk = Task_create(..., &eb);
   129     *
   130     *  if (Error_check(&eb)) {
   131     *      ...an error has been raised...
   132     *  }
   133     *  @p
   134     *
   135     *  @p(html)
   136     *  <hr />
   137     *  @p
   138     *
   139     *  Example 3: The following C code shows that you may pass `NULL` to a
   140     *  function requiring an error block. In this case, if the function
   141     *  raises an error, the program is aborted (via
   142     *  `{@link System#abort xdc_runtime_System_abort()}`), thus execution
   143     *  control will never return to the caller.
   144     *
   145     *  @p(code)
   146     *  #include <xdc/runtime/Error.h>
   147     *  #include <ti/sysbios/knl/Task.h>
   148     *
   149     *  tsk = Task_create(..., NULL);
   150     *  ...will never get here if an error was raised in Task_create...
   151     *  @p
   152     *
   153     *  @p(html)
   154     *  <hr />
   155     *  @p
   156     *
   157     *  Example 4: The following C code shows how to write a function that
   158     *  is not part of a module and that takes an error block and raises
   159     *  the generic error type provided by the Error module. Note, if the
   160     *  caller passes `NULL` for the error block or if the error policy is
   161     *  `{@link #Policy TERMINATE}`, then the call to
   162     *  `{@link #raise Error_raise()}` will call
   163     *  `{@link System#abort xdc_runtime_System_abort()}` and never return.
   164     *
   165     *  @p(code)
   166     *  #include <xdc/runtime/Error.h>
   167     *
   168     *  Void myFunc(..., Error_Block *eb)
   169     *  {
   170     *      ...
   171     *
   172     *      if (...error condition detected...) {
   173     *          String  myErrorMsg = "my custom error message";
   174     *          Error_raise(eb, Error_E_generic, myErrorMsg, 0);
   175     *          ...add error handling code here...
   176     *          return;
   177     *      }
   178     *  }
   179     *  @p
   180     */
   181    @DirectCall
   182    
   183    module Error {
   184    
   185        /*!
   186         *  ======== Policy ========
   187         *  Error handling policies
   188         *
   189         *  Regardless of the current policy in use, raising an error by
   190         *  calling `{@link #raise Error_raise}` will always invoke the
   191         *  error raise hook function assigned to the
   192         *  `{@link #raiseHook Error.raiseHook}` configuration parameter.
   193         *
   194         *  @field(TERMINATE) All raised errors are fatal. A call to
   195         *  `{@link #raise Error_raise}` will never return to the caller.
   196         *
   197         *  @field(UNWIND) Errors are returned to the caller. A call to
   198         *  `{@link #raise Error_raise}` will return back to the caller.
   199         */
   200        enum Policy {
   201            TERMINATE,
   202            UNWIND
   203        };
   204    
   205        /*!
   206         *  ======== Desc ========
   207         *  Error descriptor
   208         *
   209         *  Each type of error is defined with an error descriptor. This
   210         *  structure groups common information about the errors of this type.
   211         *
   212         *  @field(msg) The error message using a `printf` style format string, 
   213         *              but limited to `{@link #NUMARGS}` arguments.
   214         *              This format string together with the two arguments passed
   215         *              to `Error_raise`` are used to create a human readable
   216         *              error message.
   217         *
   218         *  @field(code) A user assignable code, 0 by default. The user may
   219         *              optionally set this field during config to give the
   220         *              error a well-known numeric code. 
   221         */
   222        metaonly struct Desc {
   223            String msg;
   224            UInt16 code;
   225        };
   226    
   227        /*!
   228         *  ======== Id ========
   229         *  Error identifier
   230         *
   231         *  Each type of error raised is defined with a metaonly
   232         *  `{@link Error#Desc}`.  An `Error_Id` is a 32-bit target value that
   233         *  encodes the information in the `Desc`.  Target programs use
   234         *  `Error_Id` values to "raise" and check for specific errors.
   235         *
   236         *  @a(Warning) `{@link #Id}` values may vary among different
   237         *  configurations of an application.  For example, the addition of a
   238         *  new module to a program may result in a different absolute value for
   239         *  `{@link #E_generic}`.  If you need error numbers that remain
   240         *  invariant, use the user definable `{@link #Desc Desc.code}` field.
   241         */
   242        @Encoded typedef Desc Id;
   243        
   244        /*!
   245         *  ======== HookFxn ========
   246         *  Function called whenever an error is raised
   247         *
   248         *  The first parameter and only parameter passed to this function is a
   249         *  pointer to an `Error_Block`.  Even if the client passes a `NULL` error
   250         *  block pointer to `{@link #raise Error_raise}`, this parameter passed 
   251         *  to this "hook" function is always `non-NULL`.
   252         */
   253        typedef Void (*HookFxn)(Block *);
   254    
   255        /*!
   256         *  ======== NUMARGS ========
   257         *  Maximum number of arguments supported by an error
   258         */
   259        const Int NUMARGS = 2;
   260    
   261        /*!
   262         *  ======== Data ========
   263         *  Error args
   264         *
   265         *  The two arguments (arg1, arg2) passed to `{@link #raise}` are 
   266         *  stored in one of these arrays within the associated Error_Block.
   267         *  To access these arguments use `{@link #getData}` to obtain a 
   268         *  pointer to the Error_Block's Data array.
   269         *
   270         *  @see #getData
   271         */
   272        struct Data {
   273            IArg arg[NUMARGS];
   274        }
   275    
   276        /*!
   277         *  ======== Block ========
   278         *  Error block
   279         *
   280         *  An opaque structure used to store information about errors once raised.
   281         *  This structure must be initialized via `{@link #init Error_init()}`
   282         *  before being used for the first time.
   283         */
   284        @Opaque struct Block {
   285            UInt16      unused;     /* for backward compatibility (was code) */
   286            Data        data;       /* arguments passed to raise() */
   287            Id          id;         /* id passed to raise() */
   288            String      msg;        /* msg associated with id */
   289            Types.Site  site;       /* info about Error_raise call site */
   290            IArg        xtra[4];    /* future expansion */
   291        };
   292    
   293        /*!
   294         *  ======== PolicyFxn ========
   295         *  Error policy function signature
   296         *
   297         *  @a(Parameters)
   298         *  A policy function is passed the following parameters:
   299         *  @p(dlist)
   300         *      - `eb`
   301         *        A pointer to an `{@link #Block Error_Block}` structure to be
   302         *        initialized using the subsequent arguments.  This pointer may 
   303         *        be `NULL`.
   304         *      - `modId`
   305         *        The module ID of the module calling
   306         *        `{@link #raise Error_raise()}`
   307         *      - `fileName`
   308         *        A string naming the source file which made the call to
   309         *        `{@link #raise Error_raise()}`
   310         *      - `lineNumber`
   311         *        An integer line number within the file named above where
   312         *        the call `{@link #raise Error_raise()}` occured
   313         *      - `errId`
   314         *        The `{@link #Id Error_Id}` of the error being raised
   315         *      - `arg1` and `arg2`
   316         *        Two `IArg` arguments associated with the error being raised
   317         *  @p
   318         */
   319        typedef Void (*PolicyFxn)(Block *, Types.ModuleId, CString, Int, Id,
   320                                  IArg, IArg);
   321    
   322        /*!
   323         *  ======== policyFxn ========
   324         *  Error handler function
   325         *
   326         *  This function is called to handle all raised errors but, unlike
   327         *  `{@link raiseHook}`, this function is responsible for completely
   328         *  handling the error (including calling `{@link #raiseHook raiseHook}`
   329         *  with an appropriately initialized `{@link #Block Error_Block}`, if
   330         *  `raiseHook` functionality is required). 
   331         *
   332         *  The default value is a function which, in addition to calling `raiseHook`
   333         *  with an initialized `Error_Block` structure, logs the error using this
   334         *  module's logger.  
   335         *  
   336         *  Alternately, `{@link #policySpin}`, which simply loops 
   337         *  infinitely, can be used to minimize target footprint.  Note, this function
   338         *  does NOT call `raiseHook`.
   339         */
   340        config PolicyFxn policyFxn = Error.policyDefault;
   341    
   342        /*!
   343         *  ======== E_generic ========
   344         *  Generic error
   345         *
   346         *  This error takes advantage of the $S specifier to allow for recursive
   347         *  formatting of the error message passed to error raise.
   348         *
   349         *  For example, the following is possible:
   350         *  @p(code)
   351         *  Error_raise(eb, Error_E_generic, "Error occurred, code: %d", code);
   352         *  @p
   353         *
   354         *  @see System#extendedFormats
   355         *  @see System#printf
   356         */
   357        config Id E_generic = {msg: "%$S"};
   358    
   359        /*!
   360         *  ======== E_memory ========
   361         *  Out of memory error
   362         *
   363         *  The first parameter must be the heap instance handle. The second
   364         *  parameter is the size of the object for which the allocation failed.
   365         */
   366        config Id E_memory = {msg: "out of memory: heap=0x%x, size=%u"}; 
   367    
   368        /*!
   369         *  ======== E_msgCode ========
   370         *  Generic error that displays a string and a numeric value
   371         */
   372        config Id E_msgCode = {msg: "%s 0x%x"}; 
   373    
   374        /*!
   375         *  ======== policy ========
   376         *  System-wide error handling policy
   377         */
   378        config Policy policy = UNWIND;
   379    
   380        /*!
   381         *  ======== raiseHook ========
   382         *  The function to call whenever an error is raised
   383         *
   384         *  If set to a non-`null` value, the referenced function is always
   385         *  called when an error is raised, even if the `Error` policy is
   386         *  `{@link #Policy TERMINATE}`.  In rare cases, it is possible that a
   387         *  raised error does not trigger a call to `raiseHook`; see
   388         *  `{@link #maxDepth}`.
   389         *
   390         *  By default, this function is set to `{@link #print Error_print}`
   391         *  which causes the error to be formatted and output via
   392         *  `{@link xdc.runtime.System#aprintf System_printf}`.  Setting this
   393         *  configuration parameter to `null` indicates that no function hook
   394         *  should be called.
   395         *
   396         *  @see #maxDepth
   397         *  @see #HookFxn
   398         *  @see #print
   399         */
   400        config HookFxn raiseHook = Error.print;
   401    
   402        /*!
   403         *  ======== maxDepth ========
   404         *  Maximum number of concurrent calls to `{@link #raiseHook}`
   405         *
   406         *  To prevent errors that occur in the raiseHook function from
   407         *  causing an infinite recursion, the maximum number of concurrent
   408         *  calls to `{@link #raiseHook}` is limited by `Error_maxDepth`.  If
   409         *  the number of concurrent calls exceeds `Error_maxDepth`, the
   410         *  `raiseHook` function is not called.
   411         *
   412         *  In multi-threaded systems, errors raised by separate threads may
   413         *  be detected as recursive calls to `raiseHook`.  So, setting
   414         *  `Error.maxDepth` to a small value may - in rare instances - result in
   415         *  `errorHook` not being called for some raised errors.
   416         *
   417         *  If it is important that all raised errors trigger a call to the
   418         *  `raiseHook` function, set `Error.maxDepth` to an impossibly large
   419         *  number (0xffff) and either ensure that the raise hook never calls a
   420         *  function that can raise an error or add checks in `raiseHook` to
   421         *  protect against "double faults".
   422         */
   423        config UInt16 maxDepth = 16;
   424        
   425        /*!
   426         *  ======== check ========
   427         *  Return TRUE if an error was raised
   428         *
   429         *  @param(eb) pointer to an `Error_Block` or `NULL`
   430         *
   431         *  @a(returns)
   432         *  If `eb` is non-`NULL` and `{@link #policy Error.policy} == UNWIND` and
   433         *  an error was raised on `eb`, this function returns `TRUE`.  Otherwise,
   434         *  it returns `FALSE`.
   435         */
   436        Bool check(Block *eb);
   437    
   438        /*!
   439         *  ======== getData ========
   440         *  Get an error's argument list
   441         *
   442         *  @param(eb)      non-`NULL` pointer to an `Error_Block`
   443         *
   444         *  @a(returns)
   445         *  `getData` returns an array of type `{@link #Data}` with
   446         *  `{@link #NUMARGS}` elements containing the arguments provided
   447         *  at the time the error was raised.
   448         *
   449         *  @see #raise
   450         */
   451        Data *getData(Block *eb);
   452    
   453        /*!
   454         *  ======== getCode ========
   455         *  Get an error's code
   456         *
   457         *  @param(eb) non-`NULL` pointer to an `Error_Block`
   458         *
   459         *  @a(returns)
   460         *  `getCode` returns the error code associated with this error block.
   461         *
   462         *  @see #raise
   463         *  @see #Desc
   464         */
   465        UInt16 getCode(Block *eb);
   466    
   467        /*!
   468         *  ======== getId ========
   469         *  Get an error's id
   470         *
   471         *  @param(eb) non-`NULL` pointer to an `Error_Block`
   472         *
   473         *  @a(Warning)
   474         *  `Error_Id` values may vary among different configurations
   475         *  of an application.  For example, the addition of a new module to a
   476         *  program may result in a different absolute value for
   477         *  `{@link #E_generic}`.  If you need error numbers that remain
   478         *  invariant, use the user definable `{@link #Desc Desc.code}` field.
   479         *
   480         *  @see #raise
   481         *  @see #Desc
   482         */
   483        Id getId(Block *eb);
   484    
   485        /*!
   486         *  ======== getMsg ========
   487         *  Get an error's "printf" format string
   488         *
   489         *  @param(eb) non-`NULL` pointer to an `Error_Block`
   490         *
   491         *  @see #raise
   492         *  @see #Desc
   493         */
   494        String getMsg(Block *eb);
   495    
   496        /*!
   497         *  ======== getSite ========
   498         *  Get an error's call site info
   499         *
   500         *  @param(eb) non-`NULL` pointer to an `Error_Block`
   501         *
   502         *  @a(returns)
   503         *  `getSite` returns a pointer to an initialized
   504         *  `{@link Types#Site Types.Site}` structure.  However, in the
   505         *  event that the call site was compiled with `xdc_FILE` defined to
   506         *  be `NULL` (to minimize string space overhead) the `file`
   507         *  field may be set to `NULL`.
   508         *
   509         *  @see #raise
   510         *  @see #Desc
   511         */
   512        Types.Site *getSite(Block *eb);
   513    
   514        /*!
   515         *  ======== idToCode ========
   516         *  Extract the user's error code associated with an `Error_Id`
   517         *
   518         *  @param(id) `Error_Id` from which to extract the user defined
   519         *             code 
   520         *  @_nodoc
   521         */
   522        @Macro UInt16 idToCode(Id id);
   523        
   524        /*!
   525         *  ======== idToUid ========
   526         *  Extract the unique error id associated with an `Error_Id`
   527         *
   528         *  @param(id) `Error_Id` from which to extract the system unique
   529         *             id associated with the specified `Error_Id`
   530         *  @_nodoc
   531         */
   532        @Macro UInt16 idToUid(Id id);
   533    
   534        /*!
   535         *  ======== init ========
   536         *  Put an error block into its initial state
   537         *
   538         *  To ensure reliable error detection, clients must call `init` for
   539         *  an `Error_Block` prior to any use.
   540         *  
   541         *  If the same Error Block is used multiple times, only the last error
   542         *  raised is retained.
   543         *
   544         *  @param(eb) pointer to an `Error_Block` or `NULL`
   545         *
   546         *      If `eb` is `NULL` this function simply returns.
   547         */
   548        Void init(Block *eb);
   549    
   550        /*!
   551         *  ======== print ========
   552         *  Print error using System.printf()
   553         *
   554         *  This function prints the error using `System_printf()`.  The output
   555         *  is on a single line terminated with a new line character and has the
   556         *  following form:
   557         *  @p(code)
   558         *      <site>: <file>, line <line_num>: <err_msg>
   559         *  @p
   560         *  where `<site>` is the module that raised the error, `<file>` and
   561         *  `<line_num>` are the file and line number of the containing the call
   562         *  site of the `Error_raise()`, and `<err_msg>` is the error message
   563         *  rendered with the arguments associated with the error.
   564         *
   565         *  @param(eb) pointer to an `Error_Block` or `NULL`
   566         *
   567         *      If `eb` is `NULL` this function simply returns with no output.
   568         *
   569         *  @a(Warning)
   570         *  This function is not protected by a gate and, as a result,
   571         *  if two threads call this method concurrently, the output of the two
   572         *  calls will be intermingled.  To prevent intermingled error output,
   573         *  you can either wrap all calls to this method with an appropriate
   574         *  `Gate_enter`/`Gate_leave` pair or simply ensure that only one
   575         *  thread in the system ever calls this method.
   576         */
   577        Void print(Block *eb);
   578        
   579        /*!
   580         *  ======== policyDefault ========
   581         *  Default implementation of the policyFxn
   582         *
   583         *  This function is the implementation which is plugged in by default to
   584         *  the `{@link #policyFxn}`. It processes the error and logs it before
   585         *  returning to the caller or aborting - depending on the error policy
   586         *  `{@link #policy}`.
   587         */
   588        Void policyDefault(Block *eb, Types.ModuleId mod, CString file, Int line,
   589            Id id, IArg arg1, IArg arg2);
   590    
   591        /*!
   592         *  ======== policySpin ========
   593         *  Lightweight implementation of the policyFxn
   594         *
   595         *  This function is a lightweight alternative  which can be plugged in to
   596         *  the `{@link #policyFxn}`. It just loops infinitely.
   597         *
   598         *  @a(Warning)
   599         *  This function does not call `{@link #raiseHook}` and never returns to 
   600         *  the caller.  As a result, ANY error raised by the application will cause 
   601         *  it to indefinitly hang.
   602         */
   603        Void policySpin(Block *eb, Types.ModuleId mod, CString file, Int line,
   604            Id id, IArg arg1, IArg arg2);
   605    
   606        /*!
   607         *  ======== raise ========
   608         *  Raise an error
   609         *
   610         *  This function is used to raise an `Error` by writing call site,
   611         *  error ID, and error argument information into the `Error_Block`
   612         *  pointed to by `eb`.
   613         *
   614         *  If `Error_raise` is called more than once on an `Error_Block` object,
   615         *  the previous error information is overwritten; only the last error 
   616         *  is retained in the `Error_Block` object.
   617         *
   618         *  In all cases, any configured `{@link #raiseHook Error.raiseHook}`
   619         *  function is called with a non-`NULL` pointer to a fully
   620         *  initialized `Error_Block` object.
   621         *
   622         *  @param(eb) pointer to an `Error_Block` or `NULL`
   623         *
   624         *      If `eb` is `NULL` or `{@link #policy Error.policy} == TERMINATE`,
   625         *      this function does not return to the caller; after calling any
   626         *      configured `{@link #raiseHook}`, `System_abort` is called with the
   627         *      string `"xdc.runtime.Error.raise: terminating execution\n"`.
   628         *
   629         *  @param(id) the error to raise
   630         *
   631         *      This pointer identifies the class of error being raised;
   632         *      the error class indicates how to interpret any subsequent 
   633         *      arguments passed to `{@link #raise}`.
   634         *
   635         *  @param(arg1) error's first argument
   636         *
   637         *      The argument interpreted by the first control character
   638         *      in the error message format string. It is ignored if not needed.
   639         *
   640         *  @param(arg2) error's second argument
   641         *
   642         *      The argument interpreted by the second control character
   643         *      in the error message format string. It is ignored if not needed.
   644         */
   645        @Macro Void raise(Block *eb, Id id, IArg arg1, IArg arg2);
   646    
   647        /*! @_nodoc */
   648        Void raiseX(Block *eb, Types.ModuleId mod, CString file, Int line,
   649            Id id, IArg arg1, IArg arg2);
   650    
   651        /*! @_nodoc EXPERIMENTAL */
   652        Void setX(Block *eb, Types.ModuleId mod, CString file, Int line,
   653            Id id, IArg arg1, IArg arg2);
   654    
   655    internal:
   656    
   657        struct Module_State {
   658            UInt16      count;
   659        };
   660    
   661    }
   662    /*
   663     *  @(#) xdc.runtime; 2, 1, 0,471; 3-20-2014 17:05:45; /db/ztree/library/trees/xdc/xdc-A32x/src/packages/
   664     */
   665